Connecting Frame Grabbers#
Safety Information#
WARNING – Laser Safety Instructions
To avoid injuries, always follow these safety instructions:
Optical fiber connections emit laser radiation in the infrared range. Laser radiation is invisible and can cause eye damage if the eyes are exposed to it directly. Never look into open fiber ends or active optical ports. Before any installation, maintenance, or cleaning, disconnect the connection or shut it down safely. Dispose of fiber remnants with care.
Electric Shock Hazard
Installing the frame grabber while the computer is connected to power may cause electric shock. Serious injury or death may occur.
- Before installing the frame grabber, switch off the computer and the connected devices and unplug all power cables from the computer.
- Before power-up, close the computer case
Electrostatic discharge may damage electronic components.
- Before touching the frame grabber, drain static charges from yourself to ground, e.g., by touching a metal water tap.
- During installation, make sure that you remain properly grounded, e.g., by wearing an antistatic wrist strap.
Overheating may damage the frame grabber and other components.
Make sure that you use an adequate ventilation system within your computer, and leave sufficient free space between your frame grabber and other cards. Boards with active cooling should have at least one free slot between cards. Secure the frame grabber so that it cannot move or vibrate. Do not block the ventilation openings.
Connecting Fiber Frame Grabbers to a Host Computer#
These instructions apply to imaFlex 2 Dual 100.
To install the frame grabber:
Info
-
To avoid damaging the cooling plate, only touch the frame grabber at the edges of the circuit board and on the slot bracket, and only apply pressure there when inserting it.
-
To ensure that the frame grabber achieves its maximum speed, the PCIe slot must have at least 16 wired PCIe lanes and support at least PCIe Generation 3 (Gen 3).
- Turn off the Fast Start-Up feature under Windows, see www.windowscentral.com
- Shut down your computer.
- Disconnect your computer from power supply.
-
Plug your frame grabber into a free PCIe x16 Gen3 (or higher) slot of your computer. To find out which PCIe interface is required on your computer for your frame grabber, see Requirements (Frame Grabbers).
Info
Make sure that the frame grabber is not tilted and is fully inserted.
-
Plug the female 8-pin computer power supply connector into the frame grabber. If your computer doesn't provide a matching power supply connector, use an adapter.
- Re-connect your computer to the power outlet.
- Boot your computer.
Connecting the QSFP28 Modules#
The imaFlex 2 Dual 100 frame grabber provides QSFP28 connectors C0 and C1. The QSFP28 modules connect these connectors to the fiber optic cable.
To connect the QSFP28 modules to connectors C0 and C1:
- Check that the module type, the wavelength, the reach, and the fiber type match the application. The Basler Module QSFP28 100G SR4 MPO 100m is a multimode module with a nominal wavelength of 850 nm. For the wavelength, the reach, and the fiber type, see General Specifications.
- Check that the transmitter (TX) and receiver (RX) fiber assignments are correct. For a typical CoaXPress-over-Fiber setup, use a type B polarity cable such as the Basler Cable Optical, MPO, 8x PC/F. For the fiber positions and for type B polarity, see MPO Connector.
- If the cable doesn't sit firmly on the modules, clean the optical interfaces, and then insert the cable into the modules. For cleaning instructions, see the Handling and Cleaning topic of the Basler Module QSFP28 100G SR4 MPO 100m.
- Insert each QSFP28 module into the host port until the locking mechanism engages. Keep unused ports covered with dust caps.
- Route the cable as described in the Safety and Handling topic of the Basler Cable Optical, MPO, 8x PC/F. For airflow and module temperature, see the Safety and Handling topic of the Basler Module QSFP28 100G SR4 MPO 100m. For the operating temperature, see Recommended Operating Conditions.
If the optical link is unstable or packets are lost, see If the Optical Link Is Unstable.
Connecting CoaXPress Frame Grabbers to a Host Computer#
These instructions apply to all CoaXPress frame grabbers: imaFlex CXP-12 Quad, imaFlex CXP-12 Penta, imaWorx CXP-12 Quad, marathon ACX-SP, marathon ACX-DP, marathon ACX-QP, and marathon VCX-QP.
To install the frame grabber:
- Turn off the Fast Start-Up Feature under Windows, see www.windowscentral.com.
- Shut down your computer.
- Disconnect your computer from power.
-
Plug your frame grabber into a free PCIe slot of your computer.
To find out which PCIe interface is required on your computer for your frame grabber, see Hardware Requirements.Info
To operate the frame grabber, you can either power it via the CoaxPress cable using the power over CoaXPress functionality (PoCXO), or you must connect the frame grabber to the computer power supply with an additional cable.
If you want to power the camera via the frame grabber, the frame grabber needs an extra connection to the computer power supply.
-
Plug the female computer power supply connector into the frame grabber. If your computer doesn't provide a matching power supply, use an according adapter.


-
Re-connect your computer to the power outlet.
- Boot your computer.
Info
If you are using Linux, proceed with Installing the Framegrabber SDK Software under Linux, and after installing the Framegrabber SDK, continue with section Board Test.
Connecting Camera Link Frame Grabbers to a Host computer#
Connecting an externally powered Camera Link camera while it is powered on may damage electric components.
Before connecting an externally powered Camera Link camera to the frame grabber, make sure it is powered off. This does not apply to cameras powered via Power over Camera Link (PoCL).
These instructions apply to all Camera Link frame grabbers: marathon ACL, marathon VCL, and marathon VCLx.
To install the frame grabber:
- Turn off the Fast Start-Up Feature under Windows.
- Shut down your computer.
- Disconnect your computer from power.
-
Plug your frame grabber into a free PCIe (Gen. 2) x4 slot of your computer.

-
Re-connect your computer to the power outlet.
- Boot your computer.
Info
If you are using Linux, proceed with Installing the Framegrabber SDK Software under Linux, and after installing the Framegrabber SDK, continue with section Enabling PoCL Support.
Checking Whether Your Frame Grabber is Recognized in the Windows Device Manager#
After booting, your frame grabber is recognized in the Windows Device Manager under Multifunction adapters.

Info
If your frame grabber isn't displayed under Multifunction adapters, or if even Multifunction adapters isn't displayed in the Windows Device Manager, the Framegrabber SDK software has not been installed yet on your computer.
For installation instructions, see section Installing the Framegrabber SDK Software. The relevant driver will be installed together with the Framegrabber SDK.
Installing the Framegrabber SDK Software#
For instructions on how to install the Framegrabber SDK software, refer to section Installing the Framegrabber SDK Software.
Frame Grabber Licenses for Programmable Frame Grabbers#
This information applies to programmable frame grabbers, i.e., imaFlex 2 Dual 100, imaFlex CXP-12 Penta, imaFlex CXP-12 Quad, marathon VCX-QP, marathon VCL, and marathon VCLx.
You must license your programmable frame grabber in the following cases:
- You are using a specific VisualApplets application, for instance 3D-StereoVision, which requires a separate frame grabber license.
- You are using user code related applets.
Before running applets that require a frame grabber license, the system checks whether the according frame grabber license is stored in memory. If no license is found, the applet won't run.
For more information, see Licensing a Programmable Frame Grabber.