Flashing via Command Line#
You find GrabberFirmwareFlasher.exe in the Framegrabber SDK installation directory <Framegrabber SDK installation directory>/bin.
The Grabber Firmware Flasher allows to write an applet (*.dll or *.hap file) onto a specific partition of the flash memory of a specific board. You need to specify:
- Board index (within your system)
- Flash memory partition
- File name (with extension) of applet file
- The Grabber Firmware Flasher looks within your Framegrabber SDK software installation for the specified applet file (in directory <Framegrabber SDK installation directory>/firmware/<frame grabber type>
To start the Grabber Firmware Flasher:
-
Go to the bin directory and run GrabberFirmwareFlasher.exe.
The help information is displayed:

-
Specify board index, memory partition, and applet file name. You have the following commands available:
GrabberFirmwareFlasher.exe --b <board_index> --partition <flashing partition> <name of applet file>Example:
GrabberFirmwareFlasher.exe --board 0 --partition 4 Acq_SingleBaseGray.dll -
Press Enter.
The tool starts flashing the named partition with the specified applet:

-
Restart all applications that are using the board:
- Close all applications of the Framegrabber SDK (microDisplay X, microDiagnostics, GenICam Explorer).
- After re-opening them, the applications provide access to the applet you set as active.
You can continue with configuring the applet via microDisplay X (see Initial System Test (microDisplay X)) or via Framegrabber API.