marathon ACL#
Depending on the applets you are running on the board, you may need to enable the PoCL support via microDiagnostics. The automatic PoCL detection is disabled per default on marathon ACL when running standard applets version 2.0 or higher, or when running individual applets created with VisualApplets version 3.0.6 or higher. When you use PoCL cameras together with such applets, you must enable automatic PoCL detection. This is possible in microDiagnostics (runtime version 5.5.1 or higher). For details, see Enabling PoCL Support.

To install the marathon ACL in your computer, plug it into a PCIe Gen. 2 x4 slot or higher. The following image shows a marathon ACL with two Camera Link cameras connected:

Image Processing#
Image processing functionality is available on request. If you are interested, contact Basler Support.
Production Line Integration#
For integration into a production line, marathon ACL offers multiple general purpose inputs and outputs. Depending on the hardware add-ons used, 4 to 20 GPIOs are available, also galvanically isolated.
These GPIOs enable you to do the following:
- Control peripheral devices by sending trigger signals, e.g. lighting signals and cameras signals.
- Receive various trigger signals from peripheral devices, e.g., shaft encoders and light barriers.
- Synchronize multiple marathon ACL frame grabbers
- Synchronize connected devices.

Communication between camera and marathon ACL is realized via serial interface and four CC signals per Camera Link cable.
Software Programming and Configuration Interface#
marathon ACL offers an easy-to-use API. The Framegrabber API allows to integrate the frame grabber into any image processing application. You can use the Framegrabber API to write code in the following languages:
- C/C++
- C# (wrapper available)
- Python (wrapper available)
For more information about the Framegrabber API, see the Framegrabber API documentation.
Alternatively, you can use Basler's GenTL Interface to develop your application in form of a GenTL consumer. For more information about the Basler GenTL Interface, see GenTL Interface documentation.
Connectors and LEDs#
Connectors#
marathon ACL has the following connectors:

Configuration Switch#
marathon ACL offers an on-board configuration switch for activating a fall-back FPGA configuration, called SAVE configuration. For details regarding the SAVE configuration, see FPGA Fall-Back Configuration.

LEDs on the Board#
marathon ACL provides the following LEDs on the board:

| LED Name | LED Color | Meaning |
|---|---|---|
| TRG_PWR | Green | Front GPIO is connected to external power (power IN). |
| SAVE | RED | SAVE configuration is used for FPGA configuration |
| READY | Orange | The FPGA has been configured successfully and is ready for operation. LED READY also gives light when SAVE configuration is used on FPGA. |
| PGOOD | Orange | PGOOD=Power Good All voltages are applied correctly. |
| CL A | Orange | Port A is connected to a camera that provides a clock. |
| CL B | Orange | Port B is connected to a camera that provides a clock. |
| PoCL A | Green | Power over Camera Link active on port A: Camera on port A is provided with power by frame grabber via Camera Link cable. |
| PoCL B | Green | Power over Camera Link active on port B: Camera on port B is provided with power by frame grabber via Camera Link cable. |
| USR1 | Orange | User-defined. The LEDs can be controlled via software. They aren't related to camera connectors and can be used for any purpose. |
| USR2 | Orange | User-defined. The LEDs can be controlled via software. They aren't related to camera connectors and can be used for any purpose. |
| PWR | Green | Frame grabber gets 12 VDC IN via PCIe interface. |
Specifications#
| marathon ACL | |
|---|---|
| Order Number | 2200000358 |
| Host Interface | PCIe Gen 2 x4 (Direct Memory Access) |
| Bandwidth (typ./max.) | Up to 1.8 GB/s sustainable data bandwidth (maximal Camera Link data rate 850 MByte/s) |
| On-Board Memory | 512 MByte DDR3-RAM |
| Power Supply (Input) / Current PCIe Slot | 12 VDC (±5 %) / <1.5 A (actual values depend on processing) |
| PoCXP Supply (Output) | 4 W of 12 VDC regulated power per each Camera Link connector |
| Power Consumption | Typ. 1 A @ 12 VDC (actual values depend on processing) |
| Size (L x H) | PCIe standard height Half length card: 167.64 mm x 111.15 mm |
| Weight | 200 g |
| Camera Interface | 2 x Camera Link 2.0 standard (2 * SDR 26) (mini CL) |
| Ambient Temperature | 50 °C (0 LFMa) 60 °C (100 LFMa) An adequate airflow in the computer is recommended. |
| FPGA Operating Temperatureb | 0–85 °C at 100 LFMa |
| Storage Temperature | -50–80 °C |
| Humidity during Operation | 5–90 % non-condensing |
| Humidity during Storage | 5–95 % |
| Compliance | CE, FCC, UKCA, RoHS |
Info
The PCIe bus data throughput depends on the mainboard, the chip set, and the BIOS configuration of the host computer. The number of installed PCIe boards also affects the throughput, e.g. a PCIe x4 connector may support only x1 performance. Always check the mainboard manual thoroughly to be sure.
The Front GPIO Connector#
The front GPIO connector covers the basic trigger setup of your frame grabber. Its trigger connector allows you to control peripheral devices (PLC) and to synchronize multiple marathon ACL boards.

The socket is located directly on the slot bracket:

In default configuration, the trigger connector of the front GPIO connector offers:
- 3 differential input signals or 2 differential and 1 single-ended input signal in pull-up mode
- 2 TTL output signals
Info
You can configure the pin assignment of the front GPIO connector to provide different input signals, e.g.:
- Pull-down
- 4 single-ended signals (and no differential signals).
To change the GPIO configuration, use the command line tool installed with the Framegrabber SDK.
For more information, see Input Configuration and gpioTool.
Pin Layout of the Front GPIO Connector#

| PIN Number | Galvanically Isolated | Signal | Reference Signal |
|---|---|---|---|
| 1 | No | GPO 0 (TTL) | 5 VDC / global GND (pin 6) |
| 2 | No | GPO 1 (TTL) | 5 VDC / global GND (pin 6) |
| 3 | No | Reserved for RS 485 (GND) | |
| 4 | No | Reserved for RS 485 | |
| 5 | No | — | |
| 6 | No | GND (global GND) | |
| 7 | No | 5 V_OUT (0.5 A max) | |
| 8 | Yes | Single-ended signal: GPI 2 Differential signal: GPI2+ | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 9 | Yes | Single-ended signal: GPI 3 Differential signal: GPI2- (i.e., the inverted signal of GPI 2) | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 10 | Yes | GPI voltage IN (4.5–28 VDC) | |
| 11 | Yes | Single-ended signal: GPI 0 Differential signal: GPI0+ See also the info box below. | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 12 | Yes | Differential signal: GPI0- (i.e., the inverted signal of GPI 0) See also the info box below. | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 13 | Yes | Single-ended signal: GPI 1 Differential signal: GPI1+ See also the info box below. | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 14 | Yes | Differential signal: GPI1- (i.e., the inverted signal of GPI 1) See also the info box below. | GPI voltage IN (pin 10) / GPI GND (pin 15) |
| 15 | Yes | GPI GND |
Info
You can also connect a single-ended signal to pin 11 (GPI 0) and pin 13 (GPI 1). Do not use pin 12 and pin 14 for these single-ended signals.
In GPI0-, GPI1-, and GPI2-, the minus sign marks the inverted signal of GPI 0, GPI 1, and GPI 2. It does not mark a negative voltage.
Extra Voltage IN/GND for Galvanically Isolated Circuit#
All General Purpose Inputs (GPIs) of the front GPIO connector are galvanically isolated. The incoming signals are transferred to the frame grabber via digital isolators. This way, the frame grabber is securely protected against high incoming voltages.
However, to operate the internal GPI circuits, you must connect a voltage source and ground: On pin 10, you apply the voltage (GPI voltage IN) that serves as operating voltage for the internal operational amplifiers. On pin 15, you connect the according ground (GPI GND).
Supply Voltage Required
The marathon ACL trigger system needs to get supply voltage on the GPI Voltage IN pin (pin 10). If you want to connect devices that have no PWR pin, you must provide the power supply to the GPI Voltage IN pin (pin 10) from an external source.
Possible Topologies#
You can operate marathon ACL as follows:
| Number of Cameras | Number of Camera Ports | Number of Frame Grabber Ports | Mode | Topology |
|---|---|---|---|---|
| 1 | 1 | 2 | Bayer Pattern | |
| 1 | 1 | 2 | Grayscale | |
| 1 | 1 | 2 | RGB | |
| 1 | 2 | 2 | Bayer Pattern | |
| 1 | 2 | 2 | Grayscale | |
| 1 | 2 | 2 | RGB | |
| 2 | 1 | 2 | Bayer Pattern | |
| 2 | 1 | 2 | Grayscale | |
| 2 | 1 | 2 | RGB |
To find out which topology you can use with which applet, refer to Choosing the Right Area Scan Applet or Choosing the Right Line Scan Applet.
Acquisition Applets#
To ensure optimum use of system resources, not all image acquisition and processing features designed for marathon ACL are loaded onto marathon ACL simultaneously.
Instead, Basler provides various compilations of specific image acquisition and processing features that are combined to meet the requirements of a specific application field.
Typically, an applet supports a specific camera interface standard and topology, specific image acquisition features, and possibly specific image (pre-)processing features.
Applets come in .dll files.
Refer to Acquisition Applets for marathon ACL for more detailed information about the delivered acquisition applets and their dependency on the topology used.
For PDF documentation of the delivered acquisition applets (GenTL and Fglib), see Acquisition Applets for marathon ACL Documentation.
Precautions#
→ See Safety Instructions (Frame Grabbers).
Installation#
→ See Connecting Frame Grabbers.
→ See Connecting Cameras.