Skip to content

Heat Sinks for Basler boost V Cameras#

The heat sinks for Basler boost V cameras provide an efficient way for heat dissipation during camera operation.

Info

This heat sink isn't suitable for Basler boost R cameras.

Installing heat sinks is only necessary if your application causes the camera to exceed its maximum operating temperature specified in the "Environmental Requirements" section of your camera model topic.

Heat Sinks for Basler boost V Cameras

  • Order number: 2200001253
  • Two heat sinks will be delivered under this order number. Each heat sink is delivered with two screws for mounting on the camera's side.

For optimum cooling results, Basler recommends using two heat sinks on either side of the camera.

Technical Drawings#

Basler boost V Heat Sinks Dimensions

Physical Specifications#

Dimensions See Technical Drawings
Material Black anodized aluminum
Screws M4 × 10, DIN 7984

General Information#

RoHS Compliance Yes
Warranty 1 year

For more information about your camera, installation, and providing heat dissipation, read the topic about your boost V camera model, the Hardware Installation, and the Providing Heat Dissipation topics.