Skip to content

Device Information Parameters#

Device information parameters allow you to retrieve basic information about the camera.

This topic describes the parameters and the information each parameter provides.

Using the Feature#

Standard Device Information Parameters#

All Basler cameras mentioned in this documentation provide the following device information parameters:

Parameter Name Display Name Description
DeviceFirmwareVersion Device Firmware Version The camera's firmware version number.
DeviceManufacturerInfo Device Manufacturer Info The camera's manufacturer name. Usually contains an empty string.
DeviceModelName Device Model Name The camera's model name, e.g., acA3800-14um.
DeviceScanType Device Scan Type The scan type of the camera's sensor (Areascan or Linescan)
DeviceSerialNumber Device Serial Number The camera's serial number.
DeviceUserID Device User ID Used to assign a user-defined name to a camera. The name is displayed in the Basler pylon Viewer and the Basler pylon USB Configurator. The name is also visible in the "friendly name" field of the device information objects returned by pylon's device enumeration procedure.
On USB cameras, you must reset the camera using the DeviceReset command for the changes to take effect.
DeviceVendorName Device Vendor Name The camera's vendor name, e.g., Basler.
DeviceVersion Device Version The camera's version number.
HeightMax Height Max The maximum allowed height of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available).
SensorHeight Sensor Height The actual height of the camera's sensor in pixels.
SensorWidth Sensor Width The actual width of the camera's sensor in pixels.
WidthMax Width Max The maximum allowed width of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available).

Additional Device Information Parameters#

Depending on your camera model, the following additional device information parameters are available:

Parameter Name Display Name Description
DeviceFamilyName Device Family Name The identifier of the product family of the device, e.g., "Basler ace 2"
DeviceIndicatorMode Device Indicator Mode Allows you to set the behavior of the camera's status LED. To turn the status LED on, set the parameter to Active. To turn the status LED off, set the parameter to Inactive. To turn the status LED off unless an error occurs, set the parameter to ErrorStatus (if available).
DeviceLinkCurrentThroughput Device Link Current Throughput The actual bandwidth currently used for data transmission in bytes per second.
DeviceLinkSelector Device Link Selector Allows you to select the link for data transmission. The parameter is preset to 0. Don't change this parameter.
DeviceLinkSpeed Device Link Speed The net link speed. The unit varies by camera model. On newer cameras, the speed is specified in bits per second.
DeviceLinkThroughputLimit Device Link Throughput Limit Specifies the maximum available bandwidth for data transmission in bytes per second. To enable the limit, set the DeviceLinkThroughputLimitMode parameter to On.
On GigE cameras, the camera automatically adjusts the inter-packet delay to set the bandwidth to the specified limit.
DeviceLinkThroughputLimitMode Device Link Throughput Limit Mode Allows you to limit the maximum available bandwidth for data transmission. On some cameras, this parameter is read-only. If not, set the parameter to On to enable the limit. The maximum bandwidth is limited to the DeviceLinkThroughputLimit parameter value. Note that the actual bandwidth used for data transmission may be lower than the DeviceLinkThroughputLimit parameter value.
DeviceSFNCVersionMajor Device SFNC Version Major The major version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "2" for SFNC 2.3.1.
DeviceSFNCVersionMinor Device SFNC Version Minor The minor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "3" for SFNC 2.3.1.
DeviceSFNCVersionSubMinor Device SFNC Version Sub Minor The subminor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "1" for SFNC 2.3.1.

Specifics#

Show all camera models

Camera Model Additional Device Information Parameters
a2A640-240gmSWIR DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A640-240umSWIR DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1280-80gmSWIR DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1280-125umSWIR DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-51gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-51gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-51gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-51gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-160ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-160ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-160umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-160umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-165g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A1920-165g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2440-98g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2440-98g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-23gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-23gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-23gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-23gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-75ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-75ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-75umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-75umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-105g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-105g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-120cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-120cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-210cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2448-210cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-22gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-22gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-22gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-22gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-60ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-60ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-60umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2590-60umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-20gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-20gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-20gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-20gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-64ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-64ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-64umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2600-64umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-14gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-14gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-14gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-14gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-14gmUV DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-48ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-48ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-48umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-48umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-48umUV DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-67g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-67g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-67g5mUV DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-86cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A2840-86cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-13gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-13gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-13gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-13gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-45ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-45ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-45umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A3840-45umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-9gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-9gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-9gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-9gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-30ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-30ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-30umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-30umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-44g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-44g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-67cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4096-67cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-12gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-12gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-12gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-12gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-40ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-40ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-40umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4200-40umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-5gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-5gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-5gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-5gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-18ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-18ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-18umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-18umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-27g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-27g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-42cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4504-42cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-6gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-6gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-6gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-6gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-20ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-20ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-20umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A4508-20umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-7gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-7gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-7gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-7gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-23ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-23ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-23umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-23umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-34g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-34g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-52cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5320-52cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-4gcBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-4gcPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-4gmBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-4gmPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-15ucBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-15ucPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-15umBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-15umPRO DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-22g5cBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-22g5mBAS DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-35cc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
a2A5328-35cm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
acA640-121gm None
acA640-300gc None
acA640-300gm None
acA640-750uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA640-750um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA720-290gc None
acA720-290gm None
acA720-520uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA720-520um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA800-200gc None
acA800-200gm None
acA800-510uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA800-510um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1280-60gc None
acA1280-60gm None
acA1300-60gc None
acA1300-60gm None
acA1300-60gmNIR None
acA1300-75gc None
acA1300-75gm None
acA1300-200uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1300-200um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1440-73gc None
acA1440-73gm None
acA1440-220uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1440-220um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1600-20gc None
acA1600-20uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1600-60gc None
acA1600-60gm None
acA1920-25gc None
acA1920-25gm None
acA1920-25uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-25um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-40gc None
acA1920-40gm None
acA1920-40uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-40ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-40um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-40umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-48gc None
acA1920-48gm None
acA1920-50gc None
acA1920-50gm None
acA1920-150uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-150um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-155uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-155ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-155um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA1920-155umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2000-50gc None
acA2000-50gm None
acA2000-165uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2000-165um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-25gc None
acA2040-25gm None
acA2040-25gmNIR None
acA2040-35gc None
acA2040-35gm None
acA2040-55uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-55um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-90uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-90um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-90umNIR DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-120uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2040-120um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-20gc None
acA2440-20gm None
acA2440-35uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-35ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-35um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-35umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-75uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-75ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-75um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2440-75umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2500-14gc None
acA2500-14gm None
acA2500-14uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2500-14um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2500-20gc None
acA2500-20gcMED None
acA2500-20gm None
acA2500-20gmMED None
acA2500-60uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA2500-60um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3088-16gc None
acA3088-16gm None
acA3088-57uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3088-57ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3088-57um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3088-57umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3800-10gc None
acA3800-10gm None
acA3800-14uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA3800-14um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4024-8gc None
acA4024-8gm None
acA4024-29uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4024-29um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-11gc None
acA4096-11gm None
acA4096-30uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-30ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-30um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-30umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-40uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-40ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-40um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4096-40umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-8gc None
acA4112-8gm None
acA4112-20uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-20ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-20um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-20umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-30uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-30ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-30um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA4112-30umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA5472-5gc None
acA5472-5gm None
acA5472-17uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA5472-17ucMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA5472-17um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
acA5472-17umMED DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceLinkCurrentThroughput
boA1936-400cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA1936-400cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA2448-250cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA2448-250cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA2832-190cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA2832-190cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4096-93cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4096-93cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4096-180cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4096-180cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4112-68cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4112-68cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4500-45cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4500-45cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4504-100cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA4504-100cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5120-150cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5120-150cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5120-230cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5120-230cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5320-150cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5320-150cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5328-100cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA5328-100cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA6500-36cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA6500-36cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA8100-16cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA8100-16cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA9344-30cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA9344-30cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA9344-70cc DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA9344-70cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
boA13440-17cm DeviceFamilyName
DeviceIndicatorMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA720-520uc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA720-520um DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA1280-54uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1280-54um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1440-220uc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA1440-220um DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA1600-60uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1600-60um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1920-15um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1920-30uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1920-30um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA1920-160uc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA1920-160um DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA2448-70uc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA2448-70um DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA2500-14uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA2500-14um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
DeviceIndicatorMode
daA3840-45uc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
daA3840-45um DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA720-290gc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA720-290gm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA1440-73gc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA1440-73gm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA1920-51gc DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
dmA1920-51gm DeviceFamilyName
DeviceIndicatorMode
DeviceLinkCurrentThroughput
DeviceLinkSpeed
DeviceLinkThroughputLimit
DeviceLinkThroughputLimitMode (read-only)
DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
puA1280-54uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA1280-54um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA1600-60uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA1600-60um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA1920-30uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA1920-30um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA2500-14uc DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit
puA2500-14um DeviceSFNCVersionMajor
DeviceSFNCVersionMinor
DeviceSFNCVersionSubMinor
DeviceLinkSelector
DeviceLinkSpeed
DeviceLinkThroughputLimitMode
DeviceLinkThroughputLimit