Legacy Behavior Control#
If your application is built on a previous firmware and you want to keep using it as it is, the following features allow you to restore the previous behavior:
Info
Changes to the parameters associated with these features are persisted automatically.
Legacy Intensity Scaling#
This controls the default value for the Intensity Scaling feature, which is an internal-only feature. To use the same default value as in firmware versions before 5.x.x, enable the LegacyIntensityScaling parameter.
Legacy Image Inpainting#
This controls whether the Image Inpainting feature is enabled by default. By enabling the LegacyImageInpainting parameter, image inpainting is disabled to simulate the same behavior as in firmware versions before version 5.x.x.
Legacy Illumination Position Correction#
This controls whether the Illumination Position Correction feature is enabled by default. By enabling the LegacyIlluminationPositionCorrection parameter, illumination position correction is disabled to simulate the same behavior as in firmware versions before version 5.x.x.