Device Information Parameters#
This topic describes the parameters and the information each parameter provides.
Using the Feature#
Standard Device Information Parameters#
All Basler cameras mentioned in this documentation provide the following device information parameters:
Parameter Name | Display Name | Description |
---|---|---|
DeviceFirmwareVersion | Device Firmware Version | The camera's firmware version number. |
DeviceManufacturerInfo | Device Manufacturer Info | The camera's manufacturer name. Usually contains an empty string. |
DeviceModelName | Device Model Name | The camera's model name, e.g., acA3800-14um. |
DeviceScanType | Device Scan Type | The scan type of the camera's sensor (Areascan or Linescan ) |
DeviceSerialNumber | Device Serial Number | The camera's serial number. |
DeviceUserID | Device User ID | Used to assign a user-defined name to a camera. The name is displayed in the Basler pylon Viewer and the Basler pylon USB Configurator. The name is also visible in the "friendly name" field of the device information objects returned by pylon's device enumeration procedure. On USB cameras, you must reset the camera using the DeviceReset command for the changes to take effect. |
DeviceVendorName | Device Vendor Name | The camera's vendor name, e.g., Basler. |
DeviceVersion | Device Version | The camera's version number. |
HeightMax | Height Max | The maximum allowed height of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available). |
SensorHeight | Sensor Height | The actual height of the camera's sensor in pixels. |
SensorWidth | Sensor Width | The actual width of the camera's sensor in pixels. |
WidthMax | Width Max | The maximum allowed width of the image ROI in pixels. The value adapts to the current settings for Binning, Decimation, or Scaling (if available). |
Additional Device Information Parameters#
Depending on your camera model, the following additional device information parameters are available:
Parameter Name | Display Name | Description |
---|---|---|
DeviceFamilyName | Device Family Name | The identifier of the product family of the device, e.g., "Basler ace 2" |
DeviceIndicatorMode | Device Indicator Mode | Allows you to set the behavior of the camera's status LED. To turn the status LED on, set the parameter to Active . To turn the status LED off, set the parameter to Inactive . To turn the status LED off unless an error occurs, set the parameter to ErrorStatus (if available). |
DeviceLinkCurrentThroughput | Device Link Current Throughput | The actual bandwidth currently used for data transmission in bytes per second. |
DeviceLinkSelector | Device Link Selector | Allows you to select the link for data transmission. The parameter is preset to 0. Don't change this parameter. |
DeviceLinkSpeed | Device Link Speed | The net link speed in bits per second. |
DeviceLinkThroughputLimit | Device Link Throughput Limit | Specifies the maximum available bandwidth for data transmission in bytes per second. To enable the limit, set the DeviceLinkThroughputLimitMode parameter to On .On GigE cameras, the camera automatically adjusts the inter-packet delay to set the bandwidth to the specified limit. |
DeviceLinkThroughputLimitMode | Device Link Throughput Limit Mode | Allows you to limit the maximum available bandwidth for data transmission. On some cameras, this parameter is read-only. If not, set the parameter to On to enable the limit. The maximum bandwidth is limited to the DeviceLinkThroughputLimit parameter value. Note that the actual bandwidth used for data transmission may be lower than the DeviceLinkThroughputLimit parameter value. |
DeviceSFNCVersionMajor | Device SFNC Version Major | The major version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "2" for SFNC 2.3.1. |
DeviceSFNCVersionMinor | Device SFNC Version Minor | The minor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "3" for SFNC 2.3.1. |
DeviceSFNCVersionSubMinor | Device SFNC Version Sub Minor | The subminor version of the Standard Features Naming Convention (SFNC) that the camera complies with, e.g., "1" for SFNC 2.3.1. |
Specifics#
Camera Model | Additional Device Information Parameters |
---|---|
a2A640-240gmSWIR | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A640-240umSWIR | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1280-80gmSWIR | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1280-125umSWIR | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-51gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-51gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-51gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-51gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-160ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-160ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-160umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-160umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-165g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A1920-165g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2440-98g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2440-98g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-23gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-23gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-23gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-23gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-75ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-75ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-75umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-75umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-105g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2448-105g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-22gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-22gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-22gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-22gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-60ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-60ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-60umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2590-60umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-20gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-20gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-20gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-20gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-64ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-64ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-64umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2600-64umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-14gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-14gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-14gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-14gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-48ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-48ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-48umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-48umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-67g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A2840-67g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-13gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-13gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-13gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-13gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-45ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-45ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-45umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A3840-45umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-9gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-9gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-9gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-9gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-30ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-30ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-30umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-30umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-44g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4096-44g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-12gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-12gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-12gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-12gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-40ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-40ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-40umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4200-40umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-5gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-5gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-5gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-5gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-18ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-18ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-18umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-18umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-27g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4504-27g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-6gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-6gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-6gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-6gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-20ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-20ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-20umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A4508-20umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-7gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-7gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-7gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-7gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-23ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-23ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-23umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-23umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-34g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5320-34g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-4gcBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-4gcPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-4gmBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-4gmPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-15ucBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-15ucPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-15umBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-15umPRO | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-22g5cBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
a2A5328-22g5mBAS | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkSpeed DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode (read-only) DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
acA640-121gm | None |
acA640-300gc | None |
acA640-300gm | None |
acA640-750uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA640-750um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA720-290gc | None |
acA720-290gm | None |
acA720-520uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA720-520um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA800-200gc | None |
acA800-200gm | None |
acA800-510uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA800-510um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1280-60gc | None |
acA1280-60gm | None |
acA1300-60gc | None |
acA1300-60gm | None |
acA1300-60gmNIR | None |
acA1300-75gc | None |
acA1300-75gm | None |
acA1300-200uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1300-200um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1440-73gc | None |
acA1440-73gm | None |
acA1440-220uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1440-220um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1600-20gc | None |
acA1600-20uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1600-60gc | None |
acA1600-60gm | None |
acA1920-25gc | None |
acA1920-25gm | None |
acA1920-25uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-25um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-40gc | None |
acA1920-40gm | None |
acA1920-40uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-40ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-40um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-40umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-48gc | None |
acA1920-48gm | None |
acA1920-50gc | None |
acA1920-50gm | None |
acA1920-150uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-150um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-155uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-155ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-155um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA1920-155umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2000-50gc | None |
acA2000-50gm | None |
acA2000-165uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2000-165um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-25gc | None |
acA2040-25gm | None |
acA2040-25gmNIR | None |
acA2040-35gc | None |
acA2040-35gm | None |
acA2040-55uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-55um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-90uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-90um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-90umNIR | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-120uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2040-120um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-20gc | None |
acA2440-20gm | None |
acA2440-35uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-35ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-35um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-35umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-75uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-75ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-75um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2440-75umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2500-14gc | None |
acA2500-14gm | None |
acA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2500-20gc | None |
acA2500-20gcMED | None |
acA2500-20gm | None |
acA2500-20gmMED | None |
acA2500-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA2500-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3088-16gc | None |
acA3088-16gm | None |
acA3088-57uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3088-57ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3088-57um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3088-57umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3800-10gc | None |
acA3800-10gm | None |
acA3800-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA3800-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4024-8gc | None |
acA4024-8gm | None |
acA4024-29uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4024-29um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-11gc | None |
acA4096-11gm | None |
acA4096-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-30ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-30umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-40uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-40ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-40um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4096-40umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-8gc | None |
acA4112-8gm | None |
acA4112-20uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-20ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-20um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-20umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-30ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA4112-30umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA5472-5gc | None |
acA5472-5gm | None |
acA5472-17uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA5472-17ucMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA5472-17um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
acA5472-17umMED | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceLinkCurrentThroughput |
boA1936-400cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA1936-400cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA2448-250cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA2448-250cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA2832-190cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA2832-190cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4096-93cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4096-93cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4096-180cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4096-180cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4112-68cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4112-68cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4500-45cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4500-45cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4504-100cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA4504-100cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5120-150cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5120-150cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5120-230cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5120-230cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5320-150cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5320-150cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5328-100cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA5328-100cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA6500-36cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA6500-36cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA8100-16cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA8100-16cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA9344-30cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA9344-30cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA9344-70cc | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
boA9344-70cm | DeviceFamilyName DeviceIndicatorMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA720-520uc | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA720-520um | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA1280-54uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1280-54um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1440-220uc | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA1440-220um | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA1600-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1600-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1920-15um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1920-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1920-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA1920-160uc | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA1920-160um | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA2448-70uc | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA2448-70um | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit DeviceIndicatorMode |
daA3840-45uc | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
daA3840-45um | DeviceFamilyName DeviceIndicatorMode DeviceLinkCurrentThroughput DeviceLinkThroughputLimit DeviceLinkThroughputLimitMode DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor |
puA1280-54uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA1280-54um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA1600-60uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA1600-60um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA1920-30uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA1920-30um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA2500-14uc | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |
puA2500-14um | DeviceSFNCVersionMajor DeviceSFNCVersionMinor DeviceSFNCVersionSubMinor DeviceLinkSelector DeviceLinkSpeed DeviceLinkThroughputLimitMode DeviceLinkThroughputLimit |