Skip to content

Brightness and Contrast#

The Brightness and Contrast camera feature allows you to adjust the tonal values of your images.

Brightness and contrast are always processed together as parts of a common mathematical Brightness/Contrast function.

Using the Feature#

Adjusting Contrast and Contrast Mode#

To adjust the contrast:

  1. Set the BslContrastMode parameter to one of the following values (if available):
  2. Enter a value for the BslContrast parameter. The parameter's value range is from -1 to 1. By default, the parameter is set to 0 which means that the contrast remains unchanged.

Adjusting Brightness#

To adjust the brightness, enter a value for the BslBrightness parameter. The parameter's value range is from -1 to 1. By default, the parameter is set to 0 which means that the brightness remains unchanged.

How It Works#

Contrast#

Adjusting the contrast changes the degree of difference between light and dark areas in the image. The more contrast you apply, the more pronounced the difference will be.

How the contrast is applied depends on the contrast mode that you select.

Linear Contrast Mode#

If this contrast mode is selected, the camera uses a linear function to adjust the contrast. Increasing or decreasing the contrast, increases or decreases the gradient of the linear function.

Contrast = 0, Brightness = 0, Linear Contrast Mode

Contrast = 0.3, Brightness = 0, Linear Contrast Mode

With a contrast setting greater than 0, more output pixel values will be set to completely black (0) or completely white (maximum pixel value).

If the contrast is set to 0.3 (see second figure), input values from 0 to approximately 50 are set to completely black, and input values from approximately 205 to 255 are set to completely white. This means that the overall range of tonal values, i.e, the dynamic range of the image, is reduced. The darkest and lightest regions of the image will appear completely black or completely white, but the other areas will appear more defined.

Decreasing the contrast has the opposite effect.

S-Curve Contrast Mode#

If this contrast mode is selected, the camera uses an S-curve function to adjust the contrast.

This allows you to improve the perceived contrast while preserving the dynamic range of the image.

The more you increase the contrast, the more S-shaped the graph of the function will be:

Contrast = 0.3, Brightness = 0, S-Curve Contrast Mode

Contrast = 0.5, Brightness = 0, S-Curve Contrast Mode

The figures above show that increasing the contrast in S-Curve mode has the following effects:

  • The S-curve gets flatter around its starting and end points and steeper around the center. As a result, contrast in light and dark areas of the image is reduced, and contrast in mid tones is increased.
  • Low input pixel values are lowered and high input pixel values are increased. As a result, extreme dark and light areas of your image are compressed, which further improves the perceived contrast.
  • As the curve always starts at (0,0) and ends at (Xmax,Ymax), the dynamic range of the image is preserved.

Contrast settings below 0 in S-Curve mode will result in an inverted S-curve with opposite effects.

Brightness#

Adjusting the brightness allows you to lighten or darken the image by increasing or decreasing its tonal values.

Adjusting the brightness moves the pivot point of the Brightness/Contrast function:

  • Increasing the brightness moves the pivot point towards the upper left. This means that the image will appear lighter.
  • Decreasing the brightness moves the pivot point to the lower right. This means that the image will appear darker.

The figures below show examples with the S-Curve contrast mode selected.

Contrast = 0.3, Brightness = 0, S-Curve Contrast Mode

Contrast = 0.3, Brightness = 0.3, S-Curve Contrast Mode

Additional Parameters#

If available, the BslBrightnessRaw and BslContrastRaw parameters allow you to enter integer values instead of float values for the brightness and contrast parameters. Normally, you don't need to set these parameters.

Specifics#

Show all camera models

Camera Model Available Contrast Modes
a2A640-240gmSWIR Linear
S-Curve
a2A640-240umSWIR Linear
S-Curve
a2A1280-80gmSWIR Linear
S-Curve
a2A1280-125umSWIR Linear
S-Curve
a2A1920-51gcBAS Linear
S-Curve
a2A1920-51gcPRO Linear
S-Curve
a2A1920-51gmBAS Linear
S-Curve
a2A1920-51gmPRO Linear
S-Curve
a2A1920-160ucBAS Linear
S-Curve
a2A1920-160ucPRO Linear
S-Curve
a2A1920-160umBAS Linear
S-Curve
a2A1920-160umPRO Linear
S-Curve
a2A1920-165g5cBAS Linear
S-Curve
a2A1920-165g5mBAS Linear
S-Curve
a2A2048-35gmSWIR Linear
S-Curve
a2A2048-37gcBAS Linear
S-Curve
a2A2048-37gcPRO Linear
S-Curve
a2A2048-37gmBAS Linear
S-Curve
a2A2048-37gmPRO Linear
S-Curve
a2A2048-110umSWIR Linear
S-Curve
a2A2048-114g5cBAS Linear
S-Curve
a2A2048-114g5mBAS Linear
S-Curve
a2A2048-114ucBAS Linear
S-Curve
a2A2048-114ucPRO Linear
S-Curve
a2A2048-114umBAS Linear
S-Curve
a2A2048-114umPRO Linear
S-Curve
a2A2440-98g5cBAS Linear
S-Curve
a2A2440-98g5mBAS Linear
S-Curve
a2A2448-23gcBAS Linear
S-Curve
a2A2448-23gcPRO Linear
S-Curve
a2A2448-23gmBAS Linear
S-Curve
a2A2448-23gmPRO Linear
S-Curve
a2A2448-75ucBAS Linear
S-Curve
a2A2448-75ucPRO Linear
S-Curve
a2A2448-75umBAS Linear
S-Curve
a2A2448-75umPRO Linear
S-Curve
a2A2448-105g5cBAS Linear
S-Curve
a2A2448-105g5mBAS Linear
S-Curve
a2A2448-120cc Linear
S-Curve
a2A2448-120cm Linear
S-Curve
a2A2448-210cc Linear
S-Curve
a2A2448-210cm Linear
S-Curve
a2A2560-20gmSWIR Linear
S-Curve
a2A2560-70umSWIR Linear
S-Curve
a2A2590-22gcBAS Linear
S-Curve
a2A2590-22gcPRO Linear
S-Curve
a2A2590-22gmBAS Linear
S-Curve
a2A2590-22gmPRO Linear
S-Curve
a2A2590-60ucBAS Linear
S-Curve
a2A2590-60ucPRO Linear
S-Curve
a2A2590-60umBAS Linear
S-Curve
a2A2590-60umPRO Linear
S-Curve
a2A2600-20gcBAS Linear
S-Curve
a2A2600-20gcPRO Linear
S-Curve
a2A2600-20gmBAS Linear
S-Curve
a2A2600-20gmPRO Linear
S-Curve
a2A2600-64ucBAS Linear
S-Curve
a2A2600-64ucPRO Linear
S-Curve
a2A2600-64umBAS Linear
S-Curve
a2A2600-64umPRO Linear
S-Curve
a2A2840-14gcBAS Linear
S-Curve
a2A2840-14gcPRO Linear
S-Curve
a2A2840-14gmBAS Linear
S-Curve
a2A2840-14gmPRO Linear
S-Curve
a2A2840-14gmUV Linear
S-Curve
a2A2840-48ucBAS Linear
S-Curve
a2A2840-48ucPRO Linear
S-Curve
a2A2840-48umBAS Linear
S-Curve
a2A2840-48umPRO Linear
S-Curve
a2A2840-48umUV Linear
S-Curve
a2A2840-67g5cBAS Linear
S-Curve
a2A2840-67g5mBAS Linear
S-Curve
a2A2840-67g5mUV Linear
S-Curve
a2A2840-86cc Linear
S-Curve
a2A2840-86cm Linear
S-Curve
a2A3536-9gcBAS Linear
S-Curve
a2A3536-9gcPRO Linear
S-Curve
a2A3536-9gmBAS Linear
S-Curve
a2A3536-9gmPRO Linear
S-Curve
a2A3536-31ucBAS Linear
S-Curve
a2A3536-31ucPRO Linear
S-Curve
a2A3536-31umBAS Linear
S-Curve
a2A3536-31umPRO Linear
S-Curve
a2A3536-42g5cBAS Linear
S-Curve
a2A3536-42g5mBAS Linear
S-Curve
a2A3840-13gcBAS Linear
S-Curve
a2A3840-13gcPRO Linear
S-Curve
a2A3840-13gmBAS Linear
S-Curve
a2A3840-13gmPRO Linear
S-Curve
a2A3840-45ucBAS Linear
S-Curve
a2A3840-45ucPRO Linear
S-Curve
a2A3840-45umBAS Linear
S-Curve
a2A3840-45umPRO Linear
S-Curve
a2A4096-9gcBAS Linear
S-Curve
a2A4096-9gcPRO Linear
S-Curve
a2A4096-9gmBAS Linear
S-Curve
a2A4096-9gmPRO Linear
S-Curve
a2A4096-30ucBAS Linear
S-Curve
a2A4096-30ucPRO Linear
S-Curve
a2A4096-30umBAS Linear
S-Curve
a2A4096-30umPRO Linear
S-Curve
a2A4096-44g5cBAS Linear
S-Curve
a2A4096-44g5mBAS Linear
S-Curve
a2A4096-67cc Linear
S-Curve
a2A4096-67cm Linear
S-Curve
a2A4200-12gcBAS Linear
S-Curve
a2A4200-12gcPRO Linear
S-Curve
a2A4200-12gmBAS Linear
S-Curve
a2A4200-12gmPRO Linear
S-Curve
a2A4200-40ucBAS Linear
S-Curve
a2A4200-40ucPRO Linear
S-Curve
a2A4200-40umBAS Linear
S-Curve
a2A4200-40umPRO Linear
S-Curve
a2A4504-5gcBAS Linear
S-Curve
a2A4504-5gcPRO Linear
S-Curve
a2A4504-5gmBAS Linear
S-Curve
a2A4504-5gmPRO Linear
S-Curve
a2A4504-18ucBAS Linear
S-Curve
a2A4504-18ucPRO Linear
S-Curve
a2A4504-18umBAS Linear
S-Curve
a2A4504-18umPRO Linear
S-Curve
a2A4504-27g5cBAS Linear
S-Curve
a2A4504-27g5mBAS Linear
S-Curve
a2A4504-42cc Linear
S-Curve
a2A4504-42cm Linear
S-Curve
a2A4508-6gcBAS Linear
S-Curve
a2A4508-6gcPRO Linear
S-Curve
a2A4508-6gmBAS Linear
S-Curve
a2A4508-6gmPRO Linear
S-Curve
a2A4508-20ucBAS Linear
S-Curve
a2A4508-20ucPRO Linear
S-Curve
a2A4508-20umBAS Linear
S-Curve
a2A4508-20umPRO Linear
S-Curve
a2A5060-4gcBAS Linear
S-Curve
a2A5060-4gmBAS Linear
S-Curve
a2A5060-15ucBAS Linear
S-Curve
a2A5060-15umBAS Linear
S-Curve
a2A5060-21g5cBAS Linear
S-Curve
a2A5060-21g5mBAS Linear
S-Curve
a2A5320-7gcBAS Linear
S-Curve
a2A5320-7gcPRO Linear
S-Curve
a2A5320-7gmBAS Linear
S-Curve
a2A5320-7gmPRO Linear
S-Curve
a2A5320-23ucBAS Linear
S-Curve
a2A5320-23ucPRO Linear
S-Curve
a2A5320-23umBAS Linear
S-Curve
a2A5320-23umPRO Linear
S-Curve
a2A5320-34g5cBAS Linear
S-Curve
a2A5320-34g5mBAS Linear
S-Curve
a2A5320-52cc Linear
S-Curve
a2A5320-52cm Linear
S-Curve
a2A5328-4gcBAS Linear
S-Curve
a2A5328-4gcPRO Linear
S-Curve
a2A5328-4gmBAS Linear
S-Curve
a2A5328-4gmPRO Linear
S-Curve
a2A5328-15ucBAS Linear
S-Curve
a2A5328-15ucPRO Linear
S-Curve
a2A5328-15umBAS Linear
S-Curve
a2A5328-15umPRO Linear
S-Curve
a2A5328-22g5cBAS Linear
S-Curve
a2A5328-22g5mBAS Linear
S-Curve
a2A5328-35cc Linear
S-Curve
a2A5328-35cm Linear
S-Curve
acA640-121gm Brightness and Contrast feature not supported
acA640-300gc Brightness and Contrast feature not supported
acA640-300gm Brightness and Contrast feature not supported
acA640-750uc Brightness and Contrast feature not supported
acA640-750um Brightness and Contrast feature not supported
acA720-290gc Brightness and Contrast feature not supported
acA720-290gm Brightness and Contrast feature not supported
acA720-520uc Brightness and Contrast feature not supported
acA720-520um Brightness and Contrast feature not supported
acA800-200gc Brightness and Contrast feature not supported
acA800-200gm Brightness and Contrast feature not supported
acA800-510uc Brightness and Contrast feature not supported
acA800-510um Brightness and Contrast feature not supported
acA1280-60gc Brightness and Contrast feature not supported
acA1280-60gm Brightness and Contrast feature not supported
acA1300-60gc Brightness and Contrast feature not supported
acA1300-60gm Brightness and Contrast feature not supported
acA1300-60gmNIR Brightness and Contrast feature not supported
acA1300-75gc Brightness and Contrast feature not supported
acA1300-75gm Brightness and Contrast feature not supported
acA1300-200uc Brightness and Contrast feature not supported
acA1300-200um Brightness and Contrast feature not supported
acA1440-73gc Brightness and Contrast feature not supported
acA1440-73gm Brightness and Contrast feature not supported
acA1440-220uc Brightness and Contrast feature not supported
acA1440-220um Brightness and Contrast feature not supported
acA1600-20gc Brightness and Contrast feature not supported
acA1600-20uc Brightness and Contrast feature not supported
acA1600-60gc Brightness and Contrast feature not supported
acA1600-60gm Brightness and Contrast feature not supported
acA1920-25gc Brightness and Contrast feature not supported
acA1920-25gm Brightness and Contrast feature not supported
acA1920-25uc Brightness and Contrast feature not supported
acA1920-25um Brightness and Contrast feature not supported
acA1920-40gc Brightness and Contrast feature not supported
acA1920-40gm Brightness and Contrast feature not supported
acA1920-40uc Brightness and Contrast feature not supported
acA1920-40ucMED Linear
S-Curve
acA1920-40um Brightness and Contrast feature not supported
acA1920-40umMED Linear
S-Curve
acA1920-48gc Brightness and Contrast feature not supported
acA1920-48gm Brightness and Contrast feature not supported
acA1920-50gc Brightness and Contrast feature not supported
acA1920-50gm Brightness and Contrast feature not supported
acA1920-150uc Brightness and Contrast feature not supported
acA1920-150um Brightness and Contrast feature not supported
acA1920-155uc Brightness and Contrast feature not supported
acA1920-155ucMED Linear
S-Curve
acA1920-155um Brightness and Contrast feature not supported
acA1920-155umMED Linear
S-Curve
acA2000-50gc Brightness and Contrast feature not supported
acA2000-50gm Brightness and Contrast feature not supported
acA2000-165uc Brightness and Contrast feature not supported
acA2000-165um Brightness and Contrast feature not supported
acA2040-25gc Brightness and Contrast feature not supported
acA2040-25gm Brightness and Contrast feature not supported
acA2040-25gmNIR Brightness and Contrast feature not supported
acA2040-35gc Brightness and Contrast feature not supported
acA2040-35gm Brightness and Contrast feature not supported
acA2040-55uc Brightness and Contrast feature not supported
acA2040-55um Brightness and Contrast feature not supported
acA2040-90uc Brightness and Contrast feature not supported
acA2040-90um Brightness and Contrast feature not supported
acA2040-90umNIR Brightness and Contrast feature not supported
acA2040-120uc Brightness and Contrast feature not supported
acA2040-120um Brightness and Contrast feature not supported
acA2440-20gc Brightness and Contrast feature not supported
acA2440-20gm Brightness and Contrast feature not supported
acA2440-35uc Brightness and Contrast feature not supported
acA2440-35ucMED Linear
S-Curve
acA2440-35um Brightness and Contrast feature not supported
acA2440-35umMED Linear
S-Curve
acA2440-75uc Brightness and Contrast feature not supported
acA2440-75ucMED Linear
S-Curve
acA2440-75um Brightness and Contrast feature not supported
acA2440-75umMED Linear
S-Curve
acA2500-14gc Brightness and Contrast feature not supported
acA2500-14gm Brightness and Contrast feature not supported
acA2500-14uc Brightness and Contrast feature not supported
acA2500-14um Brightness and Contrast feature not supported
acA2500-20gc Brightness and Contrast feature not supported
acA2500-20gcMED Linear
S-Curve
acA2500-20gm Brightness and Contrast feature not supported
acA2500-20gmMED Linear
S-Curve
acA2500-60uc Brightness and Contrast feature not supported
acA2500-60um Brightness and Contrast feature not supported
acA3088-16gc Brightness and Contrast feature not supported
acA3088-16gm Brightness and Contrast feature not supported
acA3088-57uc Brightness and Contrast feature not supported
acA3088-57ucMED Linear
S-Curve
acA3088-57um Brightness and Contrast feature not supported
acA3088-57umMED Linear
S-Curve
acA3800-10gc Brightness and Contrast feature not supported
acA3800-10gm Brightness and Contrast feature not supported
acA3800-14uc Brightness and Contrast feature not supported
acA3800-14um Brightness and Contrast feature not supported
acA4024-8gc Brightness and Contrast feature not supported
acA4024-8gm Brightness and Contrast feature not supported
acA4024-29uc Brightness and Contrast feature not supported
acA4024-29um Brightness and Contrast feature not supported
acA4096-11gc Brightness and Contrast feature not supported
acA4096-11gm Brightness and Contrast feature not supported
acA4096-30uc Brightness and Contrast feature not supported
acA4096-30ucMED Linear
S-Curve
acA4096-30um Brightness and Contrast feature not supported
acA4096-30umMED Linear
S-Curve
acA4096-40uc Brightness and Contrast feature not supported
acA4096-40ucMED Linear
S-Curve
acA4096-40um Brightness and Contrast feature not supported
acA4096-40umMED Linear
S-Curve
acA4112-8gc Brightness and Contrast feature not supported
acA4112-8gm Brightness and Contrast feature not supported
acA4112-20uc Brightness and Contrast feature not supported
acA4112-20ucMED Linear
S-Curve
acA4112-20um Brightness and Contrast feature not supported
acA4112-20umMED Linear
S-Curve
acA4112-30uc Brightness and Contrast feature not supported
acA4112-30ucMED Linear
S-Curve
acA4112-30um Brightness and Contrast feature not supported
acA4112-30umMED Linear
S-Curve
acA5472-5gc Brightness and Contrast feature not supported
acA5472-5gm Brightness and Contrast feature not supported
acA5472-17uc Brightness and Contrast feature not supported
acA5472-17ucMED Linear
S-Curve
acA5472-17um Brightness and Contrast feature not supported
acA5472-17umMED Linear
S-Curve
boA1936-400cc Linear
S-Curve
boA1936-400cm Linear
S-Curve
boA2448-250cc Linear
S-Curve
boA2448-250cm Linear
S-Curve
boA2832-190cc Linear
S-Curve
boA2832-190cm Linear
S-Curve
boA4096-93cc Linear
S-Curve
boA4096-93cm Linear
S-Curve
boA4096-180cc Linear
S-Curve
boA4096-180cm Linear
S-Curve
boA4112-68cc Linear
S-Curve
boA4112-68cm Linear
S-Curve
boA4500-45cc Linear
S-Curve
boA4500-45cm Linear
S-Curve
boA4504-100cc Linear
S-Curve
boA4504-100cm Linear
S-Curve
boA5120-150cc Brightness and Contrast feature not supported
boA5120-150cm Brightness and Contrast feature not supported
boA5120-230cc Brightness and Contrast feature not supported
boA5120-230cm Brightness and Contrast feature not supported
boA5320-150cc Linear
S-Curve
boA5320-150cm Linear
S-Curve
boA5328-100cc Linear
S-Curve
boA5328-100cm Linear
S-Curve
boA6500-36cc Linear
S-Curve
boA6500-36cm Linear
S-Curve
boA8100-16cc Linear
S-Curve
boA8100-16cm Linear
S-Curve
boA9344-30cc Brightness and Contrast feature not supported
boA9344-30cm Brightness and Contrast feature not supported
boA9344-70cc Brightness and Contrast feature not supported
boA9344-70cm Brightness and Contrast feature not supported
boA13440-17cm Brightness and Contrast feature not supported
daA720-520uc Linear
S-Curve
daA720-520um Linear
S-Curve
daA1280-54uc Linear
S-Curve
daA1280-54um Linear
S-Curve
daA1440-220uc Linear
S-Curve
daA1440-220um Linear
S-Curve
daA1600-60uc Linear
S-Curve
daA1600-60um Linear
S-Curve
daA1920-15um Linear
S-Curve
daA1920-30uc Linear
S-Curve
daA1920-30um Linear
S-Curve
daA1920-160uc Linear
S-Curve
daA1920-160um Linear
S-Curve
daA2448-70uc Linear
S-Curve
daA2448-70um Linear
S-Curve
daA2500-14uc Linear
S-Curve
daA2500-14um Linear
S-Curve
daA3840-45uc Linear
S-Curve
daA3840-45um Linear
S-Curve
dmA720-290gc Linear
S-Curve
dmA720-290gm Linear
S-Curve
dmA1440-73gc Linear
S-Curve
dmA1440-73gm Linear
S-Curve
dmA1920-51gc Linear
S-Curve
dmA1920-51gm Linear
S-Curve
dmA2448-23gc Linear
S-Curve
dmA2448-23gm Linear
S-Curve
dmA2840-14gc Linear
S-Curve
dmA2840-14gm Linear
S-Curve
dmA3536-9gc Linear
S-Curve
dmA3536-9gm Linear
S-Curve
dmA4096-9gc Linear
S-Curve
dmA4096-9gm Linear
S-Curve
puA1280-54uc Linear
S-Curve
puA1280-54um Linear
S-Curve
puA1600-60uc Linear
S-Curve
puA1600-60um Linear
S-Curve
puA1920-30uc Linear
S-Curve
puA1920-30um Linear
S-Curve
puA2500-14uc Linear
S-Curve
puA2500-14um Linear
S-Curve
r2L2048-29gc Linear
S-Curve
r2L2048-58gm Linear
S-Curve
r2L2048-62cc Linear
S-Curve
r2L2048-62g5c Linear
S-Curve
r2L2048-172cm Linear
S-Curve
r2L2048-172g5m Linear
S-Curve
r2L4096-14gc Linear
S-Curve
r2L4096-29gm Linear
S-Curve
r2L4096-42cc Linear
S-Curve
r2L4096-42g5c Linear
S-Curve
r2L4096-84cm Linear
S-Curve
r2L4096-84g5m Linear
S-Curve
r2L8192-200cm Linear
S-Curve
r2L16384-120cm Linear
S-Curve

Sample Code#

// Set the Brightness parameter to 0.5
camera.BslBrightness.SetValue(0.5);
// Set the contrast mode to Linear
camera.BslContrastMode.SetValue(BslContrastMode_Linear);
// Set the Contrast parameter to 1.2
camera.BslContrast.SetValue(1.2);
INodeMap& nodemap = camera.GetNodeMap();
// Set the Brightness parameter to 0.5
CFloatParameter(nodemap, "BslBrightness").SetValue(0.5);
// Set the contrast mode to Linear
CEnumParameter(nodemap, "BslContrastMode").SetValue("Linear");
// Set the Contrast parameter to 1.2
CFloatParameter(nodemap, "BslContrast").SetValue(1.2);
// Set the Brightness parameter to 0.5
camera.Parameters[PLCamera.BslBrightness].SetValue(0.5);
// Set the contrast mode to Linear
camera.Parameters[PLCamera.BslContrastMode].SetValue(PLCamera.BslContrastMode.Linear);
// Set the Contrast parameter to 1.2
camera.Parameters[PLCamera.BslContrast].SetValue(1.2);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Set the Brightness parameter to 0.5 */
errRes = PylonDeviceSetFloatFeature(hdev, "BslBrightness", 0.5);
CHECK(errRes);
/* Set the contrast mode to Linear */
errRes = PylonDeviceFeatureFromString(hdev, "BslContrastMode", "Linear");
CHECK(errRes);
/* Set the Contrast parameter to 1.2 */
errRes = PylonDeviceSetFloatFeature(hdev, "BslContrast", 1.2);
CHECK(errRes);
# Set the Brightness parameter to 0.5
camera.BslBrightness.Value = 0.5
# Set the contrast mode to Linear
camera.BslContrastMode.Value = "Linear"
# Set the Contrast parameter to 1.2
camera.BslContrast.Value = 1.2

You can also use the pylon Viewer to easily set the parameters.