Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Decimation#

The Decimation camera feature allows you to reduce the number of sensor pixel columns or rows that are transmitted by the camera.

This procedure is also known as "subsampling". It reduces the amount of data to be transferred and may increase the camera's frame rate.

Info

  • When decimation is used (horizontal, vertical, or both), the Scaling feature is not available.
  • When horizontal decimation is used, horizontal binning is not available.
  • When vertical decimation is used, vertical binning is not available.

Using the Feature#

How It Works#

You can choose between horizontal and vertical decimation.

Vertical Decimation#

If you enable vertical decimation, the following applies:

  • On mono cameras, if you specify a vertical decimation factor of n, the camera transmits only every nth row. For example, when you specify a vertical decimation factor of 2, the camera transmits row 1, skips row 2, transmits row 3, and so on:

    Vertical Decimation by 2 on Mono Cameras

  • On color cameras, if you specify a vertical decimation factor of n, the camera transmits only every nth pair of rows. For example, when you specify a vertical decimation factor of 2, the camera transmits rows 1 and 2, skips rows 3 and 4, transmits rows 5 and 6, and so on:

    Vertical Decimation by 2 on Color Cameras

As a result, the image height is reduced. For example, enabling vertical decimation by 2 halves the image height. The camera automatically adjusts the image ROI settings.

Vertical decimation significantly increases the camera's frame rate.

Horizontal Decimation#

If you enable horizontal decimation, the following applies:

  • On mono cameras, if you specify a horizontal decimation factor of n, the camera transmits only every nth column. For example, if specify set a horizontal decimation factor of 2, the camera transmits column 1, skips column 2, transmits column 3, and so on:

    Horizontal Decimation by 2 on Mono Cameras

  • On color cameras, if you specify a horizontal decimation factor of n, the camera transmits only every nth pair of columns. For example, if you specify a horizontal decimation factor of 2, the camera transmits columns 1 and 2, skips columns 3 and 4, transmits columns 5 and 6, and so on:

    Horizontal Decimation by 2 on Color Cameras

As a result, the image width is reduced. For example, enabling horizontal decimation by 2 halves the image width. The camera automatically adjusts the image ROI settings.

Horizontal decimation does not (or only to a very small extent) increase the camera's frame rate.

Configuring Decimation#

To configure decimation:

  1. Make sure the camera is idle, i.e., not capturing images.
  2. Disable binning, if available.
  3. Disable scaling, if available, by setting the scaling factor to 1.
  4. To configure vertical decimation, enter a value for the DecimationVertical parameter.
  5. To configure horizontal decimation, enter a value for the DecimationHorizontal parameter.

The value of the parameters defines the decimation factor. Depending on your camera model, the following values are available:

  • 1: Disables decimation.
  • 2, 3, 4, …: Enables decimation by 2, 3, 4, and so on.

For example, setting DecimationHorizontal to 3 enables horizontal decimation by 3.

Info

If decimation is enabled and you set one or both of the parameters back to 1, the image ROI size may be smaller than the maximum possible size. In this case, you must manually restore the image ROI parameters back to their maximum values.

Considerations When Using Decimation#

Effect on ROI Settings

When you are using decimation, the settings for your image ROIs and auto function ROIs refer to the resulting number of rows and columns.

For example, assume that you are using a camera with a 1280 x 960 sensor. Horizontal decimation by 2 and vertical decimation by 2 are enabled. In this case, the maximum ROI width would be 640 and the maximum ROI height would be 480.

Reduced Resolution

Using decimation effectively reduces the resolution of the camera's image sensor. For example, if you set a camera with a 1280 x 960 sensor to use horizontal decimation by 2 and vertical decimation by 2, the effective resolution of the sensor is reduced to 640 x 480.

Possible Image Distortion

Objects will only appear undistorted in the image if the vertical and horizontal decimation factors are equal. With all other combinations, objects will appear distorted. For example, if you combine vertical decimation by 2 with horizontal decimation by 4, the target objects will appear squashed.

Specifics#

Show all camera models

Camera Model Horizontal Decimation Factors Vertical Decimation Factors
a2A640-240gmSWIR Decimation feature not supported Decimation feature not supported
a2A640-240umSWIR Decimation feature not supported Decimation feature not supported
a2A1280-80gmSWIR Decimation feature not supported Decimation feature not supported
a2A1280-125umSWIR Decimation feature not supported Decimation feature not supported
a2A1920-51gcBAS Decimation feature not supported Decimation feature not supported
a2A1920-51gcIP67 Decimation feature not supported Decimation feature not supported
a2A1920-51gcPRO Decimation feature not supported Decimation feature not supported
a2A1920-51gmBAS Decimation feature not supported Decimation feature not supported
a2A1920-51gmIP67 Decimation feature not supported Decimation feature not supported
a2A1920-51gmPRO Decimation feature not supported Decimation feature not supported
a2A1920-160ucBAS Decimation feature not supported Decimation feature not supported
a2A1920-160ucPRO Decimation feature not supported Decimation feature not supported
a2A1920-160umBAS Decimation feature not supported Decimation feature not supported
a2A1920-160umPRO Decimation feature not supported Decimation feature not supported
a2A1920-165g5cBAS Decimation feature not supported Decimation feature not supported
a2A1920-165g5mBAS Decimation feature not supported Decimation feature not supported
a2A2048-35gmSWIR Decimation feature not supported Decimation feature not supported
a2A2048-37gcBAS Decimation feature not supported Decimation feature not supported
a2A2048-37gcPRO Decimation feature not supported Decimation feature not supported
a2A2048-37gmBAS Decimation feature not supported Decimation feature not supported
a2A2048-37gmPRO Decimation feature not supported Decimation feature not supported
a2A2048-110umSWIR Decimation feature not supported Decimation feature not supported
a2A2048-114g5cBAS Decimation feature not supported Decimation feature not supported
a2A2048-114g5mBAS Decimation feature not supported Decimation feature not supported
a2A2048-114ucBAS Decimation feature not supported Decimation feature not supported
a2A2048-114ucPRO Decimation feature not supported Decimation feature not supported
a2A2048-114umBAS Decimation feature not supported Decimation feature not supported
a2A2048-114umPRO Decimation feature not supported Decimation feature not supported
a2A2048-173cmSWIR Decimation feature not supported Decimation feature not supported
a2A2440-98g5cBAS Decimation feature not supported Decimation feature not supported
a2A2440-98g5mBAS Decimation feature not supported Decimation feature not supported
a2A2448-23gcBAS Decimation feature not supported Decimation feature not supported
a2A2448-23gcIP67 Decimation feature not supported Decimation feature not supported
a2A2448-23gcPRO Decimation feature not supported Decimation feature not supported
a2A2448-23gmBAS Decimation feature not supported Decimation feature not supported
a2A2448-23gmIP67 Decimation feature not supported Decimation feature not supported
a2A2448-23gmPRO Decimation feature not supported Decimation feature not supported
a2A2448-75ucBAS Decimation feature not supported Decimation feature not supported
a2A2448-75ucPRO Decimation feature not supported Decimation feature not supported
a2A2448-75umBAS Decimation feature not supported Decimation feature not supported
a2A2448-75umPRO Decimation feature not supported Decimation feature not supported
a2A2448-105g5cBAS Decimation feature not supported Decimation feature not supported
a2A2448-105g5mBAS Decimation feature not supported Decimation feature not supported
a2A2448-120cc Decimation feature not supported Decimation feature not supported
a2A2448-120cm Decimation feature not supported Decimation feature not supported
a2A2448-210cc Decimation feature not supported Decimation feature not supported
a2A2448-210cm Decimation feature not supported Decimation feature not supported
a2A2560-20gmSWIR Decimation feature not supported Decimation feature not supported
a2A2560-70umSWIR Decimation feature not supported Decimation feature not supported
a2A2560-131cmSWIR Decimation feature not supported Decimation feature not supported
a2A2590-22gcBAS Decimation feature not supported Decimation feature not supported
a2A2590-22gcPRO Decimation feature not supported Decimation feature not supported
a2A2590-22gmBAS Decimation feature not supported Decimation feature not supported
a2A2590-22gmPRO Decimation feature not supported Decimation feature not supported
a2A2590-60ucBAS Decimation feature not supported Decimation feature not supported
a2A2590-60ucPRO Decimation feature not supported Decimation feature not supported
a2A2590-60umBAS Decimation feature not supported Decimation feature not supported
a2A2590-60umPRO Decimation feature not supported Decimation feature not supported
a2A2600-20gcBAS Decimation feature not supported Decimation feature not supported
a2A2600-20gcPRO Decimation feature not supported Decimation feature not supported
a2A2600-20gmBAS Decimation feature not supported Decimation feature not supported
a2A2600-20gmPRO Decimation feature not supported Decimation feature not supported
a2A2600-64ucBAS Decimation feature not supported Decimation feature not supported
a2A2600-64ucPRO Decimation feature not supported Decimation feature not supported
a2A2600-64umBAS Decimation feature not supported Decimation feature not supported
a2A2600-64umPRO Decimation feature not supported Decimation feature not supported
a2A2840-14gcBAS Decimation feature not supported Decimation feature not supported
a2A2840-14gcIP67 Decimation feature not supported Decimation feature not supported
a2A2840-14gcPRO Decimation feature not supported Decimation feature not supported
a2A2840-14gmBAS Decimation feature not supported Decimation feature not supported
a2A2840-14gmIP67 Decimation feature not supported Decimation feature not supported
a2A2840-14gmPRO Decimation feature not supported Decimation feature not supported
a2A2840-14gmUV Decimation feature not supported Decimation feature not supported
a2A2840-48ucBAS Decimation feature not supported Decimation feature not supported
a2A2840-48ucPRO Decimation feature not supported Decimation feature not supported
a2A2840-48umBAS Decimation feature not supported Decimation feature not supported
a2A2840-48umPRO Decimation feature not supported Decimation feature not supported
a2A2840-48umUV Decimation feature not supported Decimation feature not supported
a2A2840-67g5cBAS Decimation feature not supported Decimation feature not supported
a2A2840-67g5mBAS Decimation feature not supported Decimation feature not supported
a2A2840-67g5mUV Decimation feature not supported Decimation feature not supported
a2A2840-86cc Decimation feature not supported Decimation feature not supported
a2A2840-86cm Decimation feature not supported Decimation feature not supported
a2A3536-9gcBAS Decimation feature not supported Decimation feature not supported
a2A3536-9gcPRO Decimation feature not supported Decimation feature not supported
a2A3536-9gmBAS Decimation feature not supported Decimation feature not supported
a2A3536-9gmPRO Decimation feature not supported Decimation feature not supported
a2A3536-31ucBAS Decimation feature not supported Decimation feature not supported
a2A3536-31ucPRO Decimation feature not supported Decimation feature not supported
a2A3536-31umBAS Decimation feature not supported Decimation feature not supported
a2A3536-31umPRO Decimation feature not supported Decimation feature not supported
a2A3536-42g5cBAS Decimation feature not supported Decimation feature not supported
a2A3536-42g5mBAS Decimation feature not supported Decimation feature not supported
a2A3840-13gcBAS Decimation feature not supported Decimation feature not supported
a2A3840-13gcPRO Decimation feature not supported Decimation feature not supported
a2A3840-13gmBAS Decimation feature not supported Decimation feature not supported
a2A3840-13gmPRO Decimation feature not supported Decimation feature not supported
a2A3840-45ucBAS Decimation feature not supported Decimation feature not supported
a2A3840-45ucPRO Decimation feature not supported Decimation feature not supported
a2A3840-45umBAS Decimation feature not supported Decimation feature not supported
a2A3840-45umPRO Decimation feature not supported Decimation feature not supported
a2A4096-9gcBAS Decimation feature not supported Decimation feature not supported
a2A4096-9gcIP67 Decimation feature not supported Decimation feature not supported
a2A4096-9gcPRO Decimation feature not supported Decimation feature not supported
a2A4096-9gmBAS Decimation feature not supported Decimation feature not supported
a2A4096-9gmIP67 Decimation feature not supported Decimation feature not supported
a2A4096-9gmPRO Decimation feature not supported Decimation feature not supported
a2A4096-30ucBAS Decimation feature not supported Decimation feature not supported
a2A4096-30ucPRO Decimation feature not supported Decimation feature not supported
a2A4096-30umBAS Decimation feature not supported Decimation feature not supported
a2A4096-30umPRO Decimation feature not supported Decimation feature not supported
a2A4096-44g5cBAS Decimation feature not supported Decimation feature not supported
a2A4096-44g5mBAS Decimation feature not supported Decimation feature not supported
a2A4096-67cc Decimation feature not supported Decimation feature not supported
a2A4096-67cm Decimation feature not supported Decimation feature not supported
a2A4200-12gcBAS Decimation feature not supported Decimation feature not supported
a2A4200-12gcPRO Decimation feature not supported Decimation feature not supported
a2A4200-12gmBAS Decimation feature not supported Decimation feature not supported
a2A4200-12gmPRO Decimation feature not supported Decimation feature not supported
a2A4200-40ucBAS Decimation feature not supported Decimation feature not supported
a2A4200-40ucPRO Decimation feature not supported Decimation feature not supported
a2A4200-40umBAS Decimation feature not supported Decimation feature not supported
a2A4200-40umPRO Decimation feature not supported Decimation feature not supported
a2A4504-5gcBAS Decimation feature not supported Decimation feature not supported
a2A4504-5gcIP67 Decimation feature not supported Decimation feature not supported
a2A4504-5gcPRO Decimation feature not supported Decimation feature not supported
a2A4504-5gmBAS Decimation feature not supported Decimation feature not supported
a2A4504-5gmIP67 Decimation feature not supported Decimation feature not supported
a2A4504-5gmPRO Decimation feature not supported Decimation feature not supported
a2A4504-18ucBAS Decimation feature not supported Decimation feature not supported
a2A4504-18ucPRO Decimation feature not supported Decimation feature not supported
a2A4504-18umBAS Decimation feature not supported Decimation feature not supported
a2A4504-18umPRO Decimation feature not supported Decimation feature not supported
a2A4504-27g5cBAS Decimation feature not supported Decimation feature not supported
a2A4504-27g5mBAS Decimation feature not supported Decimation feature not supported
a2A4504-42cc Decimation feature not supported Decimation feature not supported
a2A4504-42cm Decimation feature not supported Decimation feature not supported
a2A4508-6gcBAS Decimation feature not supported Decimation feature not supported
a2A4508-6gcPRO Decimation feature not supported Decimation feature not supported
a2A4508-6gmBAS Decimation feature not supported Decimation feature not supported
a2A4508-6gmPRO Decimation feature not supported Decimation feature not supported
a2A4508-20ucBAS Decimation feature not supported Decimation feature not supported
a2A4508-20ucPRO Decimation feature not supported Decimation feature not supported
a2A4508-20umBAS Decimation feature not supported Decimation feature not supported
a2A4508-20umPRO Decimation feature not supported Decimation feature not supported
a2A5060-4gcBAS Decimation feature not supported Decimation feature not supported
a2A5060-4gmBAS Decimation feature not supported Decimation feature not supported
a2A5060-15ucBAS Decimation feature not supported Decimation feature not supported
a2A5060-15umBAS Decimation feature not supported Decimation feature not supported
a2A5060-21g5cBAS Decimation feature not supported Decimation feature not supported
a2A5060-21g5mBAS Decimation feature not supported Decimation feature not supported
a2A5060-35cc Decimation feature not supported Decimation feature not supported
a2A5060-35cm Decimation feature not supported Decimation feature not supported
a2A5320-7gcBAS Decimation feature not supported Decimation feature not supported
a2A5320-7gcIP67 Decimation feature not supported Decimation feature not supported
a2A5320-7gcPRO Decimation feature not supported Decimation feature not supported
a2A5320-7gmBAS Decimation feature not supported Decimation feature not supported
a2A5320-7gmPRO Decimation feature not supported Decimation feature not supported
a2A5320-7gmip67 Decimation feature not supported Decimation feature not supported
a2A5320-23ucBAS Decimation feature not supported Decimation feature not supported
a2A5320-23ucPRO Decimation feature not supported Decimation feature not supported
a2A5320-23umBAS Decimation feature not supported Decimation feature not supported
a2A5320-23umPRO Decimation feature not supported Decimation feature not supported
a2A5320-34g5cBAS Decimation feature not supported Decimation feature not supported
a2A5320-34g5mBAS Decimation feature not supported Decimation feature not supported
a2A5320-52cc Decimation feature not supported Decimation feature not supported
a2A5320-52cm Decimation feature not supported Decimation feature not supported
a2A5328-4gcBAS Decimation feature not supported Decimation feature not supported
a2A5328-4gcIP67 Decimation feature not supported Decimation feature not supported
a2A5328-4gcPRO Decimation feature not supported Decimation feature not supported
a2A5328-4gmBAS Decimation feature not supported Decimation feature not supported
a2A5328-4gmIP67 Decimation feature not supported Decimation feature not supported
a2A5328-4gmPRO Decimation feature not supported Decimation feature not supported
a2A5328-15ucBAS Decimation feature not supported Decimation feature not supported
a2A5328-15ucPRO Decimation feature not supported Decimation feature not supported
a2A5328-15umBAS Decimation feature not supported Decimation feature not supported
a2A5328-15umPRO Decimation feature not supported Decimation feature not supported
a2A5328-22g5cBAS Decimation feature not supported Decimation feature not supported
a2A5328-22g5mBAS Decimation feature not supported Decimation feature not supported
a2A5328-35cc Decimation feature not supported Decimation feature not supported
a2A5328-35cm Decimation feature not supported Decimation feature not supported
acA640-121gm Decimation feature not supported Decimation feature not supported
acA640-300gc Decimation feature not supported Decimation feature not supported
acA640-300gm Decimation feature not supported Decimation feature not supported
acA640-750uc Decimation feature not supported Decimation feature not supported
acA640-750um Decimation feature not supported Decimation feature not supported
acA720-290gc Decimation feature not supported Decimation feature not supported
acA720-290gm Decimation feature not supported Decimation feature not supported
acA720-520uc Decimation feature not supported Decimation feature not supported
acA720-520um Decimation feature not supported Decimation feature not supported
acA800-200gc Decimation feature not supported Decimation feature not supported
acA800-200gm Decimation feature not supported Decimation feature not supported
acA800-510uc Decimation feature not supported Decimation feature not supported
acA800-510um Decimation feature not supported Decimation feature not supported
acA1280-60gc 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1280-60gm 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1300-60gc 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1300-60gm 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1300-60gmNIR 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1300-75gc Decimation feature not supported Decimation feature not supported
acA1300-75gm Decimation feature not supported Decimation feature not supported
acA1300-200uc Decimation feature not supported Decimation feature not supported
acA1300-200um Decimation feature not supported Decimation feature not supported
acA1440-73gc Decimation feature not supported Decimation feature not supported
acA1440-73gm Decimation feature not supported Decimation feature not supported
acA1440-220uc Decimation feature not supported Decimation feature not supported
acA1440-220um Decimation feature not supported Decimation feature not supported
acA1600-20gc Decimation feature not supported Decimation feature not supported
acA1600-20uc Decimation feature not supported Decimation feature not supported
acA1600-60gc 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1600-60gm 1, 2, 3, …, 32 1, 2, 3, …, 32
acA1920-25gc Decimation feature not supported Decimation feature not supported
acA1920-25gm Decimation feature not supported Decimation feature not supported
acA1920-25uc Decimation feature not supported Decimation feature not supported
acA1920-25um Decimation feature not supported Decimation feature not supported
acA1920-40gc Decimation feature not supported Decimation feature not supported
acA1920-40gm Decimation feature not supported Decimation feature not supported
acA1920-40uc Decimation feature not supported Decimation feature not supported
acA1920-40ucMED Decimation feature not supported Decimation feature not supported
acA1920-40um Decimation feature not supported Decimation feature not supported
acA1920-40umMED Decimation feature not supported Decimation feature not supported
acA1920-48gc Decimation feature not supported Decimation feature not supported
acA1920-48gm Decimation feature not supported Decimation feature not supported
acA1920-50gc Decimation feature not supported Decimation feature not supported
acA1920-50gm Decimation feature not supported Decimation feature not supported
acA1920-150uc Decimation feature not supported Decimation feature not supported
acA1920-150um Decimation feature not supported Decimation feature not supported
acA1920-155uc Decimation feature not supported Decimation feature not supported
acA1920-155ucMED Decimation feature not supported Decimation feature not supported
acA1920-155um Decimation feature not supported Decimation feature not supported
acA1920-155umMED Decimation feature not supported Decimation feature not supported
acA2000-50gc Not supported 1, 2, 3, …, 542
acA2000-50gm Not supported 1, 2, 3, …, 1087
acA2000-165uc Decimation feature not supported Decimation feature not supported
acA2000-165um Decimation feature not supported Decimation feature not supported
acA2040-25gc Not supported 1, 2, 3, …, 1022
acA2040-25gm Not supported 1, 2, 3, …, 2047
acA2040-25gmNIR Not supported 1, 2, 3, …, 2047
acA2040-35gc Decimation feature not supported Decimation feature not supported
acA2040-35gm Decimation feature not supported Decimation feature not supported
acA2040-55uc Decimation feature not supported Decimation feature not supported
acA2040-55um Decimation feature not supported Decimation feature not supported
acA2040-90uc Decimation feature not supported Decimation feature not supported
acA2040-90um Decimation feature not supported Decimation feature not supported
acA2040-90umNIR Decimation feature not supported Decimation feature not supported
acA2040-120uc Decimation feature not supported Decimation feature not supported
acA2040-120um Decimation feature not supported Decimation feature not supported
acA2440-20gc Decimation feature not supported Decimation feature not supported
acA2440-20gm Decimation feature not supported Decimation feature not supported
acA2440-35uc Decimation feature not supported Decimation feature not supported
acA2440-35ucMED Decimation feature not supported Decimation feature not supported
acA2440-35um Decimation feature not supported Decimation feature not supported
acA2440-35umMED Decimation feature not supported Decimation feature not supported
acA2440-75uc Decimation feature not supported Decimation feature not supported
acA2440-75ucMED Decimation feature not supported Decimation feature not supported
acA2440-75um Decimation feature not supported Decimation feature not supported
acA2440-75umMED Decimation feature not supported Decimation feature not supported
acA2500-14gc Decimation feature not supported Decimation feature not supported
acA2500-14gm Decimation feature not supported Decimation feature not supported
acA2500-14uc Decimation feature not supported Decimation feature not supported
acA2500-14um Decimation feature not supported Decimation feature not supported
acA2500-20gc Decimation feature not supported Decimation feature not supported
acA2500-20gcMED Decimation feature not supported Decimation feature not supported
acA2500-20gm Decimation feature not supported Decimation feature not supported
acA2500-20gmMED Decimation feature not supported Decimation feature not supported
acA2500-60uc Decimation feature not supported Decimation feature not supported
acA2500-60um Decimation feature not supported Decimation feature not supported
acA3088-16gc Decimation feature not supported Decimation feature not supported
acA3088-16gm Decimation feature not supported Decimation feature not supported
acA3088-57uc Decimation feature not supported Decimation feature not supported
acA3088-57ucMED Decimation feature not supported Decimation feature not supported
acA3088-57um Decimation feature not supported Decimation feature not supported
acA3088-57umMED Decimation feature not supported Decimation feature not supported
acA3800-10gc 1, 2, 4 1, 2, 4
acA3800-10gm 1, 2, 4 1, 2, 4
acA3800-14uc 1, 2, 4 1, 2, 4
acA3800-14um 1, 2, 4 1, 2, 4
acA4024-8gc Decimation feature not supported Decimation feature not supported
acA4024-8gm Decimation feature not supported Decimation feature not supported
acA4024-29uc Decimation feature not supported Decimation feature not supported
acA4024-29um Decimation feature not supported Decimation feature not supported
acA4096-11gc Decimation feature not supported Decimation feature not supported
acA4096-11gm Decimation feature not supported Decimation feature not supported
acA4096-30uc Decimation feature not supported Decimation feature not supported
acA4096-30ucMED Decimation feature not supported Decimation feature not supported
acA4096-30um Decimation feature not supported Decimation feature not supported
acA4096-30umMED Decimation feature not supported Decimation feature not supported
acA4096-40uc Decimation feature not supported Decimation feature not supported
acA4096-40ucMED Decimation feature not supported Decimation feature not supported
acA4096-40um Decimation feature not supported Decimation feature not supported
acA4096-40umMED Decimation feature not supported Decimation feature not supported
acA4112-8gc Decimation feature not supported Decimation feature not supported
acA4112-8gm Decimation feature not supported Decimation feature not supported
acA4112-20uc Decimation feature not supported Decimation feature not supported
acA4112-20ucMED Decimation feature not supported Decimation feature not supported
acA4112-20um Decimation feature not supported Decimation feature not supported
acA4112-20umMED Decimation feature not supported Decimation feature not supported
acA4112-30uc Decimation feature not supported Decimation feature not supported
acA4112-30ucMED Decimation feature not supported Decimation feature not supported
acA4112-30um Decimation feature not supported Decimation feature not supported
acA4112-30umMED Decimation feature not supported Decimation feature not supported
acA5472-5gc Decimation feature not supported Decimation feature not supported
acA5472-5gm Decimation feature not supported Decimation feature not supported
acA5472-17uc Decimation feature not supported Decimation feature not supported
acA5472-17ucMED Decimation feature not supported Decimation feature not supported
acA5472-17um Decimation feature not supported Decimation feature not supported
acA5472-17umMED Decimation feature not supported Decimation feature not supported
boA1936-400cc Decimation feature not supported Decimation feature not supported
boA1936-400cm Decimation feature not supported Decimation feature not supported
boA2448-250cc Decimation feature not supported Decimation feature not supported
boA2448-250cm Decimation feature not supported Decimation feature not supported
boA2832-190cc Decimation feature not supported Decimation feature not supported
boA2832-190cm Decimation feature not supported Decimation feature not supported
boA4096-93cc Decimation feature not supported Decimation feature not supported
boA4096-93cm Decimation feature not supported Decimation feature not supported
boA4096-180cc Decimation feature not supported Decimation feature not supported
boA4096-180cm Decimation feature not supported Decimation feature not supported
boA4112-68cc Decimation feature not supported Decimation feature not supported
boA4112-68cm Decimation feature not supported Decimation feature not supported
boA4500-45cc Decimation feature not supported Decimation feature not supported
boA4500-45cm Decimation feature not supported Decimation feature not supported
boA4504-100cc Decimation feature not supported Decimation feature not supported
boA4504-100cm Decimation feature not supported Decimation feature not supported
boA5120-150cc Decimation feature not supported Decimation feature not supported
boA5120-150cm 1, 2 1, 2
boA5120-230cc Decimation feature not supported Decimation feature not supported
boA5120-230cm Decimation feature not supported Decimation feature not supported
boA5320-150cc Decimation feature not supported Decimation feature not supported
boA5320-150cm Decimation feature not supported Decimation feature not supported
boA5328-100cc Decimation feature not supported Decimation feature not supported
boA5328-100cm Decimation feature not supported Decimation feature not supported
boA6500-36cc Decimation feature not supported Decimation feature not supported
boA6500-36cm Decimation feature not supported Decimation feature not supported
boA8100-16cc Decimation feature not supported Decimation feature not supported
boA8100-16cm Decimation feature not supported Decimation feature not supported
boA9344-30cc Decimation feature not supported Decimation feature not supported
boA9344-30cm 1, 2 1, 2
boA9344-70cc Decimation feature not supported Decimation feature not supported
boA9344-70cm 1, 2 1, 2
boA13440-17cm Decimation feature not supported Decimation feature not supported
daA720-520uc Decimation feature not supported Decimation feature not supported
daA720-520um Decimation feature not supported Decimation feature not supported
daA1280-54uc Decimation feature not supported Decimation feature not supported
daA1280-54um Decimation feature not supported Decimation feature not supported
daA1440-220uc Decimation feature not supported Decimation feature not supported
daA1440-220um Decimation feature not supported Decimation feature not supported
daA1600-60uc Decimation feature not supported Decimation feature not supported
daA1600-60um Decimation feature not supported Decimation feature not supported
daA1920-15um Decimation feature not supported Decimation feature not supported
daA1920-30uc Decimation feature not supported Decimation feature not supported
daA1920-30um Decimation feature not supported Decimation feature not supported
daA1920-160uc Decimation feature not supported Decimation feature not supported
daA1920-160um Decimation feature not supported Decimation feature not supported
daA2448-70uc Decimation feature not supported Decimation feature not supported
daA2448-70um Decimation feature not supported Decimation feature not supported
daA2500-14uc Decimation feature not supported Decimation feature not supported
daA2500-14um Decimation feature not supported Decimation feature not supported
daA3840-45uc Decimation feature not supported Decimation feature not supported
daA3840-45um Decimation feature not supported Decimation feature not supported
dmA720-290gc Decimation feature not supported Decimation feature not supported
dmA720-290gm Decimation feature not supported Decimation feature not supported
dmA1440-73gc Decimation feature not supported Decimation feature not supported
dmA1440-73gm Decimation feature not supported Decimation feature not supported
dmA1920-51gc Decimation feature not supported Decimation feature not supported
dmA1920-51gm Decimation feature not supported Decimation feature not supported
dmA2048-37gc Decimation feature not supported Decimation feature not supported
dmA2048-37gm Decimation feature not supported Decimation feature not supported
dmA2448-23gc Decimation feature not supported Decimation feature not supported
dmA2448-23gm Decimation feature not supported Decimation feature not supported
dmA2840-14gc Decimation feature not supported Decimation feature not supported
dmA2840-14gm Decimation feature not supported Decimation feature not supported
dmA3536-9gc Decimation feature not supported Decimation feature not supported
dmA3536-9gm Decimation feature not supported Decimation feature not supported
dmA4096-9gc Decimation feature not supported Decimation feature not supported
dmA4096-9gm Decimation feature not supported Decimation feature not supported
puA1280-54uc Decimation feature not supported Decimation feature not supported
puA1280-54um Decimation feature not supported Decimation feature not supported
puA1600-60uc Decimation feature not supported Decimation feature not supported
puA1600-60um Decimation feature not supported Decimation feature not supported
puA1920-30uc Decimation feature not supported Decimation feature not supported
puA1920-30um Decimation feature not supported Decimation feature not supported
puA2500-14uc Decimation feature not supported Decimation feature not supported
puA2500-14um Decimation feature not supported Decimation feature not supported
r2L2048-29gc Decimation feature not supported Decimation feature not supported
r2L2048-58gm Decimation feature not supported Decimation feature not supported
r2L2048-62cc Decimation feature not supported Decimation feature not supported
r2L2048-62g5c Decimation feature not supported Decimation feature not supported
r2L2048-172cm Decimation feature not supported Decimation feature not supported
r2L2048-172g5m Decimation feature not supported Decimation feature not supported
r2L4096-14gc Decimation feature not supported Decimation feature not supported
r2L4096-29gm Decimation feature not supported Decimation feature not supported
r2L4096-42cc Decimation feature not supported Decimation feature not supported
r2L4096-42g5c Decimation feature not supported Decimation feature not supported
r2L4096-84cm Decimation feature not supported Decimation feature not supported
r2L4096-84g5m Decimation feature not supported Decimation feature not supported
r2L8192-80cc Decimation feature not supported Decimation feature not supported
r2L8192-240cm Decimation feature not supported Decimation feature not supported
r2L16384-60cc Decimation feature not supported Decimation feature not supported
r2L16384-120cm Decimation feature not supported Decimation feature not supported

Sample Code#

// Enable horizontal decimation by 2
camera.DecimationHorizontal.SetValue(2);
// Enable vertical decimation by 2
camera.DecimationVertical.SetValue(2);
// Disable horizontal decimation
camera.DecimationHorizontal.SetValue(1);
// Disable vertical decimation
camera.DecimationVertical.SetValue(1);
INodeMap& nodemap = camera.GetNodeMap();
// Enable horizontal decimation by 2
CIntegerParameter(nodemap, "DecimationHorizontal").SetValue(2);
// Enable vertical decimation by 2
CIntegerParameter(nodemap, "DecimationVertical").SetValue(2);
// Disable horizontal decimation
CIntegerParameter(nodemap, "DecimationHorizontal").SetValue(1);
// Disable vertical decimation
CIntegerParameter(nodemap, "DecimationVertical").SetValue(1);
// Enable horizontal decimation by 2
camera.Parameters[PLCamera.DecimationHorizontal].SetValue(2);
// Enable vertical decimation by 2
camera.Parameters[PLCamera.DecimationVertical].SetValue(2);
// Disable horizontal decimation
camera.Parameters[PLCamera.DecimationHorizontal].SetValue(1);
// Disable vertical decimation
camera.Parameters[PLCamera.DecimationVertical].SetValue(1);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Enable horizontal decimation by 2 */
errRes = PylonDeviceSetIntegerFeature(hdev, "DecimationHorizontal", 2);
CHECK(errRes);
/* Enable vertical decimation by 2 */
errRes = PylonDeviceSetIntegerFeature(hdev, "DecimationVertical", 2);
CHECK(errRes);
/* Disable horizontal decimation */
errRes = PylonDeviceSetIntegerFeature(hdev, "DecimationHorizontal", 1);
CHECK(errRes);
/* Disable vertical decimation */
errRes = PylonDeviceSetIntegerFeature(hdev, "DecimationVertical", 1);
CHECK(errRes);
# Enable horizontal decimation by 2
camera.DecimationHorizontal.Value = 2
# Enable vertical decimation by 2
camera.DecimationVertical.Value = 2
# Disable horizontal decimation
camera.DecimationHorizontal.Value = 1
# Disable vertical decimation
camera.DecimationVertical.Value = 1

You can also use the pylon Viewer to easily set the parameters.