Exposure Time#
To automatically set the exposure time, use the Exposure Auto feature.
Using the Feature#
Setting the Exposure Time#
To set the exposure time:
- Set the
ExposureMode
parameter toTimed
. - If available, set the
ExposureAuto
parameter toOff
. -
The next steps depend on your camera model:
-
To set the Exposure Time parameter for the whole image:
- Make sure that the
ExposureTimeMode
parameter is set toCommon
. - Set the
ExposureTime
parameter to the desired exposure time in microseconds.
- Make sure that the
-
To set different exposure times for different stages (e.g., image lines):
- Set the
ExposureTimeMode
toIndividual
. - Select the desired stage via the
ExposureTimeSelector
parameter. - Set the
ExposureTime
parameter for the selected stage to the desired exposure time in microseconds. - Repeat steps 2 and 3 for the other stages you want to specify.
- Set the
-
The minimum and maximum exposure time vary by camera model.
Determining the Exposure Time#
To determine the current exposure time in microseconds:
- On ace 2 R/V/X, boost R, and dart R/M cameras, get the value of the
BslEffectiveExposureTime
parameter. This parameter is read-only. It takes factors like internal offsets or clock speed requirements into account that may cause the exposure time to differ from the exposure time set. - On other cameras, get the value of the
ExposureTime
parameter. Note that depending on the sensor type and its specific characteristics, this value may differ slightly from the effective exposure time.
Determining the exposure time can be useful, for example, if the Exposure Auto
auto function is enabled and you want to retrieve the automatically adjusted exposure time.
Exposure Time Mode#
On some camera models, the ExposureTimeMode
parameter is available. It allows you to choose between exposure time modes that provide different exposure time ranges. Depending on your camera model, you can also set individual exposure times for different regions on the sensor, e.g., for two sensor lines or for red and green pixels.
You can set the ExposureTimeMode
parameter to one of the following values:
Common
orStandard
: Enables the Common or Standard exposure time mode. This is the default setting.Individual
: Allows you to specify different exposure times for individual regions (Stage 1, Stage 2) on the image sensor. This can be useful, if you want to define different exposure times, e.g., for two sensor lines.Short
: Allows you to set a short exposure time within the value range available.UltraShort
: Allows you to set an ultra short exposure time within the value range available.
Info
- Depending on the exposure time mode, the exposure start delay changes.
- If the Short or Ultra Short exposure time mode is enabled, the Sequencer feature is not available.
- If the exposure time mode is set to
Individual
, the GainAuto and ExposureAuto features are disabled.
Exposure Time Selector#
On some camera models, the ExposureTimeSelector
parameter is available. It allows you to expose either the entire image sensor for the exposure time specified or individual regions (Stage 1, Stage 2)on the image sensor.
You can set the ExposureTimeSelector
parameter to one of the following values:
Common
: The entire image sensor is exposed for the exposure time specified.Stage 1
: Stage 1 is exposed for the exposure time specified. Stage 1 is a predefined region on the image sensor.Stage 2
: Stage 2 is exposed for the exposure time specified. Stage 2 is a predefined region on the image sensor.
Specifics#
Info
On some camera models, you can use the Remove Parameter Limits feature to increase the exposure time parameter limits.
Camera Model | Minimum Exposure Time [µs] | Maximum Exposure Time [µs] | Available Exposure Time Modes |
---|---|---|---|
a2A640-240gmSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A640-240umSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A1280-80gmSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A1280-125umSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A1920-51gcBAS | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-51gcPRO | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-51gmBAS | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-51gmPRO | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-160ucBAS | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-160ucPRO | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-160umBAS | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-160umPRO | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-165g5cBAS | Standard exposure time mode: 21 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A1920-165g5mBAS | Standard exposure time mode: 21 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
a2A2048-35gmSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A2048-110umSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A2440-98g5cBAS | 20 | 10000000 | ExposureTimeMode parameter not available |
a2A2440-98g5mBAS | 20 | 10000000 | ExposureTimeMode parameter not available |
a2A2448-23gcBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-23gcPRO | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-23gmBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-23gmPRO | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-75ucBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-75ucPRO | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-75umBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-75umPRO | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-105g5cBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-105g5mBAS | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-120cc | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-120cm | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-210cc | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2448-210cm | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A2560-20gmSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A2560-70umSWIR | Standard exposure time mode: 16 Ultra Short exposure time mode: 2 | Standard exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Standard Ultra Short |
a2A2590-22gcBAS | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-22gcPRO | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-22gmBAS | 10 | 999999 | Standard Ultra Short |
a2A2590-22gmPRO | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-60ucBAS | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-60ucPRO | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-60umBAS | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2590-60umPRO | 10 | 999999 | ExposureTimeMode parameter not available |
a2A2600-20gcBAS | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A2600-20gcPRO | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A2600-20gmBAS | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A2600-20gmPRO | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A2600-64ucBAS | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A2600-64ucPRO | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A2600-64umBAS | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A2600-64umPRO | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A2840-14gcBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-14gcPRO | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-14gmBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-14gmPRO | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-14gmUV | 9 | 10000000 | ExposureTimeMode parameter not available |
a2A2840-48ucBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-48ucPRO | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-48umBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-48umPRO | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-48umUV | 9 | 10000000 | ExposureTimeMode parameter not available |
a2A2840-67g5cBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-67g5mBAS | 10/12i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-67g5mUV | 8 | 10000000 | ExposureTimeMode parameter not available |
a2A2840-86cc | 8/9i | 10000000 | ExposureTimeMode parameter not available |
a2A2840-86cm | 8/9i | 10000000 | ExposureTimeMode parameter not available |
a2A3840-13gcBAS | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-13gcPRO | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-13gmBAS | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-13gmPRO | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-45ucBAS | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-45ucPRO | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-45umBAS | 12 | 999999 | ExposureTimeMode parameter not available |
a2A3840-45umPRO | 12 | 999999 | ExposureTimeMode parameter not available |
a2A4096-9gcBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-9gcPRO | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-9gmBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-9gmPRO | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-30ucBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-30ucPRO | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-30umBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-30umPRO | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-44g5cBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-44g5mBAS | 13/15i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-67cc | 8/9i | 10000000 | ExposureTimeMode parameter not available |
a2A4096-67cm | 8/9i | 10000000 | ExposureTimeMode parameter not available |
a2A4200-12gcBAS | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A4200-12gcPRO | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A4200-12gmBAS | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A4200-12gmPRO | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A4200-40ucBAS | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A4200-40ucPRO | 2 | 10000000 | ExposureTimeMode parameter not available |
a2A4200-40umBAS | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A4200-40umPRO | Common exposure time mode: 2 Individual exposure time mode, Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode, Stage 1: 10000000 Stage 2: 9999999 | Common Individual |
a2A4504-5gcBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-5gcPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-5gmBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-5gmPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-18ucBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-18ucPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-18umBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-18umPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-27g5cBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-27g5mBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A4504-42cc | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A4504-42cm | 10/11i | 10000000 | ExposureTimeMode parameter not available |
a2A4508-6gcBAS | 8 | 10000000 | ExposureTimeMode parameter not available |
a2A4508-6gcPRO | 8 | 10000000 | ExposureTimeMode parameter not available |
a2A4508-6gmBAS | Common: 2 Stage 1: 3 Stage 2: 2 | Common: 10000000 Stage 1: 10000000 Stage 2: Configured Stage 1 exposure time - 1 | ExposureTimeMode parameter not available |
a2A4508-6gmPRO | Common: 2 Stage 1: 3 Stage 2: 2 | Common: 10000000 Stage 1: 10000000 Stage 2: Configured Stage 1 exposure time - 1 | ExposureTimeMode parameter not available |
a2A4508-20ucBAS | 8 | 10000000 | ExposureTimeMode parameter not available |
a2A4508-20ucPRO | 8 | 10000000 | ExposureTimeMode parameter not available |
a2A4508-20umBAS | Common: 2 Stage 1: 3 Stage 2: 2 | Common: 10000000 Stage 1: 10000000 Stage 2: Configured Stage 1 exposure time - 1 | ExposureTimeMode parameter not available |
a2A4508-20umPRO | Common: 2 Stage 1: 3 Stage 2: 2 | Common: 10000000 Stage 1: 10000000 Stage 2: Configured Stage 1 exposure time - 1 | ExposureTimeMode parameter not available |
a2A5320-7gcBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-7gcPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-7gmBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-7gmPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-23ucBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-23ucPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-23umBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-23umPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-34g5cBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-34g5mBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5320-52cc | 11/12i | 10000000 | ExposureTimeMode parameter not available |
a2A5320-52cm | 11/12i | 10000000 | ExposureTimeMode parameter not available |
a2A5328-4gcBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-4gcPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-4gmBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-4gmPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-15ucBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-15ucPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-15umBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-15umPRO | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-22g5cBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-22g5mBAS | 16 | 10000000 | ExposureTimeMode parameter not available |
a2A5328-35cc | 11/12i | 10000000 | ExposureTimeMode parameter not available |
a2A5328-35cm | 11/12i | 10000000 | ExposureTimeMode parameter not available |
acA640-121gm | Standard exposure time mode: 22/23b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA640-300gc | 80 | 10000000 | ExposureTimeMode parameter not available |
acA640-300gm | 80 | 10000000 | ExposureTimeMode parameter not available |
acA640-750uc | 59 | 1000000 | ExposureTimeMode parameter not available |
acA640-750um | 59 | 1000000 | ExposureTimeMode parameter not available |
acA720-290gc | Standard exposure time mode: 22/20b Ultra Shot exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Shot exposure time mode: 13 | Standard Ultra Short |
acA720-290gm | Standard exposure time mode: 22/20b Ultra Shot exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Shot exposure time mode: 13 | Standard Ultra Short |
acA720-520uc | Standard exposure time mode: 30/24b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA720-520um | Standard exposure time mode: 30/24b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA800-200gc | 80 | 10000000 | ExposureTimeMode parameter not available |
acA800-200gm | 80 | 10000000 | ExposureTimeMode parameter not available |
acA800-510uc | 59 | 1000000 | ExposureTimeMode parameter not available |
acA800-510um | 59 | 1000000 | ExposureTimeMode parameter not available |
acA1280-60gc | 15 | 896000 | ExposureTimeMode parameter not available |
acA1280-60gm | 15 | 896000 | ExposureTimeMode parameter not available |
acA1300-60gc | 10 / 15a | 916000 / 896000a | ExposureTimeMode parameter not available |
acA1300-60gm | 10 / 15a | 916000 / 896000a | ExposureTimeMode parameter not available |
acA1300-60gmNIR | 10 / 15a | 916000 / 896000a | ExposureTimeMode parameter not available |
acA1300-75gc | 80 | 1000000 | ExposureTimeMode parameter not available |
acA1300-75gm | 80 | 1000000 | ExposureTimeMode parameter not available |
acA1300-200uc | 59 | 1000000 | ExposureTimeMode parameter not available |
acA1300-200um | 59 | 1000000 | ExposureTimeMode parameter not available |
acA1440-73gc | Standard exposure time mode: 22 / 23b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA1440-73gm | Standard exposure time mode: 22 / 23b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA1440-220uc | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA1440-220um | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 13 | Standard Ultra Short |
acA1600-20gc | 25 | 1000000 | ExposureTimeMode parameter not available |
acA1600-20uc | 25 | 10000000 | ExposureTimeMode parameter not available |
acA1600-60gc | 10/35a | 840000 | ExposureTimeMode parameter not available |
acA1600-60gm | 10/35a | 840000 | ExposureTimeMode parameter not available |
acA1920-25gc | 35 | 999985 | ExposureTimeMode parameter not available |
acA1920-25gm | 35 | 999985 | ExposureTimeMode parameter not available |
acA1920-25uc | 35 | 9999990 | ExposureTimeMode parameter not available |
acA1920-25um | 35 | 9999990 | ExposureTimeMode parameter not available |
acA1920-40gc | 34/40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-40gm | 34/40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-40uc | 34/40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-40ucMED | 34/40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-40um | 34 / 40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-40umMED | 34/40b | 10000000 | ExposureTimeMode parameter not available |
acA1920-48gc | 137 | 1000000 | ExposureTimeMode parameter not available |
acA1920-48gm | 137 | 1000000 | ExposureTimeMode parameter not available |
acA1920-50gc | 24/27b | 10000000 | ExposureTimeMode parameter not available |
acA1920-50gm | 24/27b | 10000000 | ExposureTimeMode parameter not available |
acA1920-150uc | 105 | 1000000 | ExposureTimeMode parameter not available |
acA1920-150um | 105 | 1000000 | ExposureTimeMode parameter not available |
acA1920-155uc | 20/21b | 10000000 | ExposureTimeMode parameter not available |
acA1920-155ucMED | 20/21b | 10000000 | ExposureTimeMode parameter not available |
acA1920-155um | 20/21b | 10000000 | ExposureTimeMode parameter not available |
acA1920-155umMED | 20/21b | 10000000 | ExposureTimeMode parameter not available |
acA2000-50gc | 24 | 10000000 | ExposureTimeMode parameter not available |
acA2000-50gm | 24 | 10000000 | ExposureTimeMode parameter not available |
acA2000-165uc | 28c | 10000000 | ExposureTimeMode parameter not available |
acA2000-165um | 28c | 10000000 | ExposureTimeMode parameter not available |
acA2040-25gc | 24 | 10000000 | ExposureTimeMode parameter not available |
acA2040-25gm | 24 | 10000000 | ExposureTimeMode parameter not available |
acA2040-25gmNIR | 24 | 10000000 | ExposureTimeMode parameter not available |
acA2040-35gc | Standard exposure time mode: 26 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2040-35gm | Standard exposure time mode: 26 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2040-55uc | Standard exposure time mode: 27 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2040-55um | Standard exposure time mode: 27 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2040-90uc | 28c | 10000000 | ExposureTimeMode parameter not available |
acA2040-90um | 28c | 10000000 | ExposureTimeMode parameter not available |
acA2040-90umNIR | 28c | 10000000 | ExposureTimeMode parameter not available |
acA2040-120uc | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2040-120um | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-20gc | Standard exposure time mode: 28 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-20gm | Standard exposure time mode: 28 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-35uc | Standard exposure time mode: 29 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-35ucMED | 29 | 10000000 | ExposureTimeMode parameter not available |
acA2440-35um | Standard exposure time mode: 29 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-35umMED | 29 | 10000000 | ExposureTimeMode parameter not available |
acA2440-75uc | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-75ucMED | 21/22b | 10000000 | ExposureTimeMode parameter not available |
acA2440-75um | Standard exposure time mode: 21/20b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
acA2440-75umMED | 21/22b | 10000000 | ExposureTimeMode parameter not available |
acA2500-14gc | 35 | 999985 | ExposureTimeMode parameter not available |
acA2500-14gm | 35 | 999985 | ExposureTimeMode parameter not available |
acA2500-14uc | 35 | 9999990 | ExposureTimeMode parameter not available |
acA2500-14um | 35 | 9999990 | ExposureTimeMode parameter not available |
acA2500-20gc | 137 | 1000000 | ExposureTimeMode parameter not available |
acA2500-20gcMED | 137 | 1000000 | ExposureTimeMode parameter not available |
acA2500-20gm | 137 | 1000000 | ExposureTimeMode parameter not available |
acA2500-20gmMED | 137 | 1000000 | ExposureTimeMode parameter not available |
acA2500-60uc | 81 | 1000000 | ExposureTimeMode parameter not available |
acA2500-60um | 81 | 1000000 | ExposureTimeMode parameter not available |
acA3088-16gc | Rolling shutter mode: 25 Global Reset Release shutter mode: 625 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3088-16gm | Rolling shutter mode: 25 Global Reset Release shutter mode: 625 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3088-57uc | Rolling shutter mode: 8 Global Reset Release shutter mode: 200 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3088-57ucMED | Rolling shutter mode: 8 Global Reset Release shutter mode: 200 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3088-57um | Rolling shutter mode: 8 Global Reset Release shutter mode: 200 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3088-57umMED | Rolling shutter mode: 8 Global Reset Release shutter mode: 200 | Rolling shutter mode: 10000000 Global Reset Release shutter mode: 10000000 | ExposureTimeMode parameter not available |
acA3800-10gc | 35f | 1600000 | ExposureTimeMode parameter not available |
acA3800-10gm | 35f | 1600000 | ExposureTimeMode parameter not available |
acA3800-14uc | 35f | 1600000 | ExposureTimeMode parameter not available |
acA3800-14um | 35f | 1600000 | ExposureTimeMode parameter not available |
acA4024-8gc | Rolling Shutter mode: 35 Global Reset Release shutter mode: 1260 | 10000000 | ExposureTimeMode parameter not available |
acA4024-8gm | Rolling Shutter mode: 35 Global Reset Release shutter mode: 1260 | 10000000 | ExposureTimeMode parameter not available |
acA4024-29uc | Rolling shutter mode: 10/12b Global Reset Release shutter mode: 360/432b | 10000000 | ExposureTimeMode parameter not available |
acA4024-29um | Rolling shutter mode: 10/12b Global Reset Release shutter mode: 360/432b | 10000000 | ExposureTimeMode parameter not available |
acA4096-11gc | Standard exposure time mode: 38 Ultra Short exposure time mode: 2j | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-11gm | Standard exposure time mode: 38 Ultra Short exposure time mode: 2j | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-30uc | Standard exposure time mode: 30 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-30ucMED | 30 | 10000000 | ExposureTimeMode parameter not available |
acA4096-30um | Standard exposure time mode: 30 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-30umMED | 30 | 10000000 | ExposureTimeMode parameter not available |
acA4096-40uc | Standard exposure time mode: 26/27b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-40ucMED | 26/27b | 10000000 | ExposureTimeMode parameter not available |
acA4096-40um | Standard exposure time mode: 26/27b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4096-40umMED | 26/27b | 10000000 | ExposureTimeMode parameter not available |
acA4112-8gc | Standard exposure time mode: 38 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-8gm | Standard exposure time mode: 38 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-20uc | Standard exposure time mode: 30 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-20ucMED | 30 | 10000000 | ExposureTimeMode parameter not available |
acA4112-20um | Standard exposure time mode: 30 Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-20umMED | 30 | 10000000 | ExposureTimeMode parameter not available |
acA4112-30uc | Standard exposure time mode: 26/27b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-30ucMED | 26/27b | 10000000 | ExposureTimeMode parameter not available |
acA4112-30um | Standard exposure time mode: 26/27b Ultra Short exposure time mode: 2 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 16 | Standard Ultra Short |
acA4112-30umMED | 26/27b | 10000000 | ExposureTimeMode parameter not available |
acA5472-5gc | Rolling shutter mode: 52/55b Global Reset Release shutter mode: 1872/1980b | 10000016/10000045b | ExposureTimeMode parameter not available |
acA5472-5gm | Rolling shutter mode: 52/55b Global Reset Release shutter mode: 1872/1980b | 10000016/10000045b | ExposureTimeMode parameter not available |
acA5472-17uc | Rolling shutter mode: 13/16b Global Reset Release shutter mode: 468/576b | 10000003 / 10000000b | ExposureTimeMode parameter not available |
acA5472-17ucMED | Rolling shutter mode: 13/16b Global Reset Release shutter mode: 468/576b | 10000003 / 10000000b | ExposureTimeMode parameter not available |
acA5472-17um | Rolling shutter mode: 13/16b Global Reset Release shutter mode: 468/576b | 10000003 / 10000000b | ExposureTimeMode parameter not available |
acA5472-17umMED | Rolling shutter mode: 13/16b Global Reset Release shutter mode: 468/576b | 10000003 / 10000000b | ExposureTimeMode parameter not available |
boA1936-400cc | Standard exposure time mode: 7/7/8g Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 4 | Standard Ultra Short |
boA1936-400cm | Standard exposure time mode: 7/7/8g Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 4 | Standard Ultra Short |
boA2448-250cc | Standard exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA2448-250cm | Standard exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA2832-190cc | Standard exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA2832-190cm | Standard exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA4096-93cc | Standard exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Standard exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Standard Ultra Short |
boA4096-93cm | Standard exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Standard exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Standard Ultra Short |
boA4096-180cc | Standard exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA4096-180cm | Standard exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA4112-68cc | Standard exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Standard exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Standard Ultra Short |
boA4112-68cm | Standard exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Standard exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Standard Ultra Short |
boA4500-45cc | Standard exposure time mode: 100 Short exposure time mode: 20 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA4500-45cm | Standard exposure time mode: 100 Short exposure time mode: 20 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA4504-100cc | Standard exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA4504-100cm | Standard exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA5120-150cc | 8 | 1 / frame rate | ExposureTimeMode parameter not available |
boA5120-150cm | 8 | 1 / frame rate | ExposureTimeMode parameter not available |
boA5120-230cc | 4 | 1 / frame rate | ExposureTimeMode parameter not available |
boA5120-230cm | 4 | 1 / frame rate | ExposureTimeMode parameter not available |
boA5320-150cc | Standard exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA5320-150cm | Standard exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA5328-100cc | Standard exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA5328-100cm | Standard exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Standard exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Standard Ultra Short |
boA6500-36cc | Standard exposure time mode: 100 Short exposure time mode: 20 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA6500-36cm | Standard exposure time mode: 100 Short exposure time mode: 20 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA8100-16cc | Standard exposure time mode: 100 Short exposure time mode: 45 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA8100-16cm | Standard exposure time mode: 100 Short exposure time mode: 45 | Standard exposure time mode: 8000000 Short exposure time mode: 100 | Standard Short |
boA9344-30cc | 12 | 1 / frame rate | ExposureTimeMode parameter not available |
boA9344-30cm | 12 | 1 / frame rate | ExposureTimeMode parameter not available |
boA9344-70cc | 12 | 1 / frame rate | ExposureTimeMode parameter not available |
boA9344-70cm | 12 | 1 / frame rate | ExposureTimeMode parameter not available |
boA13440-17cm | 8-bit sensor bit depth: 551 | 8000000 | Standard |
daA720-520uc | 18 / 18 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA720-520um | 18 / 18 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA1280-54uc | 10de | 1000000 | ExposureTimeMode parameter not available |
daA1280-54um | 10de | 1000000 | ExposureTimeMode parameter not available |
daA1440-220uc | 18 / 18 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA1440-220um | 18 / 18 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA1600-60uc | 10d | 850000 | ExposureTimeMode parameter not available |
daA1600-60um | 10d | 850000 | ExposureTimeMode parameter not available |
daA1920-15um | 10d | 1000000 | ExposureTimeMode parameter not available |
daA1920-30uc | 10d | 1000000 | ExposureTimeMode parameter not available |
daA1920-30um | 10d | 1000000 | ExposureTimeMode parameter not available |
daA1920-160uc | 19 / 19 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA1920-160um | 19 / 19 / 20g | 10000000 | ExposureTimeMode parameter not available |
daA2448-70uc | 10 / 11i | 10000000 | ExposureTimeMode parameter not available |
daA2448-70um | 10 / 11i | 10000000 | ExposureTimeMode parameter not available |
daA2500-14uc | 10d | 1000000 | ExposureTimeMode parameter not available |
daA2500-14um | 10d | 1000000 | ExposureTimeMode parameter not available |
daA3840-45uc | 26dh | 999999 | ExposureTimeMode parameter not available |
daA3840-45um | 26dh | 999999 | ExposureTimeMode parameter not available |
dmA720-290gc | Standard exposure time mode: 18 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
dmA720-290gm | Standard exposure time mode: 18 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
dmA1440-73gc | Standard exposure time mode: 18 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
dmA1440-73gm | Standard exposure time mode: 18 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
dmA1920-51gc | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
dmA1920-51gm | Standard exposure time mode: 19 Ultra Short exposure time mode: 1 | Standard exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Standard Ultra Short |
puA1280-54uc | 10de | 1000000 | ExposureTimeMode parameter not available |
puA1280-54um | 10de | 1000000 | ExposureTimeMode parameter not available |
puA1600-60uc | 10d | 850000 | ExposureTimeMode parameter not available |
puA1600-60um | 10d | 850000 | ExposureTimeMode parameter not available |
puA1920-30uc | 10d | 1000000 | ExposureTimeMode parameter not available |
puA1920-30um | 10d | 1000000 | ExposureTimeMode parameter not available |
puA2500-14uc | 10d | 1000000 | ExposureTimeMode parameter not available |
puA2500-14um | 10d | 1000000 | ExposureTimeMode parameter not available |
r2L2048-29gc | 2.17 | 1000000 | Common |
r2L2048-58gm | 1.57 | 1000000 | Common |
r2L2048-62cc | 3.25 | 1000000 | Common |
r2L2048-62g5c | TBD | 1000000 | Common |
r2L2048-172cm | 1.68 | 1000000 | Common |
r2L2048-172g5m | TBD | 1000000 | Common |
r2L4096-14gc | 3.15 | 1000000 | Common |
r2L4096-29gm | 2.1 | 1000000 | Common |
r2L4096-42cc | 3.15 | 1000000 | Common |
r2L4096-42g5c | TBD | 1000000 | Common |
r2L4096-84cm | 2.1 | 1000000 | Common |
r2L4096-84g5m | TBD | 1000000 | Common |
r2L8192-200cm | 3.07 | 1000000 | Common |
r2L16384-120cm | 2.56 | 1000000 | Common |
-
Global shutter mode / Rolling shutter mode
-
8-bit pixel format / 12-bit pixel format
-
Valid when the pixel format is set to a 12-bit format. For 8-bit formats, the value depends on the USB 3.0 bandwidth available. See table 1 below.
-
Depending on the camera's sensor and frame rate, the effective exposure time may vary from the exposure time set. The variation is normally in the range of microseconds, but if a very low exposure time is set, this should be taken into account.
-
Due to the sensor's specific characteristics, on exposure times below ≈70 µs, the increment may vary and may be higher than 1 µs. Therefore, not all exposure time values can be reached. This behavior also depends on the Image ROI settings and the overlap mode.
-
Due to the sensor's specific characteristics, if the shutter mode is set to Global Reset Release, the effective exposure time is longer than the exposure time set. See table 2 below.
-
8-bit sensor bit depth / 10-bit sensor bit depth / 12-bit sensor bit depth
-
Valid at default settings. Value depends on the USB 3.0 bandwidth available (
DeviceLinkThroughputLimit
parameter setting). -
10-bit sensor bit depth / 12-bit sensor bit depth
-
When setting an exposure time of 2 µs or 3 µs in Ultra Short exposure time mode, the effective exposure time may be slightly longer than specified. The difference is less than a microsecond.
-
2x CXP (AUX power or PoCXP) or 1x CXP (AUX power) (8-bit sensor bit depth) / 2x CXP (AUX power or PoCXP) or 1x CXP (AUX power) (10-bit sensor bit depth) / 2x CXP (AUX power or PoCXP) or 1x CXP (AUX power) (12-bit sensor bit depth) / 1x CXP (PoCXP) (8-bit sensor bit depth) / 1x CXP (PoCXP) (10-bit sensor bit depth) / 1x CXP (PoCXP) (12-bit sensor bit depth)
-
When setting an exposure time of 1 µs or 2 µs in Ultra Short exposure time mode, the resulting image brightness may be higher than expected.
Additional Information for ace Classic Cameras#
Table 1#
The following table applies to acA2040-90uc/um/umNIR and acA2000-165uc/um/umNIR cameras using an 8-bit pixel format.
Available USB Bandwidth (Device Link Throughput) | Minimum Exposure Time and Exposure Time Offset (8-bit Pixel Formats) |
---|---|
≤ 108000 | 42 |
108001–140000 | 32 |
140001–160020 | 28 |
160021–180000 | 25 |
180001–192112 | 24 |
192113–216000 | 42 |
216001–280000 | 32 |
280001–320040 | 28 |
320041–360000 | 25 |
360001–384224 | 24 |
Table 2#
The following table applies to the indicated camera models when operated in Global Reset Release shutter mode.
Camera Model | Additional Exposure Time in GRR [µs] |
---|---|
acA3800-10gm/gc | 5218 |
acA3800-14um/uc | 4077 |
Example: Assume you are operating an acA3800-10gm camera in Global Reset Release shutter mode. You set the exposure time to 1000 µs. The effective exposure time is 1000 + 5218 = 6218 µs.
Sample Code#
ace Classic/U/L GigE Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTimeAbs", &d);
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTimeAbs", 3500.0);
CHECK(errRes);
ace 2, boost, dart M/R, and racer 2 Cameras#
// Determine the current exposure time using Exposure Time
double d = camera.ExposureTime.GetValue();
// Determine the current exposure time using Effective Exposure Time
double d = camera.BslEffectiveExposureTime.GetValue();
// Set the exposure time mode to Common
camera.ExposureTimeMode.SetValue(ExposureTimeMode_Common);
// Set the exposure time to 3500 microseconds
camera.ExposureTime.SetValue(3500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Determine the current exposure time using Exposure Time
double d = CFloatParameter(nodemap, "ExposureTime").GetValue();
// Determine the current exposure time using Effective Exposure Time
d = CFloatParameter(nodemap, "BslEffectiveExposureTime").GetValue();
// Set the exposure time mode to Common
CEnumParameter(nodemap, "ExposureTimeMode").SetValue("Common");
// Set the exposure time to 3500 microseconds
CFloatParameter(nodemap, "ExposureTime").SetValue(3500.0);
// Determine the current exposure time using Exposure Time
double d = camera.Parameters[PLCamera.ExposureTime].GetValue();
// Determine the current exposure time using Effective Exposure Time
d = camera.Parameters[PLCamera.BslEffectiveExposureTime].GetValue();
// Set the exposure time mode to Common
camera.Parameters[PLCamera.ExposureTimeMode].SetValue(PLCamera.ExposureTimeMode.Common);
// Set the exposure time to 3500 microseconds
camera.Parameters[PLCamera.ExposureTime].SetValue(3500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time using Exposure Time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTime", &d);
CHECK(errRes);
/* Determine the current exposure time using Effective Exposure Time */
errRes = PylonDeviceGetFloatFeature(hdev, "BslEffectiveExposureTime", &d);
CHECK(errRes);
/* Set the exposure time mode to Common */
errRes = PylonDeviceFeatureFromString(hdev, "ExposureTimeMode", "Common");
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 3500.0);
CHECK(errRes);
# Determine the current exposure time using Exposure Time
d = camera.ExposureTime.Value
# Determine the current exposure time using Effective Exposure Time
d = camera.BslEffectiveExposureTime.Value
# Set the exposure time mode to Common
camera.ExposureTimeMode.Value = "Common"
# Set the exposure time to 3500 microseconds
camera.ExposureTime.Value = 3500.0
Other Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTime", &d);
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 3500.0);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.