Skip to content

Test Images#

The Test Images camera feature allows you to check the camera's basic functionality and its ability to transmit images.

Test images can be used for maintenance purposes and failure diagnostics. They are generated by the camera itself. Therefore, the optics or the image sensor of the camera are not involved in their creation.

Using the Feature#

Displaying Test Images#

  1. Select a test image by setting the TestImageSelector parameter to one of the following values:
  2. Acquire at least one image to display the selected test image. If you want to display the test image in the pylon Viewer, click the single or continuous shot button on the toolbar.

Available Test Images#

Depending on your camera model, the following test images are available:

Test Image 1 - Fixed Diagonal Gray Gradients (8 bit)#

  • Consists of fixed diagonal gray gradients ranging from 0 to 255.
  • Is best suited for when the camera is configured for monochrome 8-bit output.

Test Image Diagonal Gray Gradient

Test Image 2 - Moving Diagonal Gray Gradients (8 bit)#

  • See test image 1.
  • Difference: Consists of moving diagonal gray gradients. When a new image acquisition is triggered, the image moves left one pixel.

Test Image 3 - Moving Diagonal Gray Gradients#

  • See test image 1.
  • Difference: Consists of moving diagonal gray gradients.
  • On most cameras, this is a 12-bit pattern. On some camera models, this is a 10-bit pattern.

Test Image 4 - Moving Diagonal Gray Gradient Feature Test (8 bit)#

  • See test image 1.
  • Difference: Consists of moving diagonal gray gradients. In addition, it shows the effects of any digital processing features that are enabled (e.g., luminance lookup table).

Test Image 5 - Moving Diagonal Gray Gradient Feature Test#

  • See test image 1.
  • Difference: Consists of moving diagonal gray gradients. In addition, it shows the effects of any digital processing features that are enabled (e.g., luminance lookup table).
  • On most cameras, this is a 12-bit pattern. On some camera models, this is a 10-bit pattern.

Test Image 6 - Moving Diagonal Color Gradients#

  • If available, this test image consists of moving diagonal color gradients. When a new image acquisition is triggered, the image moves left one pixel.

Test Image Diagonal Color Gradient

Effect of Camera Settings on Test Images#

  • The camera's analog features such as Gain, Black Level, and Exposure Time have no effect on the test images.
  • The camera's digital features, e.g., the Luminance Lookup Table, only effect test images 4 and 5. Use test images 4 or 5 if you want to check the effect of using a digital feature.

Additional Parameters#

Depending on your camera model, the TestImageResetAndHold parameter is available:

  • It allows you to turn a moving test image into a fixed one.
  • When the command is issued, all gradients are displayed at their starting positions. If new image acquisitions are triggered, they remain at these positions.
  • It can be applied to fixed and moving test images.

Specifics#

Show all camera models

Camera Model Available Test Images Additional Parameters
a2A640-240gmSWIR None (see Test Patterns) None
a2A640-240umSWIR None (see Test Patterns) None
a2A1280-80gmSWIR None (see Test Patterns) None
a2A1280-125umSWIR None (see Test Patterns) None
a2A1920-51gcBAS None (see Test Patterns) None
a2A1920-51gcPRO None (see Test Patterns) None
a2A1920-51gmBAS None (see Test Patterns) None
a2A1920-51gmPRO None (see Test Patterns) None
a2A1920-160ucBAS None (see Test Patterns) None
a2A1920-160ucPRO None (see Test Patterns) None
a2A1920-160umBAS None (see Test Patterns) None
a2A1920-160umPRO None (see Test Patterns) None
a2A1920-165g5cBAS None (see Test Patterns) None
a2A1920-165g5mBAS None (see Test Patterns) None
a2A2048-35gmSWIR None (see Test Patterns) None
a2A2048-110umSWIR None (see Test Patterns) None
a2A2440-98g5cBAS None (see Test Patterns) None
a2A2440-98g5mBAS None (see Test Patterns) None
a2A2448-23gcBAS None (see Test Patterns) None
a2A2448-23gcPRO None (see Test Patterns) None
a2A2448-23gmBAS None (see Test Patterns) None
a2A2448-23gmPRO None (see Test Patterns) None
a2A2448-75ucBAS None (see Test Patterns) None
a2A2448-75ucPRO None (see Test Patterns) None
a2A2448-75umBAS None (see Test Patterns) None
a2A2448-75umPRO None (see Test Patterns) None
a2A2448-105g5cBAS None (see Test Patterns) None
a2A2448-105g5mBAS None (see Test Patterns) None
a2A2448-120cc None (see Test Patterns) None
a2A2448-120cm None (see Test Patterns) None
a2A2448-210cc None (see Test Patterns) None
a2A2448-210cm None (see Test Patterns) None
a2A2560-20gmSWIR None (see Test Patterns) None
a2A2560-70umSWIR None (see Test Patterns) None
a2A2590-22gcBAS None (see Test Patterns) None
a2A2590-22gcPRO None (see Test Patterns) None
a2A2590-22gmBAS None (see Test Patterns) None
a2A2590-22gmPRO None (see Test Patterns) None
a2A2590-60ucBAS None (see Test Patterns) None
a2A2590-60ucPRO None (see Test Patterns) None
a2A2590-60umBAS None (see Test Patterns) None
a2A2590-60umPRO None (see Test Patterns) None
a2A2600-20gcBAS None (see Test Patterns) None
a2A2600-20gcPRO None (see Test Patterns) None
a2A2600-20gmBAS None (see Test Patterns) None
a2A2600-20gmPRO None (see Test Patterns) None
a2A2600-64ucBAS None (see Test Patterns) None
a2A2600-64ucPRO None (see Test Patterns) None
a2A2600-64umBAS None (see Test Patterns) None
a2A2600-64umPRO None (see Test Patterns) None
a2A2840-14gcBAS None (see Test Patterns) None
a2A2840-14gcPRO None (see Test Patterns) None
a2A2840-14gmBAS None (see Test Patterns) None
a2A2840-14gmPRO None (see Test Patterns) None
a2A2840-14gmUV None (see Test Patterns) None
a2A2840-48ucBAS None (see Test Patterns) None
a2A2840-48ucPRO None (see Test Patterns) None
a2A2840-48umBAS None (see Test Patterns) None
a2A2840-48umPRO None (see Test Patterns) None
a2A2840-48umUV None (see Test Patterns) None
a2A2840-67g5cBAS None (see Test Patterns) None
a2A2840-67g5mBAS None (see Test Patterns) None
a2A2840-67g5mUV None (see Test Patterns) None
a2A2840-86cc None (see Test Patterns) None
a2A2840-86cm None (see Test Patterns) None
a2A3840-13gcBAS None (see Test Patterns) None
a2A3840-13gcPRO None (see Test Patterns) None
a2A3840-13gmBAS None (see Test Patterns) None
a2A3840-13gmPRO None (see Test Patterns) None
a2A3840-45ucBAS None (see Test Patterns) None
a2A3840-45ucPRO None (see Test Patterns) None
a2A3840-45umBAS None (see Test Patterns) None
a2A3840-45umPRO None (see Test Patterns) None
a2A4096-9gcBAS None (see Test Patterns) None
a2A4096-9gcPRO None (see Test Patterns) None
a2A4096-9gmBAS None (see Test Patterns) None
a2A4096-9gmPRO None (see Test Patterns) None
a2A4096-30ucBAS None (see Test Patterns) None
a2A4096-30ucPRO None (see Test Patterns) None
a2A4096-30umBAS None (see Test Patterns) None
a2A4096-30umPRO None (see Test Patterns) None
a2A4096-44g5cBAS None (see Test Patterns) None
a2A4096-44g5mBAS None (see Test Patterns) None
a2A4096-67cc None (see Test Patterns) None
a2A4096-67cm None (see Test Patterns) None
a2A4200-12gcBAS None (see Test Patterns) None
a2A4200-12gcPRO None (see Test Patterns) None
a2A4200-12gmBAS None (see Test Patterns) None
a2A4200-12gmPRO None (see Test Patterns) None
a2A4200-40ucBAS None (see Test Patterns) None
a2A4200-40ucPRO None (see Test Patterns) None
a2A4200-40umBAS None (see Test Patterns) None
a2A4200-40umPRO None (see Test Patterns) None
a2A4504-5gcBAS None (see Test Patterns) None
a2A4504-5gcPRO None (see Test Patterns) None
a2A4504-5gmBAS None (see Test Patterns) None
a2A4504-5gmPRO None (see Test Patterns) None
a2A4504-18ucBAS None (see Test Patterns) None
a2A4504-18ucPRO None (see Test Patterns) None
a2A4504-18umBAS None (see Test Patterns) None
a2A4504-18umPRO None (see Test Patterns) None
a2A4504-27g5cBAS None (see Test Patterns) None
a2A4504-27g5mBAS None (see Test Patterns) None
a2A4504-42cc None (see Test Patterns) None
a2A4504-42cm None (see Test Patterns) None
a2A4508-6gcBAS None (see Test Patterns) None
a2A4508-6gcPRO None (see Test Patterns) None
a2A4508-6gmBAS None (see Test Patterns) None
a2A4508-6gmPRO None (see Test Patterns) None
a2A4508-20ucBAS None (see Test Patterns) None
a2A4508-20ucPRO None (see Test Patterns) None
a2A4508-20umBAS None (see Test Patterns) None
a2A4508-20umPRO None (see Test Patterns) None
a2A5320-7gcBAS None (see Test Patterns) None
a2A5320-7gcPRO None (see Test Patterns) None
a2A5320-7gmBAS None (see Test Patterns) None
a2A5320-7gmPRO None (see Test Patterns) None
a2A5320-23ucBAS None (see Test Patterns) None
a2A5320-23ucPRO None (see Test Patterns) None
a2A5320-23umBAS None (see Test Patterns) None
a2A5320-23umPRO None (see Test Patterns) None
a2A5320-34g5cBAS None (see Test Patterns) None
a2A5320-34g5mBAS None (see Test Patterns) None
a2A5320-52cc None (see Test Patterns) None
a2A5320-52cm None (see Test Patterns) None
a2A5328-4gcBAS None (see Test Patterns) None
a2A5328-4gcPRO None (see Test Patterns) None
a2A5328-4gmBAS None (see Test Patterns) None
a2A5328-4gmPRO None (see Test Patterns) None
a2A5328-15ucBAS None (see Test Patterns) None
a2A5328-15ucPRO None (see Test Patterns) None
a2A5328-15umBAS None (see Test Patterns) None
a2A5328-15umPRO None (see Test Patterns) None
a2A5328-22g5cBAS None (see Test Patterns) None
a2A5328-22g5mBAS None (see Test Patterns) None
a2A5328-35cc None (see Test Patterns) None
a2A5328-35cm None (see Test Patterns) None
acA640-121gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA640-300gc 1, 2a, 3b, 4, 5b, 6 TestImageResetAndHold
acA640-300gm 1, 2a, 3b, 4, 5b TestImageResetAndHold
acA640-750uc 1, 2a, 3, 4, 5, 6 None
acA640-750um 1, 2a, 3, 4, 5 None
acA720-290gc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA720-290gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA720-520uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA720-520um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA800-200gc 1, 2a, 3b, 4, 5b, 6 TestImageResetAndHold
acA800-200gm 1, 2a, 3b, 4, 5b TestImageResetAndHold
acA800-510uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA800-510um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1280-60gc 1, 2, 3, 4, 5, 6 None
acA1280-60gm 1, 2, 3, 4, 5 None
acA1300-60gc 1, 2, 3, 4, 5 None
acA1300-60gm 1, 2, 3, 4, 5 None
acA1300-60gmNIR 1, 2, 3, 4, 5 None
acA1300-75gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1300-75gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1300-200uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1300-200um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1440-73gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1440-73gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1440-220uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1440-220um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1600-20gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1600-20uc 1, 2, 3, 4, 5, 6 None
acA1600-60gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1600-60gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-25gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-25gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-25uc 1, 2, 3, 4, 5, 6 None
acA1920-25um 1, 2, 3, 4, 5 None
acA1920-40gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-40gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-40uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1920-40ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1920-40um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-40umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-48gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-48gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-50gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-50gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-150uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1920-150um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-155uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1920-155ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA1920-155um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA1920-155umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2000-50gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2000-50gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2000-165uc 1, 2, 3, 4, 5, 6 None
acA2000-165um 1, 2, 3, 4, 5 None
acA2040-25gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-25gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-25gmNIR 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-35gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-35gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-55uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2040-55um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2040-90uc 1, 2, 3, 4, 5, 6 None
acA2040-90um 1, 2, 3, 4, 5 None
acA2040-90umNIR 1, 2, 3, 4, 5 None
acA2040-120uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2040-120um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-20gc 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-20gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-35uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2440-35ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2440-35um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-35umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-75uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2440-75ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2440-75um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2440-75umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2500-14gc 1, 2, 3, 4, 5, 6 None
acA2500-14gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2500-14uc 1, 2, 3, 4, 5, 6 None
acA2500-14um 1, 2, 3, 4, 5 None
acA2500-20gc 1, 2a, 3b, 4, 5b,6 TestImageResetAndHold
acA2500-20gcMED 1, 2a, 3b, 4, 5b TestImageResetAndHold
acA2500-20gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA2500-20gmMED 1, 2a, 3b, 4, 5b TestImageResetAndHold
acA2500-60uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA2500-60um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA3088-16gc 1, 2, 3, 4, 5, 6 TestImageResetAndHold
acA3088-16gm 1, 2, 3, 4, 5 TestImageResetAndHold
acA3088-57uc 1, 2, 3, 4, 5, 6 None
acA3088-57ucMED 1, 2, 3, 4, 5, 6 None
acA3088-57um 1, 2, 3, 4, 5 None
acA3088-57umMED 1, 2, 3, 4, 5 None
acA3800-10gc 1, 2, 3, 4, 5, 6 None
acA3800-10gm 1, 2, 3, 4, 5 None
acA3800-14uc 1, 2, 3, 4, 5, 6 None
acA3800-14um 1, 2, 3, 4, 5 None
acA4024-8gc 1, 2, 3, 4, 5, 6 TestImageResetAndHold
acA4024-8gm 1, 2, 3, 4, 5 TestImageResetAndHold
acA4024-29uc 1, 2, 3, 4, 5, 6 TestImageResetAndHold
acA4024-29um 1, 2, 3, 4, 5 TestImageResetAndHold
acA4096-11gc 1, 2, 3, 4, 5, 6 TestImageResetAndHold
acA4096-11gm 1, 2, 3, 4, 5 TestImageResetAndHold
acA4096-30uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4096-30ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4096-30um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4096-30umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4096-40uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4096-40ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4096-40um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4096-40umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4112-8gc 1, 2, 3, 4, 5, 6 TestImageResetAndHold
acA4112-8gm 1, 2, 3, 4, 5 TestImageResetAndHold
acA4112-20uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4112-20ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4112-20um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4112-20umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4112-30uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4112-30ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA4112-30um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA4112-30umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
acA5472-5gc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA5472-5gm 1, 2a, 3, 4, 5 TestImageResetAndHold
acA5472-17uc 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA5472-17ucMED 1, 2a, 3, 4, 5, 6 TestImageResetAndHold
acA5472-17um 1, 2a, 3, 4, 5 TestImageResetAndHold
acA5472-17umMED 1, 2a, 3, 4, 5 TestImageResetAndHold
boA1936-400cc None (see Test Patterns) None
boA1936-400cm None (see Test Patterns) None
boA2448-250cc None (see Test Patterns) None
boA2448-250cm None (see Test Patterns) None
boA2832-190cc None (see Test Patterns) None
boA2832-190cm None (see Test Patterns) None
boA4096-93cc None (see Test Patterns) None
boA4096-93cm None (see Test Patterns) None
boA4096-180cc None (see Test Patterns) None
boA4096-180cm None (see Test Patterns) None
boA4112-68cc None (see Test Patterns) None
boA4112-68cm None (see Test Patterns) None
boA4500-45cc None (see Test Patterns) None
boA4500-45cm None (see Test Patterns) None
boA4504-100cc None (see Test Patterns) None
boA4504-100cm None (see Test Patterns) None
boA5120-150cc None (see Test Patterns) None
boA5120-150cm None (see Test Patterns) None
boA5120-230cc None (see Test Patterns) None
boA5120-230cm None (see Test Patterns) None
boA5320-150cc None (see Test Patterns) None
boA5320-150cm None (see Test Patterns) None
boA5328-100cc None (see Test Patterns) None
boA5328-100cm None (see Test Patterns) None
boA6500-36cc None (see Test Patterns) None
boA6500-36cm None (see Test Patterns) None
boA8100-16cc None (see Test Patterns) None
boA8100-16cm None (see Test Patterns) None
boA9344-30cc None (see Test Patterns) None
boA9344-30cm None (see Test Patterns) None
boA9344-70cc None (see Test Patterns) None
boA9344-70cm None (see Test Patterns) None
boA13440-17cm None (see Test Patterns) None
daA720-520uc None (see Test Patterns) None
daA720-520um None (see Test Patterns) None
daA1280-54uc None (see Test Patterns) None
daA1280-54um None (see Test Patterns) None
daA1440-220uc None (see Test Patterns) None
daA1440-220um None (see Test Patterns) None
daA1600-60uc None (see Test Patterns) None
daA1600-60um None (see Test Patterns) None
daA1920-15um None (see Test Patterns) None
daA1920-30uc None (see Test Patterns) None
daA1920-30um None (see Test Patterns) None
daA1920-160uc None (see Test Patterns) None
daA1920-160um None (see Test Patterns) None
daA2448-70uc None (see Test Patterns) None
daA2448-70um None (see Test Patterns) None
daA2500-14uc None (see Test Patterns) None
daA2500-14um None (see Test Patterns) None
daA3840-45uc None (see Test Patterns) None
daA3840-45um None (see Test Patterns) None
dmA720-290gc None (see Test Patterns) None
dmA720-290gm None (see Test Patterns) None
dmA1440-73gc None (see Test Patterns) None
dmA1440-73gm None (see Test Patterns) None
dmA1920-51gc None (see Test Patterns) None
dmA1920-51gm None (see Test Patterns) None
puA1280-54uc None (see Test Patterns) None
puA1280-54um None (see Test Patterns) None
puA1600-60uc None (see Test Patterns) None
puA1600-60um None (see Test Patterns) None
puA1920-30uc None (see Test Patterns) None
puA1920-30um None (see Test Patterns) None
puA2500-14uc None (see Test Patterns) None
puA2500-14um None (see Test Patterns) None
r2L8192-200cm None (see Test Patterns) None
r2L16384-120cm None (see Test Patterns) None

  1. When the device temperature reaches the over temperature threshold, it no longer acquires images, but delivers the internally generated test image 2.

  2. Test images 3 and 5 are 10-bit patterns.

Sample Code#

// Select test image 1
camera.TestImageSelector.SetValue(TestImageSelector_Testimage1);
// Acquire images to display the selected test image
// ...
// (Insert your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing method.)
INodeMap& nodemap = camera.GetNodeMap();
// Select test image 1
CEnumParameter(nodemap, "TestImageSelector").SetValue("Testimage1");
// Acquire images to display the selected test image
// ...
// (Insert your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing method.)
// Select test image 1
camera.Parameters[PLCamera.TestImageSelector].SetValue(PLCamera.TestImageSelector.Testimage1);
// Acquire images to display the selected test image
// ...
// (Insert your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing method.)
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select test image 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TestImageSelector", "Testimage1");
CHECK(errRes);
/* Acquire images to display the selected test image */
/* ... */
/* (Insert your own image grabbing routine here. */
/* For example, the InstantCamera class provides the StartGrabbing method.) */
# Select test image 1
camera.TestImageSelector.Value = "Testimage1"
# Acquire images to display the selected test image
# ...
# (Insert your own image grabbing routine here.
# For example, the InstantCamera class provides the StartGrabbing method.)

You can also use the pylon Viewer to easily set the parameters.