Skip to content

Acquisition Frame Rate (blaze)#

The Acquisition Frame Rate feature available on blaze cameras allows you to set an upper limit for the camera's frame rate.

This is useful if you want to operate the camera at a constant frame rate in free run image acquisition.

Using the Feature#

How It Works#

If the Acquisition Frame Rate feature is enabled, the camera's maximum frame rate is limited by the value you enter for the acquisition frame rate parameter.

For example, setting an acquisition frame rate of 20 frames per second (fps) has the following effects:

  • If the other factors limiting the frame rate allow a frame rate of more than 20 fps, the frame rate will be kept at a constant frame rate of 20 fps.
  • If the other factors limiting the frame rate only allow a frame rate of less than 20 fps, the frame rate won't be affected by the Acquisition Frame Rate feature.

Setting the Acquisition Frame Rate#

  1. Set the AcquisitionFrameRateEnable parameter to true.
  2. Set the AcquisitionFrameRate parameter to the desired upper limit for the camera's frame rate in frames per second.