Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Overlapping Image Acquisition#

With overlapping image acquisition, the exposure of a new image begins while the camera is still reading out the sensor data of the previous image.

This is useful if you want to increase the frame rate of your camera.

How It Works#

Non-Overlapping Image Acquisition#

Whenever the camera is able to complete the entire image acquisition process (exposure + readout) before the next image acquisition starts, images will not overlap.

On global shutter cameras, non-overlapping image acquisition looks like this (using Trigger Width exposure mode as an example):

Non-Overlapped Mode of Operation (Global Shutter Cameras)

On rolling shutter cameras, non-overlapping image acquisition looks like this (using Timed exposure mode as an example):

Non-Overlapped Mode of Operation (Rolling Shutter Cameras)

Overlapping Image Acquisition#

With overlapping image acquisition, the camera exposes a new image while still reading out the sensor data of the previous image.

This is useful if you want to increase the frame rate of your camera.

On global shutter cameras, overlapping image acquisition looks like this (using Trigger Width exposure mode as an example):

Overlapped Mode of Operation (Global Shutter Cameras)

On rolling shutter cameras, overlapping image acquisition looks like this (using Timed exposure mode as an example):

Overlapped Mode of Operation (Rolling Shutter Cameras)

Enabling Overlapping Image Acquisition#

Automatic#

On most camera models, overlapping image acquisition is enabled automatically. This means that there's no camera parameter that allows you to turn overlapping image acquisition on or off. Instead, the way that you operate the camera determines whether image acquisitions are overlapped.

Image acquisitions are overlapped if the following condition applies:

Frame Period ≤ Exposure Time + Sensor Readout Time

  • Frame Period: Period of time from the start of one image acquisition to the start of the next image acquisition.
  • Exposure Time:
  • Sensor Readout Time: Time it takes to read out the data of an image from the sensor. If available, you can use the Sensor Readout Time feature to get the value.

Info

Additional conditions may apply, e.g., overlapping image acquisition may only be available in free run acquisition mode.

If the camera is configured for free run image acquisition, overlapping image acquisitions occur automatically.

If the camera is configured for triggered image acquisition, overlapping image acquisitions occur whenever you trigger the camera at a sufficiently high rate.

Manual#

On some camera models, you can manually enable or disable overlapping image acquisition. To do so, set the OverlapMode parameter to one of the following values:

  • On: Enables overlapping image acquisition. The camera automatically overlaps exposures and readouts.
  • Off: Disables overlapping image acquisition. The camera never overlaps exposures and readouts. This can improve image quality, especially when you are operating the camera at low frame rates.

Info

  • Basler recommends setting the OverlapMode parameter to Off whenever the acquisition mode is set to Continuous and you are acquiring less than 10 frames per second.
  • Additional conditions may apply, e.g., overlapping image acquisition may only be available in free run acquisition mode.

Avoiding Overtriggering#

Global Shutter Cameras#

If you want to use overlapping image acquisition on global shutter cameras operating in Trigger Width exposure mode, the following guideline applies:

You must not stop the exposure of the current frame until readout of the previously acquired frame is complete.

If you violate this guideline, the camera drops the current frame and declares a Frame Start Overtrigger event.

Overtriggering with Overlapping Image Acquisition

You can avoid violating this guideline by monitoring the camera's Frame Trigger Wait signal and by specifying an appropriate value for the Exposure Overlap Time Max parameter.

Specifics#

Show all camera models

Camera Model Overlapping Image Acquisition Availability Enabling Overlapping Image Acquisition
a2A640-240gmSWIR Always (free run and triggered image acquisition) Automatic
a2A640-240umSWIR Always (free run and triggered image acquisition) Automatic
a2A1280-80gmSWIR Always (free run and triggered image acquisition) Automatic
a2A1280-125umSWIR Always (free run and triggered image acquisition) Automatic
a2A1920-51gcBAS Always (free run and triggered image acquisition) Automatic
a2A1920-51gcIP67 Always (free run and triggered image acquisition) Automatic
a2A1920-51gcPRO Always (free run and triggered image acquisition) Automatic
a2A1920-51gmBAS Always (free run and triggered image acquisition) Automatic
a2A1920-51gmIP67 Always (free run and triggered image acquisition) Automatic
a2A1920-51gmPRO Always (free run and triggered image acquisition) Automatic
a2A1920-160ucBAS Always (free run and triggered image acquisition) Automatic
a2A1920-160ucPRO Always (free run and triggered image acquisition) Automatic
a2A1920-160umBAS Always (free run and triggered image acquisition) Automatic
a2A1920-160umPRO Always (free run and triggered image acquisition) Automatic
a2A1920-165g5cBAS Always (free run and triggered image acquisition) Automatic
a2A1920-165g5mBAS Always (free run and triggered image acquisition) Automatic
a2A1920-168mgc Always (free run and triggered image acquisition) Automatic
a2A1920-168mgm Always (free run and triggered image acquisition) Automatic
a2A2048-35gmSWIR Always (free run and triggered image acquisition) Automatic
a2A2048-37gcBAS Always (free run and triggered image acquisition) Automatic
a2A2048-37gcPRO Always (free run and triggered image acquisition) Automatic
a2A2048-37gmBAS Always (free run and triggered image acquisition) Automatic
a2A2048-37gmPRO Always (free run and triggered image acquisition) Automatic
a2A2048-110umSWIR Always (free run and triggered image acquisition) Automatic
a2A2048-114g5cBAS Always (free run and triggered image acquisition) Automatic
a2A2048-114g5mBAS Always (free run and triggered image acquisition) Automatic
a2A2048-114mgc Always (free run and triggered image acquisition) Automatic
a2A2048-114mgm Always (free run and triggered image acquisition) Automatic
a2A2048-114ucBAS Always (free run and triggered image acquisition) Automatic
a2A2048-114ucPRO Always (free run and triggered image acquisition) Automatic
a2A2048-114umBAS Always (free run and triggered image acquisition) Automatic
a2A2048-114umPRO Always (free run and triggered image acquisition) Automatic
a2A2048-173cmSWIR Always (free run and triggered image acquisition) Automatic
a2A2440-98g5cBAS Always (free run and triggered image acquisition) Automatic
a2A2440-98g5mBAS Always (free run and triggered image acquisition) Automatic
a2A2448-23gcBAS Always (free run and triggered image acquisition) Automatic
a2A2448-23gcIP67 Always (free run and triggered image acquisition) Automatic
a2A2448-23gcPRO Always (free run and triggered image acquisition) Automatic
a2A2448-23gmBAS Always (free run and triggered image acquisition) Automatic
a2A2448-23gmIP67 Always (free run and triggered image acquisition) Automatic
a2A2448-23gmPRO Always (free run and triggered image acquisition) Automatic
a2A2448-75ucBAS Always (free run and triggered image acquisition) Automatic
a2A2448-75ucPRO Always (free run and triggered image acquisition) Automatic
a2A2448-75umBAS Always (free run and triggered image acquisition) Automatic
a2A2448-75umPRO Always (free run and triggered image acquisition) Automatic
a2A2448-90mgc Always (free run and triggered image acquisition) Automatic
a2A2448-90mgm Always (free run and triggered image acquisition) Automatic
a2A2448-105g5cBAS Always (free run and triggered image acquisition) Automatic
a2A2448-105g5mBAS Always (free run and triggered image acquisition) Automatic
a2A2448-120cc Always (free run and triggered image acquisition) Automatic
a2A2448-120cm Always (free run and triggered image acquisition) Automatic
a2A2448-210cc Always (free run and triggered image acquisition) Automatic
a2A2448-210cm Always (free run and triggered image acquisition) Automatic
a2A2448-232g10c Always (free run and triggered image acquisition) Automatic
a2A2448-232g10m Always (free run and triggered image acquisition) Automatic
a2A2464-23gcBAS Always (free run and triggered image acquisition) Automatic
a2A2464-23gcPRO Always (free run and triggered image acquisition) Automatic
a2A2464-23gmBAS Always (free run and triggered image acquisition) Automatic
a2A2464-23gmPRO Always (free run and triggered image acquisition) Automatic
a2A2464-77ucBAS Always (free run and triggered image acquisition) Automatic
a2A2464-77ucPRO Always (free run and triggered image acquisition) Automatic
a2A2464-77umBAS Always (free run and triggered image acquisition) Automatic
a2A2464-77umPRO Always (free run and triggered image acquisition) Automatic
a2A2464-115g5cBAS Always (free run and triggered image acquisition) Automatic
a2A2464-115g5mBAS Always (free run and triggered image acquisition) Automatic
a2A2560-20gmSWIR Always (free run and triggered image acquisition) Automatic
a2A2560-70umSWIR Always (free run and triggered image acquisition) Automatic
a2A2560-131cmSWIR Always (free run and triggered image acquisition) Automatic
a2A2590-22gcBAS Only when the camera is configured for free run image acquisition. Automatic
a2A2590-22gcPRO Only when the camera is configured for free run image acquisition. Automatic
a2A2590-22gmBAS Only when the camera is configured for free run image acquisition. Automatic
a2A2590-22gmPRO Only when the camera is configured for free run image acquisition. Automatic
a2A2590-60ucBAS Only when the camera is configured for free run image acquisition. Automatic
a2A2590-60ucPRO Only when the camera is configured for free run image acquisition. Automatic
a2A2590-60umBAS Only when the camera is configured for free run image acquisition. Automatic
a2A2590-60umPRO Only when the camera is configured for free run image acquisition. Automatic
a2A2600-20gcBAS Always (free run and triggered image acquisition) Automatic
a2A2600-20gcPRO Always (free run and triggered image acquisition) Automatic
a2A2600-20gmBAS Always (free run and triggered image acquisition) Automatic
a2A2600-20gmPRO Always (free run and triggered image acquisition) Automatic
a2A2600-64ucBAS Always (free run and triggered image acquisition) Automatic
a2A2600-64ucPRO Always (free run and triggered image acquisition) Automatic
a2A2600-64umBAS Always (free run and triggered image acquisition) Automatic
a2A2600-64umPRO Always (free run and triggered image acquisition) Automatic
a2A2840-14gcBAS Always (free run and triggered image acquisition) Automatic
a2A2840-14gcIP67 Always (free run and triggered image acquisition) Automatic
a2A2840-14gcPRO Always (free run and triggered image acquisition) Automatic
a2A2840-14gmBAS Always (free run and triggered image acquisition) Automatic
a2A2840-14gmIP67 Always (free run and triggered image acquisition) Automatic
a2A2840-14gmPRO Always (free run and triggered image acquisition) Automatic
a2A2840-14gmUV Always (free run and triggered image acquisition) Automatic
a2A2840-48ucBAS Always (free run and triggered image acquisition) Automatic
a2A2840-48ucPRO Always (free run and triggered image acquisition) Automatic
a2A2840-48umBAS Always (free run and triggered image acquisition) Automatic
a2A2840-48umPRO Always (free run and triggered image acquisition) Automatic
a2A2840-48umUV Always (free run and triggered image acquisition) Automatic
a2A2840-57mgc Always (free run and triggered image acquisition) Automatic
a2A2840-57mgm Always (free run and triggered image acquisition) Automatic
a2A2840-67g5cBAS Always (free run and triggered image acquisition) Automatic
a2A2840-67g5mBAS Always (free run and triggered image acquisition) Automatic
a2A2840-67g5mUV Always (free run and triggered image acquisition) Automatic
a2A2840-86cc Always (free run and triggered image acquisition) Automatic
a2A2840-86cm Always (free run and triggered image acquisition) Automatic
a2A2840-150g10c Always (free run and triggered image acquisition) Automatic
a2A2840-150g10m Always (free run and triggered image acquisition) Automatic
a2A2840-150g10mUV Always (free run and triggered image acquisition) Automatic
a2A3536-9gcBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3536-9gcPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3536-9gmBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3536-9gmPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3536-31ucBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3536-31ucPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3536-31umBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3536-31umPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3536-37mgc Always (free run and triggered image acquisition) Automatic
a2A3536-37mgm Always (free run and triggered image acquisition) Automatic
a2A3536-42g5cBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3536-42g5mBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3840-13gcBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3840-13gcPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3840-13gmBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3840-13gmPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3840-45ucBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3840-45ucPRO Only when the camera is configured for free run image acquisition. Automatic
a2A3840-45umBAS Only when the camera is configured for free run image acquisition. Automatic
a2A3840-45umPRO Only when the camera is configured for free run image acquisition. Automatic
a2A4096-9gcBAS Always (free run and triggered image acquisition) Automatic
a2A4096-9gcIP67 Always (free run and triggered image acquisition) Automatic
a2A4096-9gcPRO Always (free run and triggered image acquisition) Automatic
a2A4096-9gmBAS Always (free run and triggered image acquisition) Automatic
a2A4096-9gmIP67 Always (free run and triggered image acquisition) Automatic
a2A4096-9gmPRO Always (free run and triggered image acquisition) Automatic
a2A4096-30ucBAS Always (free run and triggered image acquisition) Automatic
a2A4096-30ucPRO Always (free run and triggered image acquisition) Automatic
a2A4096-30umBAS Always (free run and triggered image acquisition) Automatic
a2A4096-30umPRO Always (free run and triggered image acquisition) Automatic
a2A4096-38mgc Always (free run and triggered image acquisition) Automatic
a2A4096-38mgm Always (free run and triggered image acquisition) Automatic
a2A4096-44g5cBAS Always (free run and triggered image acquisition) Automatic
a2A4096-44g5mBAS Always (free run and triggered image acquisition) Automatic
a2A4096-67cc Always (free run and triggered image acquisition) Automatic
a2A4096-67cm Always (free run and triggered image acquisition) Automatic
a2A4096-98g10c Always (free run and triggered image acquisition) Automatic
a2A4096-98g10m Always (free run and triggered image acquisition) Automatic
a2A4200-12gcBAS Always (free run and triggered image acquisition) Automatic
a2A4200-12gcPRO Always (free run and triggered image acquisition) Automatic
a2A4200-12gmBAS Always (free run and triggered image acquisition) Automatic
a2A4200-12gmPRO Always (free run and triggered image acquisition) Automatic
a2A4200-40ucBAS Always (free run and triggered image acquisition) Automatic
a2A4200-40ucPRO Always (free run and triggered image acquisition) Automatic
a2A4200-40umBAS Always (free run and triggered image acquisition) Automatic
a2A4200-40umPRO Always (free run and triggered image acquisition) Automatic
a2A4504-5gcBAS Always (free run and triggered image acquisition) Automatic
a2A4504-5gcIP67 Always (free run and triggered image acquisition) Automatic
a2A4504-5gcPRO Always (free run and triggered image acquisition) Automatic
a2A4504-5gmBAS Always (free run and triggered image acquisition) Automatic
a2A4504-5gmIP67 Always (free run and triggered image acquisition) Automatic
a2A4504-5gmPRO Always (free run and triggered image acquisition) Automatic
a2A4504-18ucBAS Always (free run and triggered image acquisition) Automatic
a2A4504-18ucPRO Always (free run and triggered image acquisition) Automatic
a2A4504-18umBAS Always (free run and triggered image acquisition) Automatic
a2A4504-18umPRO Always (free run and triggered image acquisition) Automatic
a2A4504-23mgc Always (free run and triggered image acquisition) Automatic
a2A4504-23mgm Always (free run and triggered image acquisition) Automatic
a2A4504-27g5cBAS Always (free run and triggered image acquisition) Automatic
a2A4504-27g5mBAS Always (free run and triggered image acquisition) Automatic
a2A4504-42cc Always (free run and triggered image acquisition) Automatic
a2A4504-42cm Always (free run and triggered image acquisition) Automatic
a2A4504-59g10c Always (free run and triggered image acquisition) Automatic
a2A4504-59g10m Always (free run and triggered image acquisition) Automatic
a2A4508-6gcBAS Always (free run and triggered image acquisition) Automatic
a2A4508-6gcPRO Always (free run and triggered image acquisition) Automatic
a2A4508-6gmBAS Always (free run and triggered image acquisition) Automatic
a2A4508-6gmPRO Always (free run and triggered image acquisition) Automatic
a2A4508-20ucBAS Always (free run and triggered image acquisition) Automatic
a2A4508-20ucPRO Always (free run and triggered image acquisition) Automatic
a2A4508-20umBAS Always (free run and triggered image acquisition) Automatic
a2A4508-20umPRO Always (free run and triggered image acquisition) Automatic
a2A5060-4gcBAS Always (free run and triggered image acquisition) Automatic
a2A5060-4gmBAS Always (free run and triggered image acquisition) Automatic
a2A5060-15ucBAS Always (free run and triggered image acquisition) Automatic
a2A5060-15umBAS Always (free run and triggered image acquisition) Automatic
a2A5060-21g5cBAS Always (free run and triggered image acquisition) Automatic
a2A5060-21g5mBAS Always (free run and triggered image acquisition) Automatic
a2A5060-35cc Always (free run and triggered image acquisition) Automatic
a2A5060-35cm Always (free run and triggered image acquisition) Automatic
a2A5320-7gcBAS Always (free run and triggered image acquisition) Automatic
a2A5320-7gcIP67 Always (free run and triggered image acquisition) Automatic
a2A5320-7gcPRO Always (free run and triggered image acquisition) Automatic
a2A5320-7gmBAS Always (free run and triggered image acquisition) Automatic
a2A5320-7gmPRO Always (free run and triggered image acquisition) Automatic
a2A5320-7gmip67 Always (free run and triggered image acquisition) Automatic
a2A5320-23ucBAS Always (free run and triggered image acquisition) Automatic
a2A5320-23ucPRO Always (free run and triggered image acquisition) Automatic
a2A5320-23umBAS Always (free run and triggered image acquisition) Automatic
a2A5320-23umPRO Always (free run and triggered image acquisition) Automatic
a2A5320-29mgc Always (free run and triggered image acquisition) Automatic
a2A5320-29mgm Always (free run and triggered image acquisition) Automatic
a2A5320-34g5cBAS Always (free run and triggered image acquisition) Automatic
a2A5320-34g5mBAS Always (free run and triggered image acquisition) Automatic
a2A5320-52cc Always (free run and triggered image acquisition) Automatic
a2A5320-52cm Always (free run and triggered image acquisition) Automatic
a2A5320-75g10c Always (free run and triggered image acquisition) Automatic
a2A5320-75g10m Always (free run and triggered image acquisition) Automatic
a2A5328-4gcBAS Always (free run and triggered image acquisition) Automatic
a2A5328-4gcIP67 Always (free run and triggered image acquisition) Automatic
a2A5328-4gcPRO Always (free run and triggered image acquisition) Automatic
a2A5328-4gmBAS Always (free run and triggered image acquisition) Automatic
a2A5328-4gmIP67 Always (free run and triggered image acquisition) Automatic
a2A5328-4gmPRO Always (free run and triggered image acquisition) Automatic
a2A5328-15ucBAS Always (free run and triggered image acquisition) Automatic
a2A5328-15ucPRO Always (free run and triggered image acquisition) Automatic
a2A5328-15umBAS Always (free run and triggered image acquisition) Automatic
a2A5328-15umPRO Always (free run and triggered image acquisition) Automatic
a2A5328-19mgc Always (free run and triggered image acquisition) Automatic
a2A5328-19mgm Always (free run and triggered image acquisition) Automatic
a2A5328-22g5cBAS Always (free run and triggered image acquisition) Automatic
a2A5328-22g5mBAS Always (free run and triggered image acquisition) Automatic
a2A5328-35cc Always (free run and triggered image acquisition) Automatic
a2A5328-35cm Always (free run and triggered image acquisition) Automatic
a2A5328-49g10c Always (free run and triggered image acquisition) Automatic
a2A5328-49g10m Always (free run and triggered image acquisition) Automatic
acA640-121gm Always (free run and triggered image acquisition) Automatic
acA640-300gc Always (free run and triggered image acquisition) Automatic
acA640-300gm Always (free run and triggered image acquisition) Automatic
acA640-750uc Always (free run and triggered image acquisition) Automatic
acA640-750um Always (free run and triggered image acquisition) Automatic
acA720-290gc Always (free run and triggered image acquisition) Automatic
acA720-290gm Always (free run and triggered image acquisition) Automatic
acA720-520uc Always (free run and triggered image acquisition) Automatic
acA720-520um Always (free run and triggered image acquisition) Automatic
acA800-200gc Always (free run and triggered image acquisition) Automatic
acA800-200gm Always (free run and triggered image acquisition) Automatic
acA800-510uc Always (free run and triggered image acquisition) Automatic
acA800-510um Always (free run and triggered image acquisition) Automatic
acA1280-60gc Only when the camera is configured for free run image acquisition. Automatic
acA1280-60gm Only when the camera is configured for free run image acquisition. Automatic
acA1300-60gc Only when the camera is configured for free run image acquisition. Automatic
acA1300-60gm Only when the camera is configured for free run image acquisition. Automatic
acA1300-60gmNIR Only when the camera is configured for free run image acquisition. Automatic
acA1300-75gc Always (free run and triggered image acquisition) Automatic
acA1300-75gm Always (free run and triggered image acquisition) Automatic
acA1300-200uc Always (free run and triggered image acquisition) Automatic
acA1300-200um Always (free run and triggered image acquisition) Automatic
acA1440-73gc Always (free run and triggered image acquisition) Automatic
acA1440-73gm Always (free run and triggered image acquisition) Automatic
acA1440-220uc Always (free run and triggered image acquisition) Automatic
acA1440-220um Always (free run and triggered image acquisition) Automatic
acA1600-60gc Only when the camera is configured for free run image acquisition. Automatic
acA1600-60gm Only when the camera is configured for free run image acquisition. Automatic
acA1920-25gc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA1920-25gm Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA1920-25uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA1920-25um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA1920-40gc Always (free run and triggered image acquisition) Automatic
acA1920-40gm Always (free run and triggered image acquisition) Automatic
acA1920-40uc Always (free run and triggered image acquisition) Automatic
acA1920-40ucMED Only when the Standard camera operation mode is enabled. Automatic
acA1920-40um Always (free run and triggered image acquisition) Automatic
acA1920-40umMED Only when the Standard camera operation mode is enabled. Automatic
acA1920-48gc Always (free run and triggered image acquisition) Automatic
acA1920-48gm Always (free run and triggered image acquisition) Automatic
acA1920-50gc Always (free run and triggered image acquisition) Automatic
acA1920-50gm Always (free run and triggered image acquisition) Automatic
acA1920-150uc Always (free run and triggered image acquisition) Automatic
acA1920-150um Always (free run and triggered image acquisition) Automatic
acA1920-155uc Always (free run and triggered image acquisition) Automatic
acA1920-155ucMED Only when the Standard camera operation mode is enabled. Automatic
acA1920-155um Always (free run and triggered image acquisition) Automatic
acA1920-155umMED Only when the Standard camera operation mode is enabled. Automatic
acA2000-50gc Always (free run and triggered image acquisition) Automatic
acA2000-50gm Always (free run and triggered image acquisition) Automatic
acA2000-165uc Always (free run and triggered image acquisition) Automatic
acA2000-165um Always (free run and triggered image acquisition) Automatic
acA2040-25gc Always (free run and triggered image acquisition) Automatic
acA2040-25gm Always (free run and triggered image acquisition) Automatic
acA2040-25gmNIR Always (free run and triggered image acquisition) Automatic
acA2040-35gc Always (free run and triggered image acquisition) Automatic
acA2040-35gm Always (free run and triggered image acquisition) Automatic
acA2040-55uc Always (free run and triggered image acquisition) Automatic
acA2040-55um Always (free run and triggered image acquisition) Automatic
acA2040-90uc Always (free run and triggered image acquisition) Automatic
acA2040-90um Always (free run and triggered image acquisition) Automatic
acA2040-90umNIR Always (free run and triggered image acquisition) Automatic
acA2040-120uc Always (free run and triggered image acquisition) Automatic
acA2040-120um Always (free run and triggered image acquisition) Automatic
acA2440-20gc Always (free run and triggered image acquisition) Automatic
acA2440-20gm Always (free run and triggered image acquisition) Automatic
acA2440-35uc Always (free run and triggered image acquisition) Automatic
acA2440-35ucMED Only when the Standard camera operation mode is enabled. Automatic
acA2440-35um Always (free run and triggered image acquisition) Automatic
acA2440-35umMED Only when the Standard camera operation mode is enabled. Automatic
acA2440-75uc Always (free run and triggered image acquisition) Automatic
acA2440-75ucMED Only when the Standard camera operation mode is enabled. Automatic
acA2440-75um Always (free run and triggered image acquisition) Automatic
acA2440-75umMED Only when the Standard camera operation mode is enabled. Automatic
acA2500-14gc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA2500-14gm Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA2500-14uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA2500-14um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA2500-20gc Always (free run and triggered image acquisition) Automatic
acA2500-20gcMED Always (free run and triggered image acquisition) Automatic
acA2500-20gm Always (free run and triggered image acquisition) Automatic
acA2500-20gmMED Always (free run and triggered image acquisition) Automatic
acA2500-60uc Always (free run and triggered image acquisition) Automatic
acA2500-60um Always (free run and triggered image acquisition) Automatic
acA3088-16gc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3088-16gm Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3088-57uc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3088-57ucMED Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA3088-57um Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3088-57umMED Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
acA3800-10gc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3800-10gm Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3800-14uc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA3800-14um Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA4024-8gc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA4024-8gm Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA4024-29uc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA4024-29um Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA4096-11gc Always (free run and triggered image acquisition) Automatic
acA4096-11gm Always (free run and triggered image acquisition) Automatic
acA4096-30uc Always (free run and triggered image acquisition) Automatic
acA4096-30ucMED Always (free run and triggered image acquisition) Automatic
acA4096-30um Always (free run and triggered image acquisition) Automatic
acA4096-30umMED Always (free run and triggered image acquisition) Automatic
acA4096-40uc Always (free run and triggered image acquisition) Automatic
acA4096-40ucMED Always (free run and triggered image acquisition) Automatic
acA4096-40um Always (free run and triggered image acquisition) Automatic
acA4096-40umMED Always (free run and triggered image acquisition) Automatic
acA4112-8gc Always (free run and triggered image acquisition) Automatic
acA4112-8gm Always (free run and triggered image acquisition) Automatic
acA4112-20uc Always (free run and triggered image acquisition) Automatic
acA4112-20ucMED Always (free run and triggered image acquisition) Automatic
acA4112-20um Always (free run and triggered image acquisition) Automatic
acA4112-20umMED Always (free run and triggered image acquisition) Automatic
acA4112-30uc Always (free run and triggered image acquisition) Automatic
acA4112-30ucMED Always (free run and triggered image acquisition) Automatic
acA4112-30um Always (free run and triggered image acquisition) Automatic
acA4112-30umMED Always (free run and triggered image acquisition) Automatic
acA5472-5gc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA5472-5gm Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA5472-17uc Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA5472-17ucMED Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA5472-17um Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
acA5472-17umMED Only when the camera is configured for free run image acquisition and the shutter mode is set to Rolling. Automatic
boA1936-400cc Always (free run and triggered image acquisition) Automatic
boA1936-400cm Always (free run and triggered image acquisition) Automatic
boA2448-250cc Always (free run and triggered image acquisition) Automatic
boA2448-250cm Always (free run and triggered image acquisition) Automatic
boA2832-190cc Always (free run and triggered image acquisition) Automatic
boA2832-190cm Always (free run and triggered image acquisition) Automatic
boA4096-93cc Always (free run and triggered image acquisition) Automatic
boA4096-93cm Always (free run and triggered image acquisition) Automatic
boA4096-180cc Always (free run and triggered image acquisition) Automatic
boA4096-180cm Always (free run and triggered image acquisition) Automatic
boA4112-68cc Always (free run and triggered image acquisition) Automatic
boA4112-68cm Always (free run and triggered image acquisition) Automatic
boA4500-45cc Always (free run and triggered image acquisition) Automatic
boA4500-45cm Always (free run and triggered image acquisition) Automatic
boA4504-100cc Always (free run and triggered image acquisition) Automatic
boA4504-100cm Always (free run and triggered image acquisition) Automatic
boA5056-95cm Always (free run and triggered image acquisition) Automatic
boA5120-150cc Always (free run and triggered image acquisition) Automatic
boA5120-150cm Always (free run and triggered image acquisition) Automatic
boA5120-230cc Always (free run and triggered image acquisition) Automatic
boA5120-230cm Always (free run and triggered image acquisition) Automatic
boA5320-150cc Always (free run and triggered image acquisition) Automatic
boA5320-150cm Always (free run and triggered image acquisition) Automatic
boA5328-100cc Always (free run and triggered image acquisition) Automatic
boA5328-100cm Always (free run and triggered image acquisition) Automatic
boA6500-36cc Always (free run and triggered image acquisition) Automatic
boA6500-36cm Always (free run and triggered image acquisition) Automatic
boA8100-16cc Always (free run and triggered image acquisition) Automatic
boA8100-16cm Always (free run and triggered image acquisition) Automatic
boA9344-30cc Always (free run and triggered image acquisition) Automatic
boA9344-30cm Always (free run and triggered image acquisition) Automatic
boA9344-70cc Always (free run and triggered image acquisition) Automatic
boA9344-70cm Always (free run and triggered image acquisition) Automatic
boA13440-17cm Always (free run and triggered image acquisition) Automatic
daA720-520uc Always (free run and triggered image acquisition) Automatic
daA720-520um Always (free run and triggered image acquisition) Automatic
daA1280-54uc Only when the camera is configured for free run image acquisition. Manual
daA1280-54um Only when the camera is configured for free run image acquisition. Manual
daA1440-220uc Always (free run and triggered image acquisition) Automatic
daA1440-220um Always (free run and triggered image acquisition) Automatic
daA1600-60uc Only when the camera is configured for free run image acquisition. Manual
daA1600-60um Only when the camera is configured for free run image acquisition. Manual
daA1920-15um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
daA1920-30uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
daA1920-30um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
daA1920-160uc Always (free run and triggered image acquisition) Automatic
daA1920-160um Always (free run and triggered image acquisition) Automatic
daA2448-70uc Always (free run and triggered image acquisition) Automatic
daA2448-70um Always (free run and triggered image acquisition) Automatic
daA2500-14uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
daA2500-14um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
daA3840-45uc Only when the camera is configured for free run image acquisition. Automatic
daA3840-45um Only when the camera is configured for free run image acquisition. Automatic
dmA720-290gc Always (free run and triggered image acquisition) Automatic
dmA720-290gm Always (free run and triggered image acquisition) Automatic
dmA1440-73gc Always (free run and triggered image acquisition) Automatic
dmA1440-73gm Always (free run and triggered image acquisition) Automatic
dmA1920-51gc Always (free run and triggered image acquisition) Automatic
dmA1920-51gm Always (free run and triggered image acquisition) Automatic
dmA2048-37gc Always (free run and triggered image acquisition) Automatic
dmA2048-37gm Always (free run and triggered image acquisition) Automatic
dmA2448-23gc Always (free run and triggered image acquisition) Automatic
dmA2448-23gm Always (free run and triggered image acquisition) Automatic
dmA2840-14gc Always (free run and triggered image acquisition) Automatic
dmA2840-14gm Always (free run and triggered image acquisition) Automatic
dmA3536-9gc Only when the camera is configured for free run image acquisition. Automatic
dmA3536-9gm Only when the camera is configured for free run image acquisition. Automatic
dmA4096-9gc Always (free run and triggered image acquisition) Automatic
dmA4096-9gm Always (free run and triggered image acquisition) Automatic
puA1280-54uc Only when the camera is configured for free run image acquisition. Manual
puA1280-54um Only when the camera is configured for free run image acquisition. Manual
puA1600-60uc Only when the camera is configured for free run image acquisition. Manual
puA1600-60um Only when the camera is configured for free run image acquisition. Manual
puA1920-30uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
puA1920-30um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
puA2500-14uc Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
puA2500-14um Only when the shutter mode is set to Rolling, i.e., when Global Reset Release shutter mode is disabled. Automatic
r2L2048-29gc Always (free run and triggered image acquisition) Automatic
r2L2048-58gm Always (free run and triggered image acquisition) Automatic
r2L2048-62cc Always (free run and triggered image acquisition) Automatic
r2L2048-62g5c Always (free run and triggered image acquisition) Automatic
r2L2048-172cm Always (free run and triggered image acquisition) Automatic
r2L2048-172g5m Always (free run and triggered image acquisition) Automatic
r2L4096-14gc Always (free run and triggered image acquisition) Automatic
r2L4096-29gm Always (free run and triggered image acquisition) Automatic
r2L4096-42cc Always (free run and triggered image acquisition) Automatic
r2L4096-42g5c Always (free run and triggered image acquisition) Automatic
r2L4096-84cm Always (free run and triggered image acquisition) Automatic
r2L4096-84g5m Always (free run and triggered image acquisition) Automatic
r2L8192-80cc Always (free run and triggered image acquisition) Automatic
r2L8192-240cm Always (free run and triggered image acquisition) Automatic
r2L16384-60cc Always (free run and triggered image acquisition) Automatic
r2L16384-120cm Always (free run and triggered image acquisition) Automatic
r2T16416-500cm Always (free run and triggered image acquisition) Automatic