Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Using blaze Cameras#

This topic gives a step-by-step overview over how to get started with Basler blaze and Smart blaze cameras. It will show you how to configure the camera, acquire images, and process the resulting image data.

The easiest way to work with blaze cameras is via the blaze Viewer, which is installed as part of the pylon Supplementary Package for blaze.

Info

All information in this topic applies to all blaze and Smart blaze camera models. For sake of brevity, "blaze" is used to refer to all models.

Step-By-Step Instructions#

  1. Connect the camera to your computer.
    For information about installing the camera and the software, see Hardware Installation (blaze) and Software Installation (blaze). When Status and Ethernet LEDs are flashing green / solid green, the camera is ready to use. For more information, see the "LED States" section of your camera model topic.
  2. Start the blaze Viewer.
    Windows: Click Start > Basler > blaze Viewer.
    Linux: Issue the following command: /opt/pylon/bin/blazeViewer
    The camera appears in the camera selector drop-down list and image acquisition starts immediately.
    In the image window area, four windows open that show the different components.
    If the camera is not shown in the camera selector, this may be due to problems with the IP address.
  3. Configure the camera:

    1. Define the region of interest (ROI).
    2. Set the acquisition frame rate.
    3. Set the exposure time.
    4. Select the desired component(s).
    5. Select the desired pixel format(s).
    6. Select an operating mode.
    7. Enable fast mode if desired.
    8. Optimize the image quality settings if the resulting images are not satisfactory:

  4. Process the measurement results.

  5. Save the camera settings if desired.
    For more information about that, see Overview of the blaze Viewer.