Line Logic#
The logic of an I/O line can either be positive or negative.
Using the Feature#
Determining the Line Logic#
To determine the logic of an I/O line:
- Set the
LineSelectorparameter to the desired I/O line. - Get the value of the
LineLogicparameter.
This parameter is read-only.
Line Logic Overview#
Positive Line Logic#
If the line logic is positive, the relation between the electrical status of an I/O line and the LineStatus parameter is as follows:
| Electrical Status | LineStatus Parameter Value |
|---|---|
| Voltage level high | True |
| Voltage level low | False |
Negative Line Logic#
If the line logic is negative, the relation between the electrical status of an I/O line and the LineStatus parameter is as follows:
| Electrical Status | LineStatus Parameter Value |
|---|---|
| Voltage level high | False |
| Voltage level low | True |
Sample Code#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Select a line */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line1");
CHECK(errRes);
/* Get the logic of the line */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "LineLogic", e_str, &len);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.