Line Mode#
You can configure the line mode of any general purpose I/O line (GPIO line). For opto-coupled I/O lines, you can only determine the current line mode.
Using the Feature#
Configuring the Line Mode#
Configure the line mode only when the I/O lines are not in use. Otherwise, the camera may show unpredictable behavior.
Set the LineSelector parameter to the desired GPIO line.
Set the LineMode parameter to one of the following values:
Input: Configures the GPIO line as an input line.Output: Configures the GPIO line as an output line.InOut: If available, configures the GPIO line as an input-output line. This is used, e.g., for the Two-Wire Interface and the Light Control features.
Determining the Line Mode#
- Set the
LineSelectorparameter to the desired I/O line. - Get the value of the
LineModeparameter to determine the current line mode of the I/O line.
Sample Code#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Select GPIO line 3 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line3");
CHECK(errRes);
/* Set the line mode to Input */
errRes = PylonDeviceFeatureFromString(hdev, "LineMode", "Input");
CHECK(errRes);
/* Get the current line mode */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "LineMode", e_str, &len);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.