Shading Correction#
Shading correction is based on files that are stored on the camera and contain appropriate correction data. During image acquisition, these are applied to the original pixel values, which results in an improved image.
The Shading Correction feature is only available on racer 2 cameras.
Using the Feature#
How It Works#
DSNU and PRNU Correction#
Shading correction minimizes image artifacts caused by dark signal non-uniformities (DSNU) and photo response non-uniformities (PRNU). The following two types of shading correction are available on the camera:
-
DSNU correction: When the camera captures a line in complete darkness, all of the pixel values in the line should be near zero and they should be equal. In practice, slight variations in the performance of the pixels in the sensor will cause some variation in the pixel values output from the camera when the camera is capturing lines in darkness. DSNU correction corrects for this type of variation. It works by adding an individual gray value (offset) to each pixel value in the lines acquired.
-
PRNU correction: When the camera captures a line while being pointed at a bright, homogeneously illuminated surface, all of the pixel values in the line should be near their maximum gray value and they should be equal. In practice, slight variations in the performance of the pixels in the sensor as well as variations in the optics and in lighting will cause variations in the pixel values output from the camera. PRNU correction corrects for this type of variation. It works by applying an individual multiplier (gain) to each pixel value in the lines acquired.
Shading correction is a pixel-to-pixel calibration method, i.e., a correction value is calculated for each single pixel.
Info
You can set the camera to only perform DSNU correction, to only perform PRNU correction, or to perform both types of shading correction. If you perform both types of shading correction, the camera first performs DSNU correction, then PRNU correction.
Shading Correction Sets#
The correction values used for DSNU and PRNU correction are stored in files referred to as shading correction sets. There are the following two types:
-
Factory correction set: Contains correction values that were stored on the camera during the camera production process. The factory correction set can only reduce image artifacts caused by dark signal non-uniformities (DSNU).
-
User correction set: Contains correction values that must be created by the user and stored on the camera. Depending on your camera model, you can create up to 32 user correction sets.
Downloading a Shading Correction File#
Info
- Downloading your shading correction files is useful to back up your correction data.
- Basler strongly recommends to back up your correction files before performing a firmware update.
- Don't edit a downloaded shading correction file.
To download a shading correction file using the pylon Viewer:
- In the pylon Viewer, open the camera you want to download the shading correction data file from.
- In the Camera menu of the pylon Viewer, click File Access.
- In the Camera File drop-down box, select PRNU Correction or DSNU Correction depending on which file you want to download.
If there's no appropriate entry, downloading a shading correction file is not supported by your camera. - Click Download, navigate to the directory where you want to save the file, and enter the desired file name.
- Click Save.
- Close the Camera File Access dialog.
Uploading a Shading Correction File#
Info
- If you upload a user shading correction file to a camera, make sure that the selected correction set was created on the camera you load the correction data on.
- Basler strongly recommends not to upload a user shading correction file that has been edited.
To upload a user shading correction file using the pylon Viewer:
- In the pylon Viewer, open the camera you want to upload the shading correction data file to.
- In the Camera menu of the pylon Viewer, click File Access.
- In the Camera File drop-down box, select PRNU Correction or DSNU Correction.
If there's no PRNU Correction or DSNU Correction entry, uploading a correction file is not supported by your camera. - Click Upload and navigate to the file that you want to upload.
- Click Open.
- Close the Camera File Access dialog.
To apply the shading correction file after uploading, make sure that the BslShadingCorrectionMode parameter is set to User and the BslShadingCorrectionSetIndex parameter is set to the corresponding index number.
Shading Correction Mode#
The shading correction mode determines whether shading correction is based on the values stored in the factory or the user correction set.
To set the shading correction mode, set the BslShadingCorrectionMode parameter to one of the following values:
Factory(default): Shading correction is based on the values stored in the factory correction set.User: Shading correction is based on the values stored in the user correction set.Off: The camera does not perform shading corrections.
Creating a Shading Correction Set#
You need the following items before you start creating a user-defined shading correction set:
- An appropriate object to completely cover the lens, e.g., the lens cap
- A target with a uniform background, e.g., a white sheet of paper
Info
- For best results, adjust the optics, line rate, exposure time, gain, and camera temperature as you would for normal operation. Basler recommends acquiring the dark and bright field images in your actual application environment.
- racer 2 L cameras: In Dual (or Quad) Line sensor acquisition mode, the status of a shading correction set created in Single (or Dual) Line mode will be indicated as empty (
BslShadingCorrectionSetStatus= Empty), although correction data already exist in this set.
If you want to create a new shading correction set in Dual or Quad Line mode, check the index numbers of your correction sets created in the mode(s) with fewer lines. If an index number has already been taken, choose another number for your new set. Otherwise, the correction data will be overwritten and replaced by the new correction values.
DSNU Correction Set#
To create a shading correction set for DSNU correction:
- Prevent any light from hitting the camera's sensor, e.g., by placing a plastic cap on the lens.
- Set the
BslShadingCorrectionSelectorparameter toDSNU. - Set the
BslShadingCorrectionModeparameter toUser. - Set the
BslShadingCorrectionSetIndexparameter to the desired index number of the set to be created, e.g., 1. - Set the
BslShadingCorrectionROISelectorparameter to the desired shading correction ROI, e.g., ROI 1. - If desired, set the position and size of the shading correction ROI by using the following parameters:
BslShadingCorrectionROIOffsetX: Horizontal offset of the shading correction ROI from the left side of the sensor (in pixels).BslShadingCorrectionROIWidth: Width of the shading correction ROI (in pixels).
- Click the Continuous Shot button in the toolbar of the pylon Viewer to start image acquisition.
-
Execute the
BslShadingCorrectionSetCreatecommand to create a new shading correction set.
A total of 256 dark images are acquired and evaluated. The resulting DSNU correction data are generated, collected in the shading correction set defined, and saved to the camera's flash memory. If the shading correction set with, e.g., index number 1, already contains correction data, these are overwritten and replaced by the new correction values.Info
If a PRNU correction set is enabled while creating DSNU correction data, the PRNU correction values will be ignored for the calculation.
The created shading correction set is enabled automatically.
-
To verify the result of the shading correction set creation, get the value of the
BslShadingCorrectionSetCreateResultparameter.
PRNU Correction Set#
To create a shading correction set for PRNU correction:
- Illuminate the sensor homogeneously to 70 % saturation, e.g., by placing a white sheet of paper in the camera's entire field of view.
- Set the
BslShadingCorrectionSelectorparameter toPRNU. - Set the
BslShadingCorrectionModeparameter toUser. - Set the
BslShadingCorrectionSetIndexparameter to the desired index number of the set to be created, e.g., 2. - Set the
BslShadingCorrectionROISelectorparameter to the desired shading correction ROI, e.g., ROI 1. - If desired, set the position and size of the shading correction ROI by using the following parameters:
BslShadingCorrectionROIOffsetX: Horizontal offset of the shading correction ROI from the left side of the sensor (in pixels).BslShadingCorrectionROIWidth: Width of the shading correction ROI (in pixels).
- Click the Continuous Shot button in the toolbar of the pylon Viewer to start image acquisition.
-
Execute the
BslShadingCorrectionSetCreatecommand to create a new shading correction set.
A total of 256 bright images are acquired and evaluated. The resulting PRNU correction data are generated, collected in the shading correction set selected, and saved to the camera's flash memory. If the shading correction set with, e.g., index number 2, already contains correction data, these are overwritten and replaced by the new correction values.Info
If a DSNU correction set is enabled while creating PRNU correction data, the DSNU correction values are taken into account for the calculation.
The created shading correction set is enabled automatically.
-
To verify the result of the shading correction set creation, get the value of the
BslShadingCorrectionSetCreateResultparameter. - If required, adjust the target gray value for PRNU correction and repeat step 7. If you're using a color camera, adjust the target gray value for PRNU correction for each color channel separately and repeat step 7.
Adjusting the Target Gray Value for PRNU Correction#
During the creation of a PRNU correction set, the camera detects the maximum brightness value in the bright field image. However, you may want to adjust the relative target gray value of the sensor brightness you want to achieve. Possible reasons for this are, e.g.:
- Your shading correction set can't be created because the correction values are outside the allowed range.
- Bright spots on the image (e.g., caused by light reflections) result in a high maximum brightness value detected by the camera during the creation of the correction set. You may want to reduce this value, which is relevant for calculating the correction data, to improve your correction data.
To adjust the target gray value for PRNU correction:
- Set the
BslShadingCorrectionTargetSelectorparameter to one of the following values:All(mono cameras only): The target gray value is applied to all sensor lines.Red,Green,Blue(color cameras only): The target gray value is applied to the respective color channel.
- Set the
BslShadingCorrectionTargetValueparameter to the desired relative target gray value. - If you're using a color camera, repeat steps 1 and 2 to apply the desired target gray value to the other color channels.
Info
- The
BslShadingCorrectionTargetValueparameter can only be used when creating PRNU correction sets. - Only pixels with an absolute target gray value lower than the value of the maximum measured value are corrected.
- For racer 2 L cameras operated in Dual or Quad Line sensor acquisition mode, adjusting the target gray value may show unpredictable results. Use the Single Line mode and a mono pixel format instead.
Further parameters:
BslShadingCorrectionAbsoluteTargetValue: Absolute target value of the sensor brightness. This is the actual brightness value that has been calculated based on the sensor bit depth of your camera.BslShadingCorrectionMaximumMeasuredValue: Maximum brightness value detected by the camera during the creation of a PRNU correction set.
Enabling a Shading Correction Set#
To enable a shading correction set:
- Set the
BslShadingCorrectionModeparameter toUser, if you want to enable a user-defined correction set, or toFactory, if you want to enable the factory correction set. -
Set the
BslShadingCorrectionSetIndexparameter to the index number of the set to be used, e.g., index number 2.The shading correction set is enabled automatically.
-
To verify whether this process was successful, get the value of the
BslShadingCorrectionSetStatusparameter. If the value isOk, the shading set has been enabled successfully. The camera now performs shading correction based on the correction values in the shading correction set selected.
Info
Changing a shading correction set is possible during image acquisition. However, slight image artifacts may occur during that process.
Disabling Shading Correction#
To disable shading correction, set the BslShadingCorrectionMode parameter to Off.
Specifics#
The following table shows the number of shading sets available for racer 2 cameras.
| Camera Model | Max. Number of Lines Exposed per Acquisition | Available Number of Shading Corrections Sets |
|---|---|---|
| r2L2048-29gc | 3 | 10 |
| r2L2048-58gm | 1 | 32 |
| r2L2048-62g5c | 3 | 10 |
| r2L2048-62cc | 3 | 10 |
| r2L2048-172cm | 1 | 32 |
| r2L2048-172g5m | 1 | 32 |
| r2L4096-14gc | 2 | 16 |
| r2L4096-29gm | 1 | 32 |
| r2L4096-42cc | 2 | 16 |
| r2L4096-42g5c | 2 | 16 |
| r2L4096-84cm | 1 | 32 |
| r2L4096-84g5m | 1 | 16 |
| r2L8192-80cc | 3 | 10 |
| r2L8192-240cm | 4 | 8 |
| r2L16384-60cc | 2 | 16 |
| r2L16384-120cm | 2 | 16 |
| r2T16416-500cm | 1 | 32 |
Sample Code#
// Set the type of shading correction to DSNU
camera.BslShadingCorrectionSelector.SetValue(BslShadingCorrectionSelector_DSNU);
// Or for PRNU: Set the type of shading correction to PRNU
camera.BslShadingCorrectionSelector.SetValue(BslShadingCorrectionSelector_PRNU);
// Note: Valid for DSNU and PRNU:
// Set the shading correction mode to User
camera.BslShadingCorrectionMode.SetValue(BslShadingCorrectionMode_User);
// Set the desired index number of the set to be created
camera.BslShadingCorrectionSetIndex.SetValue(1);
// Set the shading correction ROI selector to ROI 1
camera.BslShadingCorrectionROISelector.SetValue(BslShadingCorrectionROISelector_ROI1);
// Set the offset X of the ROI to 0
camera.BslShadingCorrectionROIOffsetX.SetValue(0);
// Set the ROI width to 2048
camera.BslShadingCorrectionROIWidth.SetValue(2048);
// Note: Valid for PRNU only:
// Set the shading correction target selector to red
camera.BslShadingCorrectionTargetSelector.SetValue(BslShadingCorrectionTargetSelector_Red);
// Set the shading correction target value for red to 1000
camera.BslShadingCorrectionTargetValue.SetValue(1.0000);
// Set the shading correction target selector to green
camera.BslShadingCorrectionTargetSelector.SetValue(BslShadingCorrectionTargetSelector_Green);
// Set the shading correction target value for green to 1000
camera.BslShadingCorrectionTargetValue.SetValue(1.0000);
// Set the shading correction target selector to blue
camera.BslShadingCorrectionTargetSelector.SetValue(BslShadingCorrectionTargetSelector_Blue);
// Set the shading correction target value for blue to 1000
camera.BslShadingCorrectionTargetValue.SetValue(1.0000);
// Note: Valid for DSNU and PRNU:
// Create new shading correction data for the shading correction set selected
camera.BslShadingCorrectionSetCreate.Execute();
// Get the status of the shading correction set selected
BslShadingCorrectionSetStatus setStatus = camera.BslShadingCorrectionSetStatus.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Set the type of shading correction to DSNU
CEnumParameter(nodemap, "BslShadingCorrectionSelector").SetValue("DSNU");
// Or for PRNU: Set the type of shading correction to PRNU
CEnumParameter(nodemap, "BslShadingCorrectionSelector").SetValue("PRNU");
// Note: Valid for DSNU and PRNU:
// Set the shading correction mode to User
CEnumParameter(nodemap, "BslShadingCorrectionMode").SetValue("User");
// Set the desired index number of the set to be created
CIntegerParameter(nodemap, "BslShadingCorrectionSetIndex").SetValue(1);
// Set the shading correction ROI selector to ROI 1
CEnumParameter(nodemap, "BslShadingCorrectionROISelector").SetValue("ROI1");
// Set the offset X of the ROI to 0
CIntegerParameter(nodemap, "BslShadingCorrectionROIOffsetX").SetValue(0);
// Set the ROI width to 2048
CIntegerParameter(nodemap, "BslShadingCorrectionROIWidth").SetValue(2048);
// Note: Valid for PRNU only:
// Set the shading correction target selector to red
CEnumParameter(nodemap, "BslShadingCorrectionTargetSelector").SetValue("Red");
// Set the shading correction target value for red to 1000
CFloatParameter(nodemap, "BslShadingCorrectionTargetValue").SetValue(1.0000);
// Set the shading correction target selector to green
CEnumParameter(nodemap, "BslShadingCorrectionTargetSelector").SetValue("Green");
// Set the shading correction target value for green to 1000
CFloatParameter(nodemap, "BslShadingCorrectionTargetValue").SetValue(1.0000);
// Set the shading correction target selector to blue
CEnumParameter(nodemap, "BslShadingCorrectionTargetSelector").SetValue("Blue");
// Set the shading correction target value for blue to 1000
CFloatParameter(nodemap, "BslShadingCorrectionTargetValue").SetValue(1.0000);
// Note: Valid for DSNU and PRNU:
// Create new shading correction data for the shading correction set selected
CCommandParameter(nodemap, "BslShadingCorrectionSetCreate").Execute();
// Get the status of the shading correction set selected
String_t setStatus = CEnumParameter(nodemap, "BslShadingCorrectionSetStatus").GetValue();
// Set the type of shading correction to DSNU
camera.Parameters[PLCamera.BslShadingCorrectionSelector].SetValue(PLCamera.BslShadingCorrectionSelector.DSNU);
// Or for PRNU: Set the type of shading correction to PRNU
camera.Parameters[PLCamera.BslShadingCorrectionSelector].SetValue(PLCamera.BslShadingCorrectionSelector.PRNU);
// Note: Valid for DSNU and PRNU:
// Set the shading correction mode to User
camera.Parameters[PLCamera.BslShadingCorrectionMode].SetValue(PLCamera.BslShadingCorrectionMode.User);
// Set the desired index number of the set to be created
camera.Parameters[PLCamera.BslShadingCorrectionSetIndex].SetValue(1);
// Set the shading correction ROI selector to ROI 1
camera.Parameters[PLCamera.BslShadingCorrectionROISelector].SetValue(PLCamera.BslShadingCorrectionROISelector.ROI1);
// Set the offset X of the ROI to 0
camera.Parameters[PLCamera.BslShadingCorrectionROIOffsetX].SetValue(0);
// Set the ROI width to 2048
camera.Parameters[PLCamera.BslShadingCorrectionROIWidth].SetValue(2048);
// Note: Valid for PRNU only:
// Set the shading correction target selector to red
camera.Parameters[PLCamera.BslShadingCorrectionTargetSelector].SetValue(PLCamera.BslShadingCorrectionTargetSelector.Red);
// Set the shading correction target value for red to 1000
camera.Parameters[PLCamera.BslShadingCorrectionTargetValue].SetValue(1.0000);
// Set the shading correction target selector to green
camera.Parameters[PLCamera.BslShadingCorrectionTargetSelector].SetValue(PLCamera.BslShadingCorrectionTargetSelector.Green);
// Set the shading correction target value for green to 1000
camera.Parameters[PLCamera.BslShadingCorrectionTargetValue].SetValue(1.0000);
// Set the shading correction target selector to blue
camera.Parameters[PLCamera.BslShadingCorrectionTargetSelector].SetValue(PLCamera.BslShadingCorrectionTargetSelector.Blue);
// Set the shading correction target value for blue to 1000
camera.Parameters[PLCamera.BslShadingCorrectionTargetValue].SetValue(1.0000);
// Note: Valid for DSNU and PRNU:
// Create new shading correction data for the shading correction set selected
camera.Parameters[PLCamera.BslShadingCorrectionSetCreate].Execute();
// Get the status of the shading correction set selected
string setStatus = camera.Parameters[PLCamera.BslShadingCorrectionSetStatus].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char setStatus_str[64] = {0};
/* Set the type of shading correction to DSNU */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionSelector", "DSNU");
CHECK(errRes);
/* Or for PRNU: Set the type of shading correction to PRNU */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionSelector", "PRNU");
CHECK(errRes);
/* Note: Valid for DSNU and PRNU: */
/* Set the shading correction mode to User */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionMode", "User");
CHECK(errRes);
/* Set the desired index number of the set to be created */
errRes = PylonDeviceSetIntegerFeature(hdev, "BslShadingCorrectionSetIndex", 1);
CHECK(errRes);
/* Set the shading correction ROI selector to ROI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionROISelector", "ROI1");
CHECK(errRes);
/* Set the offset X of the ROI to 0 */
errRes = PylonDeviceSetIntegerFeature(hdev, "BslShadingCorrectionROIOffsetX", 0);
CHECK(errRes);
/* Set the ROI width to 2048 */
errRes = PylonDeviceSetIntegerFeature(hdev, "BslShadingCorrectionROIWidth", 2048);
CHECK(errRes);
/* Note: Valid for PRNU only: */
/* Set the shading correction target selector to red */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionTargetSelector", "Red");
CHECK(errRes);
/* Set the shading correction target value for red to 1000 */
errRes = PylonDeviceSetFloatFeature(hdev, "BslShadingCorrectionTargetValue", 1.0000);
CHECK(errRes);
/* Set the shading correction target selector to green */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionTargetSelector", "Green");
CHECK(errRes);
/* Set the shading correction target value for green to 1000 */
errRes = PylonDeviceSetFloatFeature(hdev, "BslShadingCorrectionTargetValue", 1.0000);
CHECK(errRes);
/* Set the shading correction target selector to blue */
errRes = PylonDeviceFeatureFromString(hdev, "BslShadingCorrectionTargetSelector", "Blue");
CHECK(errRes);
/* Set the shading correction target value for blue to 1000 */
errRes = PylonDeviceSetFloatFeature(hdev, "BslShadingCorrectionTargetValue", 1.0000);
CHECK(errRes);
/* Note: Valid for DSNU and PRNU: */
/* Create new shading correction data for the shading correction set selected */
errRes = PylonDeviceExecuteCommandFeature(hdev, "BslShadingCorrectionSetCreate");
CHECK(errRes);
/* Get the status of the shading correction set selected */
len = sizeof(setStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "BslShadingCorrectionSetStatus", setStatus_str, &len);
CHECK(errRes);
# Set the type of shading correction to DSNU
camera.BslShadingCorrectionSelector.Value = "DSNU"
# Or for PRNU: Set the type of shading correction to PRNU
camera.BslShadingCorrectionSelector.Value = "PRNU"
# Note: Valid for DSNU and PRNU:
# Set the shading correction mode to User
camera.BslShadingCorrectionMode.Value = "User"
# Set the desired index number of the set to be created
camera.BslShadingCorrectionSetIndex.Value = 1
# Set the shading correction ROI selector to ROI 1
camera.BslShadingCorrectionROISelector.Value = "ROI1"
# Set the offset X of the ROI to 0
camera.BslShadingCorrectionROIOffsetX.Value = 0
# Set the ROI width to 2048
camera.BslShadingCorrectionROIWidth.Value = 2048
# Note: Valid for PRNU only:
# Set the shading correction target selector to red
camera.BslShadingCorrectionTargetSelector.Value = "Red"
# Set the shading correction target value for red to 1000
camera.BslShadingCorrectionTargetValue.Value = 1.0000
# Set the shading correction target selector to green
camera.BslShadingCorrectionTargetSelector.Value = "Green"
# Set the shading correction target value for green to 1000
camera.BslShadingCorrectionTargetValue.Value = 1.0000
# Set the shading correction target selector to blue
camera.BslShadingCorrectionTargetSelector.Value = "Blue"
# Set the shading correction target value for blue to 1000
camera.BslShadingCorrectionTargetValue.Value = 1.0000
# Note: Valid for DSNU and PRNU:
# Create new shading correction data for the shading correction set selected
camera.BslShadingCorrectionSetCreate.Execute()
# Get the status of the shading correction set selected
setStatus = camera.BslShadingCorrectionSetStatus.Value
You can also use the pylon Viewer to easily set the parameters.