Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Timer#

The Timer camera feature allows you to configure a timer output signal that goes high on specific camera events and goes low after a specific duration.

Using the Feature#

The implementation of this feature varies depending on the camera:

ace 2, boost R, dart M/R, and racer 2 Cameras#

How It Works#

Two timers are available, Timer 1 and Timer 2.

This is how a timer works:

  • A trigger source event that starts the internal timer occurs.
  • A delay begins to expire.
  • An arm delay begins to expire.
  • When the delay has expired, the timer output signal goes high and stays high for the duration that you have configured.
  • When the duration has expired, the timer output signal goes low.
  • When the arm delay has expired, the camera can receive the next trigger source event.

Timer Operation

Configuring a Timer#

To configure a timer:

  1. Set the TimerSelector parameter to the desired timer, e.g., Timer1.
  2. Set the TimerDuration parameter to the desired timer duration in microseconds.
  3. Set the TimerDelay parameter to the desired timer delay in microseconds.
  4. Set the TimerTriggerArmDelay parameter to the desired arm delay in microseconds.
  5. Set the LineSelector parameter to the output line that you want to use for the timer signal.
    If the line is a GPIO line, the line must be configured as output.
  6. If you selected Timer 1 in step 1, set the LineSource parameter to Timer1Active.
  7. If you selected Timer 2 in step 1, set the LineSource parameter to Timer2Active.

For information about the maximum possible Timer parameter values for your camera model, see the Specifics table.

Starting a Timer#

To start a timer:

  1. Set the TimerSelector parameter to the desired timer, e.g., Timer1.
  2. Set the TimerTriggerSource parameter to the source that you want to use to start the timer, e.g., Line2.
  3. If applicable, set the TimerTriggerActivation parameter to one of the following values:
    • RisingEdge (default): The timer starts when the signal rises, i.e., when the signal status changes from low to high.
    • FallingEdge: The timer starts when the signal falls, i.e., when the signal status changes from high to low.
    • AnyEdge: The timer starts when the signal falls or rises.
    • LevelHigh: The timer starts when the signal is high. When the signal changes to low, the timer stops and must be started again.
    • LevelLow: The timer starts when the signal is low. When the signal changes to high, the timer stops and must be started again.
  4. Start the timer by sending a signal on the selected trimer trigger source.

When started, the timer's status immediately changes from TimerTriggerWait to TimerActive, regardless of the delay set. However, the timer output signal will only go high after the delay has expired.

Info

The TimerTriggerActivation parameter is only available for timer trigger sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive.

Resetting a Timer#

To reset a timer, execute the TimerReset command.

The timer's status changes from TimerActive to TimerTriggerWait.

The timer can now be restarted immediately regardless of the arm delay set.

Getting the Status of a Timer#

To get the current status of a timer, get the value of the TimerStatus parameter. This parameter is read-only.

Possible values are:

  • TimerTriggerWait: The timer is waiting to be started.
  • TimerActive: The timer has been started. A timer immediately switches to this state when the trigger source event occurs, regardless of the delay set. If an arm delay is set, the timer remains in the TimerActive state until the arm delay has expired.
  • TimerIdle: The timer is idle. A timer is in this state whenever the TimerTriggerSource parameter is set o Off, i.e., the timer can't be started.

ace Classic/U/L Cameras#

How It Works#

One timer is available, Timer 1. This is how the timer works:

  • A trigger source event (e.g., Exposure Start) that starts the internal timer occurs.
  • A delay begins to expire.
  • When the delay has expired, the timer output signal goes high and stays high for the duration that you have configured.
  • When the signal's duration has expired, the timer output signal goes low.

Timer Operation

Configuring the Timer#

  1. Set the LineSelector parameter to the output line that you want to use for the timer signal.
    If the line is a GPIO line, the line must be configured as output.
  2. Set the LineSource parameter to TimerActive.
  3. Set the TimerTriggerSource parameter to one of the available trigger source events:

    • ExposureStart: The timer starts when the exposure starts.
    • FlashWindowStart: The timer starts when the flash window opens.
  4. Set the TimerDuration parameter to the desired timer duration in microseconds.

  5. Set the TimerDelay parameter to the desired timer delay in microseconds.

Info

On some camera models, you may have to increase the maximum timer duration and timer delay values.

Increasing the Maximum Timer Duration and Delay#

On some camera models, the TimerDuration and TimerDelay parameters are limited to a default maximum value of 4 095.

To increase the maximum timer duration on these models:

  1. Divide the desired timer duration by 4 095 and round up the result to the nearest integer.
    Example: Assume you want to set a timer duration of 50 000 µs. 50000 / 4095 = 12.21 ≈ 13.
  2. Set the TimerDurationTimebaseAbs parameter to the value determined in step 1, in this case 13.
  3. Set the TimerDuration parameter to the desired timer duration, in this case 50 000.
    Internally, the camera calculates the timer duration as follows: TimerDurationRaw x TimerDurationTimebaseAbs = TimerDurationAbs.

To increase the maximum timer delay on these models:

  1. Divide the desired timer delay by 4 095 and round up the result to the nearest integer.
    Example: Assume you want to set a timer delay of 6 000 µs. 6000 / 4095 = 1.47 ≈ 2.
  2. Set the TimerDelayTimebaseAbs parameter to the value determined in step 1, in this case 2.
  3. Set the TimerDelay parameter to the desired timer delay, in this case 6 000.
    Internally, the camera calculates the timer delay as follows: TimerDelayRaw x TimerDelayTimebaseAbs = TimerDelayAbs.

Info

Depending on the TimerDurationTimebaseAbs and TimerDelayTimebaseAbs parameter values, the camera may not be able to achieve the exact timer duration and delay desired.
For example, if you set the TimerDurationTimebaseAbs parameter to 13, the camera can only achieve timer durations that are a multiple of 13. Therefore, if you set the TimerDuration parameter to 50 000 and the TimerDurationTimebaseAbs parameter to 13, the camera will automatically change the setting to the nearest possible value (e.g., 49 998, which is the nearest multiple of 13).

Additional Parameters#

  • TimerSelector: Sets which timer to configure. Because Basler ace Classic/U/L cameras support only one timer, this parameter is preset and can't be changed.

Specifics#

Show all camera models

Camera Model Maximum Timer Value [µs]
a2A640-240gmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A640-240umSWIR Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1280-80gmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1280-125umSWIR Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1920-51gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-51gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-51gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-51gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-51gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-51gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-160ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1920-160ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1920-160umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1920-160umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A1920-165g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A1920-165g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-35gmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-37gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-37gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-37gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-37gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-110umSWIR Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2048-114g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-114g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2048-114ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2048-114ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2048-114umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2048-114umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2048-173cmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2440-98g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2440-98g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-23gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-75ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2448-75ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2448-75umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2448-75umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2448-105g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-105g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-120cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-120cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-210cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2448-210cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2560-20gmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2560-70umSWIR Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2560-131cmSWIR Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2590-22gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2590-22gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2590-22gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2590-22gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2590-60ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2590-60ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2590-60umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2590-60umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2600-20gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2600-20gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2600-20gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2600-20gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2600-64ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2600-64ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2600-64umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2600-64umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-14gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-14gmUV Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-48ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-48ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-48umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-48umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-48umUV Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A2840-67g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-67g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-67g5mUV Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-86cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A2840-86cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-9gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-9gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-9gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-9gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-31ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3536-31ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3536-31umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3536-31umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3536-42g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3536-42g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3840-13gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3840-13gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3840-13gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3840-13gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A3840-45ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3840-45ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3840-45umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A3840-45umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4096-9gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-9gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-9gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-9gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-9gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-9gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-30ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4096-30ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4096-30umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4096-30umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4096-44g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-44g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-67cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4096-67cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4200-12gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4200-12gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4200-12gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4200-12gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4200-40ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4200-40ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4200-40umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4200-40umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4504-5gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-5gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-5gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-5gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-5gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-5gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-18ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4504-18ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4504-18umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4504-18umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4504-27g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-27g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-42cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4504-42cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4508-6gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4508-6gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4508-6gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4508-6gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A4508-20ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4508-20ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4508-20umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A4508-20umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5060-4gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5060-4gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5060-15ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5060-15umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5060-21g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5060-21g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5060-35cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5060-35cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-7gmip67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-23ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5320-23ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5320-23umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5320-23umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5320-34g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-34g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-52cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5320-52cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gcBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gcIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gcPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gmBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gmIP67 Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-4gmPRO Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-15ucBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5328-15ucPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5328-15umBAS Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5328-15umPRO Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
a2A5328-22g5cBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-22g5mBAS Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-35cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
a2A5328-35cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
acA640-121gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA640-300gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA640-300gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA640-750uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA640-750um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA720-290gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA720-290gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA720-520uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA720-520um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA800-200gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA800-200gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA800-510uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA800-510um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1280-60gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1280-60gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1300-60gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1300-60gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1300-60gmNIR Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1300-75gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1300-75gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1300-200uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1300-200um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1440-73gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1440-73gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1440-220uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1440-220um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1600-60gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1600-60gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1920-25gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1920-25gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA1920-25uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-25um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-40umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-48gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-48gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-50gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-50gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-150uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-150um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-155uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-155ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-155um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA1920-155umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2000-50gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2000-50gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2000-165uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2000-165um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-25gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2040-25gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2040-25gmNIR Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2040-35gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-35gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-55uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-55um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-90uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-90um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-90umNIR Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-120uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2040-120um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-20gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-20gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-35uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-35ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-35um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-35umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-75uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-75ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-75um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2440-75umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-14gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2500-14gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA2500-14uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-14um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-20gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-20gcMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-20gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-20gmMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-60uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA2500-60um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-16gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-16gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-57uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-57ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-57um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3088-57umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3800-10gc Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA3800-10gm Timer Duration: 139 230 (default maximum: 4 095)
Timer Delay: 139 230 (default maximum: 4 095)
acA3800-14uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA3800-14um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4024-8gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4024-8gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4024-29uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4024-29um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-11gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-11gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-30uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-30ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-30um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-30umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-40uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-40ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-40um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4096-40umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-8gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-8gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-20uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-20ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-20um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-20umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-30uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-30ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-30um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA4112-30umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-5gc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-5gm Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-17uc Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-17ucMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-17um Timer Duration: 16 777 215
Timer Delay: 16 777 215
acA5472-17umMED Timer Duration: 16 777 215
Timer Delay: 16 777 215
boA1936-400cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA1936-400cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA2448-250cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA2448-250cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA2832-190cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA2832-190cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4096-93cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4096-93cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4096-180cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4096-180cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4112-68cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4112-68cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4500-45cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4500-45cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4504-100cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA4504-100cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA5120-150cc Timer feature not supported
boA5120-150cm Timer feature not supported
boA5120-230cc Timer feature not supported
boA5120-230cm Timer feature not supported
boA5320-150cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA5320-150cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA5328-100cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA5328-100cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA6500-36cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA6500-36cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA8100-16cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA8100-16cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
boA9344-30cc Timer feature not supported
boA9344-30cm Timer feature not supported
boA9344-70cc Timer feature not supported
boA9344-70cm Timer feature not supported
boA13440-17cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
daA720-520uc Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA720-520um Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA1280-54uc Timer feature not supported
daA1280-54um Timer feature not supported
daA1440-220uc Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA1440-220um Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA1600-60uc Timer feature not supported
daA1600-60um Timer feature not supported
daA1920-15um Timer feature not supported
daA1920-30uc Timer feature not supported
daA1920-30um Timer feature not supported
daA1920-160uc Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA1920-160um Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA2448-70uc Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA2448-70um Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA2500-14uc Timer feature not supported
daA2500-14um Timer feature not supported
daA3840-45uc Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
daA3840-45um Timer Duration: 21 472 152.45
Timer Delay: 21 472 152.45
Timer Trigger Arm Delay: 21 472 152.45
dmA720-290gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA720-290gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA1440-73gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA1440-73gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA1920-51gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA1920-51gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2048-37gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2048-37gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2448-23gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2448-23gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2840-14gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA2840-14gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA3536-9gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA3536-9gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA4096-9gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
dmA4096-9gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
puA1280-54uc Timer feature not supported
puA1280-54um Timer feature not supported
puA1600-60uc Timer feature not supported
puA1600-60um Timer feature not supported
puA1920-30uc Timer feature not supported
puA1920-30um Timer feature not supported
puA2500-14uc Timer feature not supported
puA2500-14um Timer feature not supported
r2L2048-29gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L2048-58gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L2048-62cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L2048-62g5c Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L2048-172cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L2048-172g5m Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-14gc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-29gm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-42cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-42g5c Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-84cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L4096-84g5m Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L8192-80cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L8192-240cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L16384-60cc Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47
r2L16384-120cm Timer Duration: 21 474 836.47
Timer Delay: 21 474 836.47
Timer Trigger Arm Delay: 21 474 836.47

Sample Code#

ace 2, boost R, dart M/R, and racer 2 Cameras#
// Select Timer 1
camera.TimerSelector.SetValue(TimerSelector_Timer1);
// Set the timer duration to 1000 microseconds
camera.TimerDuration.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelay.SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
camera.TimerTriggerArmDelay.SetValue(5000.0);
// Select Line 2 and configure the line as output
camera.LineSelector.SetValue(LineSelector_Line2);
camera.LineMode.SetValue(LineMode_Output);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_Timer1Active);
// Specify that the timer starts whenever a rising signal is detected on Line 1
camera.TimerTriggerSource.SetValue(TimerTriggerSource_Line1);
camera.TimerTriggerActivation.SetValue(TimerTriggerActivation_RisingEdge);
// Reset the timer
camera.TimerReset.Execute();
// Get the current status of the timer
TimerStatusEnums timerStatus = camera.TimerStatus.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Timer 1
CEnumParameter(nodemap, "TimerSelector").SetValue("Timer1");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDuration").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelay").SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
CFloatParameter(nodemap, "TimerTriggerArmDelay").SetValue(5000.0);
// Select Line 2 and configure the line as output
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
CEnumParameter(nodemap, "LineMode").SetValue("Output");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("Timer1Active");
// Specify that the timer starts whenever a rising signal is detected on Line 1
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("Line1");
CEnumParameter(nodemap, "TimerTriggerActivation").SetValue("RisingEdge");
// Reset the timer
CCommandParameter(nodemap, "TimerReset").Execute();
// Get the current status of the timer
String_t timerStatus = CEnumParameter(nodemap, "TimerStatus").GetValue();
// Select Timer 1
camera.Parameters[PLCamera.TimerSelector].SetValue(PLCamera.TimerSelector.Timer1);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDuration].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelay].SetValue(500.0);
// Set the timer trigger arm delay to 5000 microseconds
camera.Parameters[PLCamera.TimerTriggerArmDelay].SetValue(5000.0);
// Select Line 2 and configure the line as output
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
camera.Parameters[PLCamera.LineMode].SetValue(PLCamera.LineMode.Output);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.Timer1Active);
// Specify that the timer starts whenever a rising signal is detected on Line 1
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.Line1);
camera.Parameters[PLCamera.TimerTriggerActivation].SetValue(PLCamera.TimerTriggerActivation.RisingEdge);
// Reset the timer
camera.Parameters[PLCamera.TimerReset].Execute();
// Get the current status of the timer
string timerStatus = camera.Parameters[PLCamera.TimerStatus].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
size_t len = 0;
char timerStatus_str[64] = {0};
/* Select Timer 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TimerSelector", "Timer1");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDuration", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelay", 500.0);
CHECK(errRes);
/* Set the timer trigger arm delay to 5000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerTriggerArmDelay", 5000.0);
CHECK(errRes);
/* Select Line 2 and configure the line as output */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "LineMode", "Output");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "Timer1Active");
CHECK(errRes);
/* Specify that the timer starts whenever a rising signal is detected on Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "Line1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerActivation", "RisingEdge");
CHECK(errRes);
/* Reset the timer */
errRes = PylonDeviceExecuteCommandFeature(hdev, "TimerReset");
CHECK(errRes);
/* Get the current status of the timer */
len = sizeof(timerStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "TimerStatus", timerStatus_str, &len);
CHECK(errRes);
# Select Timer 1
camera.TimerSelector.Value = "Timer1"
# Set the timer duration to 1000 microseconds
camera.TimerDuration.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelay.Value = 500.0
# Set the timer trigger arm delay to 5000 microseconds
camera.TimerTriggerArmDelay.Value = 5000.0
# Select Line 2 and configure the line as output
camera.LineSelector.Value = "Line2"
camera.LineMode.Value = "Output"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "Timer1Active"
# Specify that the timer starts whenever a rising signal is detected on Line 1
camera.TimerTriggerSource.Value = "Line1"
camera.TimerTriggerActivation.Value = "RisingEdge"
# Reset the timer
camera.TimerReset.Execute()
# Get the current status of the timer
timerStatus = camera.TimerStatus.Value
ace Classic/U/L GigE Cameras#
// Select Line 2 (output line)
camera.LineSelector.SetValue(LineSelector_Line2);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_TimerActive);
// Specify that the timer starts when exposure starts
camera.TimerTriggerSource.SetValue(TimerTriggerSource_ExposureStart);
// Set the timer duration to 1000 microseconds
camera.TimerDurationAbs.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelayAbs.SetValue(500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2 (output line)
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("TimerActive");
// Specify that the timer starts when exposure starts
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("ExposureStart");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDurationAbs").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelayAbs").SetValue(500.0);
// Select Line 2 (output line)
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.TimerActive);
// Specify that the timer starts when exposure starts
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.ExposureStart);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDurationAbs].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelayAbs].SetValue(500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select Line 2 (output line) */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "TimerActive");
CHECK(errRes);
/* Specify that the timer starts when exposure starts */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "ExposureStart");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDurationAbs", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelayAbs", 500.0);
CHECK(errRes);
# Select Line 2 (output line)
camera.LineSelector.Value = "Line2"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "TimerActive"
# Specify that the timer starts when exposure starts
camera.TimerTriggerSource.Value = "ExposureStart"
# Set the timer duration to 1000 microseconds
camera.TimerDurationAbs.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelayAbs.Value = 500.0
Other Cameras#
// Select Line 2 (output line)
camera.LineSelector.SetValue(LineSelector_Line2);
// Specify that the timer signal is output on Line 2
camera.LineSource.SetValue(LineSource_Timer1Active);
// Specify that the timer starts when exposure starts
camera.TimerTriggerSource.SetValue(TimerTriggerSource_ExposureStart);
// Set the timer duration to 1000 microseconds
camera.TimerDuration.SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.TimerDelay.SetValue(500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2 (output line)
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Specify that the timer signal is output on Line 2
CEnumParameter(nodemap, "LineSource").SetValue("Timer1Active");
// Specify that the timer starts when exposure starts
CEnumParameter(nodemap, "TimerTriggerSource").SetValue("ExposureStart");
// Set the timer duration to 1000 microseconds
CFloatParameter(nodemap, "TimerDuration").SetValue(1000.0);
// Set the timer delay to 500 microseconds
CFloatParameter(nodemap, "TimerDelay").SetValue(500.0);
// Select Line 2 (output line)
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Specify that the timer signal is output on Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.Timer1Active);
// Specify that the timer starts when exposure starts
camera.Parameters[PLCamera.TimerTriggerSource].SetValue(PLCamera.TimerTriggerSource.ExposureStart);
// Set the timer duration to 1000 microseconds
camera.Parameters[PLCamera.TimerDuration].SetValue(1000.0);
// Set the timer delay to 500 microseconds
camera.Parameters[PLCamera.TimerDelay].SetValue(500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select Line 2 (output line) */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Specify that the timer signal is output on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "Timer1Active");
CHECK(errRes);
/* Specify that the timer starts when exposure starts */
errRes = PylonDeviceFeatureFromString(hdev, "TimerTriggerSource", "ExposureStart");
CHECK(errRes);
/* Set the timer duration to 1000 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDuration", 1000.0);
CHECK(errRes);
/* Set the timer delay to 500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "TimerDelay", 500.0);
CHECK(errRes);
# Select Line 2 (output line)
camera.LineSelector.Value = "Line2"
# Specify that the timer signal is output on Line 2
camera.LineSource.Value = "Timer1Active"
# Specify that the timer starts when exposure starts
camera.TimerTriggerSource.Value = "ExposureStart"
# Set the timer duration to 1000 microseconds
camera.TimerDuration.Value = 1000.0
# Set the timer delay to 500 microseconds
camera.TimerDelay.Value = 500.0

You can also use the pylon Viewer to easily set the parameters.