Circuit Diagrams (ace)#
Info
For electrical requirements of your camera model, see your camera topic. You can find your camera topic in the "Models" section.
Opto-Coupled Input Line#
The following diagram shows a typical circuit using the opto-coupled input line. As an example, a TTL or CMOS logic gate is used in the external circuit.
Opto-Coupled Output Line#
The following diagram shows a typical circuit using the opto-coupled output line.
The following diagram shows a typical circuit you can use to monitor the opto-coupled output line with an LED. In this example, the voltage in the external circuit is 24 VDC. Current in the circuit is limited by an external resistor.
GPIO Input Line#
The following diagram shows a typical circuit when a GPIO line, if present on your camera model, is set to operate as an input. As an example, a TTL or CMOS logic gate is used in the external circuit.
The following diagram shows a different example of an external circuit using a GPIO line, if present on your camera model.
GPIO Output Line#
The following diagram shows a typical circuit when a GPIO line, if present on your camera model, is set to operate as an output.