Balance White#
For this purpose, a digital gain correction can be applied per color channel (red, green, blue).
To automatically correct color shifts, use the Balance White Auto feature.
Using the Feature#
Why Perform White Balance Correction#
Images acquired by your camera may have a color cast, i.e., a tint of a particular color. The reason for this is that different sources of light have different color temperatures. Fluorescent lighting adds a bluish cast to images whereas tungsten incandescent light adds a yellowish cast.
The white balance feature allows you to correct these color shifts by adjusting the intensity of the colors red, green, and blue. As a result, white objects appear white in the acquired images.
Performing White Balance Correction#
To perform white balance correction:
- Set the Balance White Auto auto function to
Off. - For best results, set the black level to 0 (zero).
- Set the
BalanceRatioSelectorparameter to one of the available color channels (Red,Green, orBlue). -
Adjust the
BalanceRatioparameter value for the selected color channel:- Balance ratio = 1: The intensity of the color remains unchanged.
- Balance ratio > 1: The intensity of the color is increased relative to the other two colors.
- Balance ratio < 1: The intensity of the color is decreased relative to the other two colors. (This is only possible if your camera model supports balance ratio values lower than 1.)
- Repeat steps 3 and 4 for all available color channels.
The increase or decrease in intensity is proportional. For example, if the balance ratio for a color is set to 1.2, the intensity of that color is increased by 20 %.
Info
- Specifying a balance ratio lower than 1 also decreases the maximum intensity that the color can achieve. Unless you want to correct a strong predominance of one color, specifying a balance ratio of less than 1 is not recommended.
- Some color enhancement features, e.g., Light Source Preset or Color Transformation, also have an effect on the white balance settings. If necessary, you can manually re-adjust the white balance after having used these features.
External Links#
Sample Code#
ace Classic/U/L GigE Cameras#
// Set the red intensity to 108.789%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Red);
camera.BalanceRatioAbs.SetValue(1.08789);
// Set the green intensity to 100%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Green);
camera.BalanceRatioAbs.SetValue(1.0);
// Set the blue intensity to 219.678%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Blue);
camera.BalanceRatioAbs.SetValue(2.19678);
INodeMap& nodemap = camera.GetNodeMap();
// Set the red intensity to 108.789%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Red");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(1.08789);
// Set the green intensity to 100%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Green");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(1.0);
// Set the blue intensity to 219.678%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Blue");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(2.19678);
// Set the red intensity to 108.789%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Red);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(1.08789);
// Set the green intensity to 100%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Green);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(1.0);
// Set the blue intensity to 219.678%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Blue);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(2.19678);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the red intensity to 108.789% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Red");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 1.08789);
CHECK(errRes);
/* Set the green intensity to 100% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Green");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 1.0);
CHECK(errRes);
/* Set the blue intensity to 219.678% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Blue");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 2.19678);
CHECK(errRes);
# Set the red intensity to 108.789%
camera.BalanceRatioSelector.Value = "Red"
camera.BalanceRatioAbs.Value = 1.08789
# Set the green intensity to 100%
camera.BalanceRatioSelector.Value = "Green"
camera.BalanceRatioAbs.Value = 1.0
# Set the blue intensity to 219.678%
camera.BalanceRatioSelector.Value = "Blue"
camera.BalanceRatioAbs.Value = 2.19678
Other Cameras#
// Set the red intensity to 108.789%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Red);
camera.BalanceRatio.SetValue(1.08789);
// Set the green intensity to 100%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Green);
camera.BalanceRatio.SetValue(1.0);
// Set the blue intensity to 219.678%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Blue);
camera.BalanceRatio.SetValue(2.19678);
INodeMap& nodemap = camera.GetNodeMap();
// Set the red intensity to 108.789%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Red");
CFloatParameter(nodemap, "BalanceRatio").SetValue(1.08789);
// Set the green intensity to 100%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Green");
CFloatParameter(nodemap, "BalanceRatio").SetValue(1.0);
// Set the blue intensity to 219.678%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Blue");
CFloatParameter(nodemap, "BalanceRatio").SetValue(2.19678);
// Set the red intensity to 108.789%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Red);
camera.Parameters[PLCamera.BalanceRatio].SetValue(1.08789);
// Set the green intensity to 100%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Green);
camera.Parameters[PLCamera.BalanceRatio].SetValue(1.0);
// Set the blue intensity to 219.678%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Blue);
camera.Parameters[PLCamera.BalanceRatio].SetValue(2.19678);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the red intensity to 108.789% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Red");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 1.08789);
CHECK(errRes);
/* Set the green intensity to 100% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Green");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 1.0);
CHECK(errRes);
/* Set the blue intensity to 219.678% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Blue");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 2.19678);
CHECK(errRes);
# Set the red intensity to 108.789%
camera.BalanceRatioSelector.Value = "Red"
camera.BalanceRatio.Value = 1.08789
# Set the green intensity to 100%
camera.BalanceRatioSelector.Value = "Green"
camera.BalanceRatio.Value = 1.0
# Set the blue intensity to 219.678%
camera.BalanceRatioSelector.Value = "Blue"
camera.BalanceRatio.Value = 2.19678
You can also use the pylon Viewer to easily set the parameters.