Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Line Connection#

The Line Connection camera feature allows you to set or determine the connection signal of the currently selected general purpose I/O line (GPIO line).

Connection signals are used to control certain camera features. For example, the "TWI SDA" and "TWI SCL" signals are used for Two-Wire Interface communication.

Using the Feature#

Setting the Line Connection#

To set the line connection:

  1. Set the LineSelector parameter to the desired GPIO line.
  2. Set the BslLineConnection parameter to one of the following values:
    • ConnectionOff: No connection signal is set for the currently selected line.
    • TwiSda: The TWI SDA signal is set for the currently selected line.
    • TwiScl: The TWI SCL signal is set for the currently selected line.
    • LightControl: The light control signal is set for the currently selected line.
  3. Make sure the LineMode parameter is set to InOut. This allows you to use the GPIO line as an input-output line. If the parameter isn't automatically set to InOut, set it manually.

Determining the Line Connection#

To determine the line connection:

  1. Set the LineSelector parameter to the desired I/O line.
  2. Get the value of the BslLineConnection parameter to determine the current line connection of the I/O line.

Sample Code#

// Select Line 2
camera.LineSelector.SetValue(LineSelector_Line2);
// Set the line connection to TWI SDA
camera.BslLineConnection.SetValue(BslLineConnection_TwiSda);
// Get the current line connection
BslLineConnectionEnums e = camera.BslLineConnection.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Set the line connection to TWI SDA
CEnumParameter(nodemap, "BslLineConnection").SetValue("TwiSda");
// Get the current line connection
String_t e = CEnumParameter(nodemap, "BslLineConnection").GetValue();
// Select Line 2
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Set the line connection to TWI SDA
camera.Parameters[PLCamera.BslLineConnection].SetValue(PLCamera.BslLineConnection.TwiSda);
// Get the current line connection
string e = camera.Parameters[PLCamera.BslLineConnection].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Select Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Set the line connection to TWI SDA */
errRes = PylonDeviceFeatureFromString(hdev, "BslLineConnection", "TwiSda");
CHECK(errRes);
/* Get the current line connection */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "BslLineConnection", e_str, &len);
CHECK(errRes);
# Select Line 2
camera.LineSelector.Value = "Line2"
# Set the line connection to TWI SDA
camera.BslLineConnection.Value = "TwiSda"
# Get the current line connection
e = camera.BslLineConnection.Value

You can also use the pylon Viewer to easily set the parameters.