Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Circuit Diagrams (Basler dart M GigE Switches)#

This topic provides sample circuit diagrams for connecting your Basler dart M GigE Switch to a dart M GigE camera module.

Input Lines#

The following diagram shows a typical circuit with an input on a dart M GigE switch. As an example, GPI Cam1 is connected, and a TTL or CMOS logic gate is used in the external circuit.

Input Line Circuit Diagram with a Typical External Circuit

The following diagram shows a different example of an external circuit using an input of a dart M GigE switch.

Input Line Circuit Diagram with a Different External Circuit

Output Lines#

The following diagram shows a typical circuit using an output on a dart M GigE switch. As an example, GPO Cam 1 is connected. This circuit only works with devices that accept NPN communication.

Output Line Circuit Diagram with a Typical Voltage Output Circuit

Further Information#