GMSL Adapter Kit for Jetson Orin Nano Super Developer Kit#
This topic provides information about the characteristics of the Basler GMSL Adapter Board, how to connect it to an NVIDIA Jetson Orin Nano Super Developer Kit, and how to use the adapter board in combination with Basler GMSL cameras and the NVIDIA Jetson Orin Nano Super Developer Kit.

Info
The Basler GMSL Adapter Board is suitable for the following camera models: ace 2 GMSL cameras
Key Features#
- Works with NVIDIA's Jetson Orin Nano Super Developer Kit
- Connects up to four Basler GMSL cameras (2 Dual Deserializer ports, allowing you to connect two cameras to one port)
- Switchable PoC camera power supply
- 2 Flat Flex Cables (FFC) (22 pins, 0.5 mm pitch, 76 mm) to connect the NVIDIA Developer Kit to the Basler GMSL Adapter Board
- Y-split power cable to branch off the power supply from the NVIDIA Developer Kit.
This way the system set-up works with just one power supply unit.
General Specifications#
| Order Number | 109905 |
| Supported embedded board/host system | NVIDIA Jetson Orin Nano Super Development Kit |
| Supported cameras | Basler ace 2 GMSL cameras |
| Conformity | CE (includes RoHS), UKCA, FCC, KC For more information, see the Compliance section of the Basler website." |
GMSL Adapter Board Dimensions#
Components on Adapter Board#
Environmental Specifications#
| Operating Temperature | -10–60 °C (14–140 °F) If board is mounted in a housing, make sure that the ambient temperature is within in these limits: -40–70 °C (-40–158 °F) The NVIDIA Jetson Orin Nano Super Developer Kit is rated for 0–35 °C (32–95 °F). |
| Storage Temperature | -40–100 °C (-40–212 °F) |
| Humidity | non-condensing |
Electrical Specifications#
| Basler GMSL Adapter Board | |
|---|---|
| Supply Voltage (via DC Jack) | 19 VDC (typical) (GMSL Adapter Board and NVIDIA Jetson Orin Nano Super Developer Kit) |
| Power Requirements | 3.3 W + camera supply (This depends on the ace 2 GMSL camera model.) |
| Power Supply Voltage (for 12 VDC PoC Cameras) | 12 VDC |
| PoC Output Current per Camera | 0.6 A |
Info
- The power supply of the NVIDIA Jetson Orin Nano Super Developer Kit can be used via the Y-split power cable included in the GMSL Adapter Kit.
- Observe the maximum power output of the DC power supply when connecting multiple cameras.
Status LEDs#
There are the following LEDs on the GMSL Adapter Board
(assignment "connectors to LEDs", see in the images above):
- 4 PoC LEDs (PoC = Power over CoaX) indicating the power status of the cameras
- 1 PoC (PoC board voltage) indicating the status of the GMSL Adapter Board's PoC voltage
- 1 LED indicating the status of the GMSL Adapter Board's input voltage
See LED States table for a description of the different LED states.
LED States#
| LED State | Meaning |
|---|---|
| 4 PoC indicator LEDs (camera power) | Green: 12 V PoC to camera enabled LED not on: 12 V PoC disabled |
| 1 PoC LED (PoC board voltage status) | Green: 12V PoC voltage source is present on the GMSL Adapter Board. LED not on: 12V PoC voltage source not present |
| 1 Board input voltage LED | Orange/yellow: Input voltage for GMSL Adapter Board is present and all voltage regulators are working (normal state). Red: Input voltage is present, but the GMSL Adapter Board voltage regulators are not working. LED not on: No input voltage or the GMSL Adapter Board voltage regulators are not working. |
Installation#
Before You Start#
Make sure that the following items are available before starting the installation:
- Basler GMSL Adapter Kit, including
- Basler GMSL Adapter Board (GMSL2 Quad deserializer board)
- 2 flat flex cables (FFC cable): 22-pin socket connector with 0.5-mm pitch/ one cable for two GMSL cameras (i.e., max. four cameras can be connected)
- 1 DC power cable with Y-split, 5.5 x 2.5 mm
- Screws for mounting the board
- NVIDIA Jetson Orin Nano Super Development Kit with power supply
- Camera Enablement Package (to be installed on the NVIDIA Jetson Orin Nano Super Developer Kit). Supported by a Camera Enablement Package is the NVIDIA JetPack 6 with NVIDIA Orin SoC.
See the NVIDIA documentation for further information. - Basler ace 2 GMSL cameras
- GMSL Coaxial Cables with FAKRA Connector. You need one cable per camera.<
For ordering a suitable cable assembly, see the website product page. - Internet connection with access to the Ubuntu APT mirrors
The following image shows a setup example. Be aware that the components and their numbers (e.g., cameras) may vary.

First Steps#
- Make sure your host system (i.e., the Nvidia Jetson Orin Nano Super Development Kit) is prepared (i.e., it can be run).
See the NVIDIA documentation for further information. - Install pylon for Linux on your host system.
- Install the Camera Enablement Package for your host system.
See also further details in Installing and Setting Up the Software.
Installing Cameras, GMSL Adapter Board, and Lights#
To connect the cameras:
In the following setup, the power supply for the cameras is delivered via the power connector on the GMSL Adapter Board.
- Make sure that all power to the components is turned off.
- Remove the protective cap from the lens mount.
- Mount a lens on the camera. Be careful not to insert the lens any deeper than specified in the Maximum Allowed Lens Intrusion topic.
- If you only want to use the FAKRA connectors, skip this step and proceed with step 4.
If you want to use any of the camera's I/O lines (opto-coupled lines, GPIO lines), carry out the following steps:- For each camera, plug the 6-pin connector of the I/O cable into the I/O connector of the camera.
- For each camera, connect the other end of the I/O cable to the device that sends and receives I/O signals.
- Connect the FAKRA coaxial cables:
- For each camera, plug the FAKRA connector of the coaxial cable into the FAKRA connector of the camera. For information about the assignment of FAKRA connector to the connector on the GMSL Adapter Board, see the drawings above.
- For each camera, plug the other end of the FAKRA coaxial cable into the FAKRA port of the GMSL Adapter Board.
- Connect the FFC cables to the MIPI connectors on the adapter board and on the NVIDIA Jetson Orin Nano Developer Kit. For information about the assignment between adapter board and the NVIDIA Jetson Orin Nano Developer Kit, see drawing under Components on Adapter Board above and table below.
- Connect the Y-split DC power cable:
- Connect the male plugs of the Y-split DC power cable to the power connector of the GSML Adapter Board and to the power connector of the NVIDIA Jetson Orin Nano Developer Kit.
- Connect the input end of the Y-split DC power cable to the power source.
| Camera FAKRA Connector on GMSL Adapter Board | MIPI Connector on Jetson Orin Nano Module |
|---|---|
| YA, YB | CAM0 |
| XA, XB | CAM1 |
Info
On the 'CAM0' connector, the NVIDIA Jetson Orin Nano module only supports 2 MIPI CSI lanes. This is a limitation of the NVIDIA Jetson Orin Nano Super Development Kit and not of the GMSL Adapter Board. This reduces the available bandwidth on the GMSL connectors YA/YB (~ 250 MB/s available). 'CAM1' supports four MIPI CSI lanes (i.e., 500 MB/s available).
To install the lights
For information about the light installation steps (lights and light control), see Controller Types and Light Control Modes and Installation (Basler Lights).
Installing and Setting Up the Software#
For the following steps, you need internet access.
- Make sure that your components are powered on.
- To use the cameras, install the Camera Enablement Package. Supported is the NVIDIA JetPack 6 with NVIDIA Orin Nano SoM.
For other operating systems (e.g., Yocto) or other SoCs (e.g., NXP i.MX8, Rasperry Pi5 CM5), contact Basler support to get help. -
During installation, it may be necessary to install additional distribution-specific packages. This requires an internet connection with access to the Ubuntu APT mirrors.
The following code snippet shows the call:# -
After the successful installation, reboot your system and start the pylon Viewer either via the icon inside the Ubuntu application launcher or via the terminal (see below).
Info
- When the system starts up, the camera supply is switched on. It may take a few seconds before the cameras appear in the Devices pane.
- If the cameras aren't displayed in the Devices pane, activate the Refresh button next to the Auto-Scan check box.

Configuring#
- Depending on the number of cameras you installed, you have to adapt the bandwidth management of the cameras in the Bandwidth Manager.
Info
By default, the maximum possible bandwidth for each camera is assigned to the SoC via the CSI interface. You can change this distribution in the Bandwidth Manager. See Optimizing Bandwidth Consumption.
Further Information#
- For general information about GMSL cameras, see the General Information topic.
- For information about configuring Basler ace 2 GMSL cameras, see the Configuring Basler GMSL Cameras topic.