Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Image Sharpening vTool#

The Image Sharpening vTool allows you to sharpen contrast and image edges.

The Image Sharpening vTool accepts an image via the Image input pin and outputs the filtered image via the Image output pin.

If you use the ROI Creator vTool to specify a region of interest before enhancing, the Image Sharpening vTool accepts the ROI data via its Roi input pin. In that case, only the region of interest is sharpened which results in faster processing.

The Image Sharpening vTool is available in the Preprocessing Basic license. To buy a license, visit the Basler website.

Image Sharpening vTool

Image Sharpening vTool Versions#

Two versions of the Image Sharpening vTool are available. The following table shows the differences between the versions. Click a version in the table heading to jump directly to the relevant section in this topic.

Starter Basic
How many sharpening operations are available? 2
Sharpening Filter
Unsharp Mask
1
Valid data types for Roi input pin RectangleF RectangleF, RectangleF Array,
Region, Region Array
Buy license Included in the pylon Software Suite Visit Basler website

Image Sharpening Starter#

How It Works#

The Image Sharpening Starter vTool offers two solutions for sharpening the image.

Sharpening Filter#

The sharpening filter uses a square mask. The center pixel of that mask is multiplied by the sharpening factor. All other pixels of the mask are multiplied by -1. For mask sizes greater than 9, the border pixels of the image are excluded from the sharpening operation.

Choose the size of the filter mask according to the specific purpose of your application. Even filter mask sizes will be increased to the next uneven values. The maximum mask size is 25 x 25.

Specify the desired sharpening factor. This determines the amount of amplification. The minimum sharpening factor is calculated based on the width and height of the mask. You can increase it if desired.

Unsharp Mask#

The original image is filtered using a smoothing filter. Then, the filtered image is subtracted from the original image. Pixels with gray values above the threshold specified are multiplied by the sharpening factor.

Choose the size of the filter mask according to the specific purpose of your application. Even filter mask sizes will be increased to the next uneven values. To create square masks, you can link the Width and Height options. To do this, click the chain icon:

  • Options linked: Chain Icon
  • Options unlinked: Chain Broken Icon

Also, you can specify the desired sharpening factor and sharpening threshold. The sharpening factor determines the amount of amplification. Only pixels with gray values above the threshold will be amplified.

Configuring the vTool#

To configure the Image Sharpening Starter vTool:

Image Sharpening Starter vTool Settings

  1. In the Recipe Management pane in the vTool Settings area, click Open Settings or double-click the vTool.
    The Image Sharpening Starter dialog opens.
  2. Select the desired Sharpening Operation.
  3. Specify the Width and Height of the filter mask.
  4. Specify the desired sharpening factor.
  5. If you have selected the Unsharp mask operation, specify the sharpening threshold.

You can view the result of the sharpening in a pin data view.

Image Sharpening Basic#

How It Works#

A sharpening filter amplifies high frequency structures of an image like edges or lines.

The Image Sharpening Basic vTool compares a mean image, computed from the original image, to the original image. The differences between these two images are then amplified and added to the original image. The formula is:

Image_out = ( Image_in - mean_filter(Image_in) ) * Factor + Image_in

The strength of the sharpening is determined by the sharpening factor.

The filter mask size defines the cut-off frequency of the filter. Smaller filter masks will amplify only higher frequency structures of the image.

Mask Shapes#

Image Sharpening uses a rectangular filter mask. Choose the size of the filter mask according to the specific purpose of your application.

Only odd width and height values are allowed. Even mask sizes will automatically be increased to the next uneven values.

To create square masks, you can link the Width and Height options. To do this, click the chain icon:

  • Options linked: Chain Icon
  • Options unlinked: Chain Broken Icon

Sharpening Factor#

Specify the desired sharpening factor. This determines the amount of amplification.

Configuring the vTool#

To configure the Image Sharpening Basic vTool:

Image Sharpening Basic vTool Settings

  1. In the Recipe Management pane in the vTool Settings area, click Open Settings or double-click the vTool.
    The Image Sharpening Basic dialog opens.
  2. Specify the Width and Height of the filter mask.
  3. Specify the desired sharpening Factor.

You can view the result of the sharpening in a pin data view.

Inputs#

Image#

Accepts images directly from a Camera vTool or from a vTool that outputs images, e.g., the Image Format Converter vTool.

Roi#

Accepts a region of interest from the ROI Creator vTool or any other vTool that outputs regions or rectangles. Multiple rectangles or regions are merged internally to form a single region of interest.

  • Data type: RectangleF, RectangleF Array, Region, Region Array

Outputs#

Image#

Returns the filtered image. The output image can be used by any vTool accepting images as input.

Supported Pixel Formats#

Depending on the pixel format of the input image, the Image Sharpening Basic vTool outputs the following pixel formats (supported pixel formats for the Starter are to be confirmed at a later stage):

Input Pixel Format Output Pixel Format
Bayer GR 8 RGB 8 Planar
Bayer GR 16 RGB 16 Planar
Bayer RG 8 RGB 8 Planar
BGRA 8 Packed RGB 8 Planar
BGR 8 Packed RGB 8 Planar
Mono 8 Mono 8
Mono 10 Mono 10
Mono 12 Mono 12
Mono 16 Mono 16
RGB 8 Packed RGB 8 Planar
RGB 16 Packed RGB 16 Planar
RGB 8 Planar RGB 8 Planar
RGB 16 Planar RGB 16 Planar

Typical Predecessors#

Typical Successors#