Skip to content

PLCamera.BinningModeVerticalEnum Class#

Sets the binning mode for vertical binning.

Applies to: CameraLink

Visibility: Beginner

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BinningModeVerticalEnum

Constructors#

 NameDescription
Public methodPLCamera.BinningModeVerticalEnum Initializes a new instance of the PLCamera.BinningModeVerticalEnum class
 

Properties#

 NameDescription
Public propertyAveraging

The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.

Applies to: CameraLink

Public propertyName The full name of BinningModeVertical (Overrides ParameterListEnum.Name.)
Public propertySumming

The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.

Applies to: CameraLink

 

Methods#

 NameDescription
Public methodToString The full name of BinningModeVertical (Overrides Object.ToString()()()().)
 

PLCamera.BinningModeVerticalEnum.ToString Method#

The full name of BinningModeVertical

Return Value#

Type: String
Returns the full name of BinningModeVertical

PLCamera.BinningModeVerticalEnum Constructor#

Initializes a new instance of the PLCamera.BinningModeVerticalEnum class

PLCamera.BinningModeVerticalEnum.Averaging Property#

The values of the binned pixels are averaged. This increases the signal-to-noise ratio without affecting the camera's response to light.

Applies to: CameraLink

PLCamera.BinningModeVerticalEnum.Name Property#

The full name of BinningModeVertical

PLCamera.BinningModeVerticalEnum.Summing Property#

The values of the binned pixels are summed. This increases the camera's response to light and the signal-to-noise ratio.

Applies to: CameraLink