Skip to content

PLTransportLayer.TriggerExceededPeriodLimitsEnum Class#

Returns whether the input signal frequency exceeded the maximum specified. If the parameter returns Yes, signals were dropped.

Applies to: CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLTransportLayer.TriggerExceededPeriodLimitsEnum

Constructors#

 NameDescription
Public methodPLTransportLayer.TriggerExceededPeriodLimitsEnum Initializes a new instance of the PLTransportLayer.TriggerExceededPeriodLimitsEnum class
 

Properties#

 NameDescription
Public propertyName The full name of TriggerExceededPeriodLimits (Overrides ParameterListEnum.Name.)
Public propertyNo

The input signal frequency hasn't exceeded the maximum frequency defined by the Trigger Output Frequency parameter.

Applies to: CoaXPress

Public propertyYes

The input signal frequency has exceeded the maximum frequency defined by the Trigger Output Frequency parameter.

Applies to: CoaXPress

 

Methods#

 NameDescription
Public methodToString The full name of TriggerExceededPeriodLimits (Overrides Object.ToString()()()().)
 

PLTransportLayer.TriggerExceededPeriodLimitsEnum.ToString Method#

The full name of TriggerExceededPeriodLimits

Return Value#

Type: String
Returns the full name of TriggerExceededPeriodLimits

PLTransportLayer.TriggerExceededPeriodLimitsEnum Constructor#

Initializes a new instance of the PLTransportLayer.TriggerExceededPeriodLimitsEnum class

PLTransportLayer.TriggerExceededPeriodLimitsEnum.Name Property#

The full name of TriggerExceededPeriodLimits

PLTransportLayer.TriggerExceededPeriodLimitsEnum.No Property#

The input signal frequency hasn't exceeded the maximum frequency defined by the Trigger Output Frequency parameter.

Applies to: CoaXPress

PLTransportLayer.TriggerExceededPeriodLimitsEnum.Yes Property#

The input signal frequency has exceeded the maximum frequency defined by the Trigger Output Frequency parameter.

Applies to: CoaXPress