Skip to content

PLCamera.LegacyBinningVerticalEnum Class#

Sets whether vertical binning is used.

Applies to: CameraLink and GigE

Visibility: Beginner

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.LegacyBinningVerticalEnum

Constructors#

 NameDescription
Public methodPLCamera.LegacyBinningVerticalEnum Initializes a new instance of the PLCamera.LegacyBinningVerticalEnum class
 

Properties#

 NameDescription
Public propertyName The full name of LegacyBinningVertical (Overrides ParameterListEnum.Name.)
Public propertyOff

Vertical binning is disabled.

Applies to: CameraLink and GigE

Public propertyTwo_Rows

Vertical binning is set to 2 rows.

Applies to: CameraLink and GigE

 

Methods#

 NameDescription
Public methodToString The full name of LegacyBinningVertical (Overrides Object.ToString()()()().)
 

PLCamera.LegacyBinningVerticalEnum.ToString Method#

The full name of LegacyBinningVertical

Return Value#

Type: String
Returns the full name of LegacyBinningVertical

PLCamera.LegacyBinningVerticalEnum Constructor#

Initializes a new instance of the PLCamera.LegacyBinningVerticalEnum class

PLCamera.LegacyBinningVerticalEnum.Name Property#

The full name of LegacyBinningVertical

PLCamera.LegacyBinningVerticalEnum.Off Property#

Vertical binning is disabled.

Applies to: CameraLink and GigE

PLCamera.LegacyBinningVerticalEnum.Two_Rows Property#

Vertical binning is set to 2 rows.

Applies to: CameraLink and GigE