PLCamera.BslFrequencyConverterSignalSourceEnum Class#
Applies to: racer 2 CXP
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslFrequencyConverterSignalSourceEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslFrequencyConverterSignalSourceEnum | Initializes a new instance of the PLCamera.BslFrequencyConverterSignalSourceEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Counter1Active | The source signal for the frequency converter is set to Counter 1 Active. Applies to: racer 2 CXP |
![]() | Counter1End | The source signal for the frequency converter is set to Counter 1 End. Applies to: racer 2 CXP |
![]() | Counter1Start | The source signal for the frequency converter is set to Counter 1 Start. Applies to: racer 2 CXP |
![]() | Counter2Active | The source signal for the frequency converter is set to Counter 2 Active. Applies to: racer 2 CXP |
![]() | Counter2End | The source signal for the frequency converter is set to Counter 2 End. Applies to: racer 2 CXP |
![]() | Counter2Start | The source signal for the frequency converter is set to Counter 2 Start. Applies to: racer 2 CXP |
![]() | Counter3Active | The source signal for the frequency converter is set to Counter 3 Active. Applies to: racer 2 CXP |
![]() | Counter3End | The source signal for the frequency converter is set to Counter 3 End. Applies to: racer 2 CXP |
![]() | Counter3Start | The source signal for the frequency converter is set to Counter 3 Start. Applies to: racer 2 CXP |
![]() | CxpTrigger0 | The source signal for the frequency converter is set to CXP trigger 0. Applies to: racer 2 CXP |
![]() | CxpTrigger1 | The source signal for the frequency converter is set to CXP trigger 1. Applies to: racer 2 CXP |
![]() | Encoder1 | The source signal for the frequency converter is set to Encoder 1. Applies to: racer 2 CXP |
![]() | EncoderReverse1 | The source signal for the frequency converter is set to Encoder Reverse 1. Applies to: racer 2 CXP |
![]() | FrequencyConverter | The source signal for the frequency converter is set to Frequency Converter. Applies to: racer 2 CXP |
![]() | Line1 | The source signal for the frequency converter is set to Line 1. Applies to: racer 2 CXP |
![]() | Line2 | The source signal for the frequency converter is set to Line 2. Applies to: racer 2 CXP |
![]() | Line3 | The source signal for the frequency converter is set to Line 3. Applies to: racer 2 CXP |
![]() | Name | The full name of BslFrequencyConverterSignalSource (Overrides ParameterListEnum.Name.) |
![]() | Timer1Active | The source signal for the frequency converter is set to Timer 1 Active. Applies to: racer 2 CXP |
![]() | Timer1End | The source signal for the frequency converter is set to Timer 1 End. Applies to: racer 2 CXP |
![]() | Timer2Active | The source signal for the frequency converter is set to Timer 2 Active. Applies to: racer 2 CXP |
![]() | Timer2End | The source signal for the frequency converter is set to Timer 2 End. Applies to: racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslFrequencyConverterSignalSource (Overrides Object.ToString()()()().) |
PLCamera.BslFrequencyConverterSignalSourceEnum.ToString Method#
The full name of BslFrequencyConverterSignalSource
Return Value#
Type: String
Returns the full name of BslFrequencyConverterSignalSource
PLCamera.BslFrequencyConverterSignalSourceEnum Constructor#
Initializes a new instance of the PLCamera.BslFrequencyConverterSignalSourceEnum class
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter1Active Property#
The source signal for the frequency converter is set to Counter 1 Active.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter1End Property#
The source signal for the frequency converter is set to Counter 1 End.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter1Start Property#
The source signal for the frequency converter is set to Counter 1 Start.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter2Active Property#
The source signal for the frequency converter is set to Counter 2 Active.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter2End Property#
The source signal for the frequency converter is set to Counter 2 End.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter2Start Property#
The source signal for the frequency converter is set to Counter 2 Start.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter3Active Property#
The source signal for the frequency converter is set to Counter 3 Active.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter3End Property#
The source signal for the frequency converter is set to Counter 3 End.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Counter3Start Property#
The source signal for the frequency converter is set to Counter 3 Start.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.CxpTrigger0 Property#
The source signal for the frequency converter is set to CXP trigger 0.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.CxpTrigger1 Property#
The source signal for the frequency converter is set to CXP trigger 1.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Encoder1 Property#
The source signal for the frequency converter is set to Encoder 1.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.EncoderReverse1 Property#
The source signal for the frequency converter is set to Encoder Reverse 1.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.FrequencyConverter Property#
The source signal for the frequency converter is set to Frequency Converter.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Line1 Property#
The source signal for the frequency converter is set to Line 1.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Line2 Property#
The source signal for the frequency converter is set to Line 2.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Line3 Property#
The source signal for the frequency converter is set to Line 3.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Name Property#
The full name of BslFrequencyConverterSignalSource
PLCamera.BslFrequencyConverterSignalSourceEnum.Timer1Active Property#
The source signal for the frequency converter is set to Timer 1 Active.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Timer1End Property#
The source signal for the frequency converter is set to Timer 1 End.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Timer2Active Property#
The source signal for the frequency converter is set to Timer 2 Active.
Applies to: racer 2 CXP
PLCamera.BslFrequencyConverterSignalSourceEnum.Timer2End Property#
The source signal for the frequency converter is set to Timer 2 End.
Applies to: racer 2 CXP