PLCamera.BslShadingCorrectionSelectorEnum Class#
Applies to: racer 2 CXP
Visibility: Beginner
Selecting Parameters: BslShadingCorrectionAbsoluteTargetValue, BslShadingCorrectionMaximumMeasuredValue, BslShadingCorrectionMode, BslShadingCorrectionSetCreate, BslShadingCorrectionSetCreateResult, BslShadingCorrectionSetIndex, BslShadingCorrectionSetStatus, BslShadingCorrectionTargetValue
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslShadingCorrectionSelectorEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BslShadingCorrectionSelectorEnum | Initializes a new instance of the PLCamera.BslShadingCorrectionSelectorEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | DSNU | Dark Signal Non-Uniformity (DSNU) correction is performed. Applies to: racer 2 CXP |
![]() | Name | The full name of BslShadingCorrectionSelector (Overrides ParameterListEnum.Name.) |
![]() | PRNU | Photo Response Non-Uniformity (PRNU) correction is performed. Applies to: racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BslShadingCorrectionSelector (Overrides Object.ToString()()()().) |
PLCamera.BslShadingCorrectionSelectorEnum.ToString Method#
The full name of BslShadingCorrectionSelector
Return Value#
Type: String
Returns the full name of BslShadingCorrectionSelector
PLCamera.BslShadingCorrectionSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslShadingCorrectionSelectorEnum class
PLCamera.BslShadingCorrectionSelectorEnum.DSNU Property#
Dark Signal Non-Uniformity (DSNU) correction is performed.
Applies to: racer 2 CXP
PLCamera.BslShadingCorrectionSelectorEnum.Name Property#
The full name of BslShadingCorrectionSelector
PLCamera.BslShadingCorrectionSelectorEnum.PRNU Property#
Photo Response Non-Uniformity (PRNU) correction is performed.
Applies to: racer 2 CXP