PLCamera.EncoderSourceAEnum Class#
Applies to: racer 2 CXP
Visibility: Expert
Selected by: EncoderSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.EncoderSourceAEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.EncoderSourceAEnum | Initializes a new instance of the PLCamera.EncoderSourceAEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Line1 | The source signal for the A input of the encoder control is set to Line 1. Applies to: racer 2 CXP |
![]() | Line2 | The source signal for the A input of the encoder control is set to Line 2. Applies to: racer 2 CXP |
![]() | Line3 | The source signal for the A input of the encoder control is set to Line 3. Applies to: racer 2 CXP |
![]() | Name | The full name of EncoderSourceA (Overrides ParameterListEnum.Name.) |
![]() | Off | No source signal is set for the A input of the encoder control. Applies to: racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of EncoderSourceA (Overrides Object.ToString()()()().) |
PLCamera.EncoderSourceAEnum.ToString Method#
The full name of EncoderSourceA
Return Value#
Type: String
Returns the full name of EncoderSourceA
PLCamera.EncoderSourceAEnum Constructor#
Initializes a new instance of the PLCamera.EncoderSourceAEnum class
PLCamera.EncoderSourceAEnum.Line1 Property#
The source signal for the A input of the encoder control is set to Line 1.
Applies to: racer 2 CXP
PLCamera.EncoderSourceAEnum.Line2 Property#
The source signal for the A input of the encoder control is set to Line 2.
Applies to: racer 2 CXP
PLCamera.EncoderSourceAEnum.Line3 Property#
The source signal for the A input of the encoder control is set to Line 3.
Applies to: racer 2 CXP
PLCamera.EncoderSourceAEnum.Name Property#
The full name of EncoderSourceA
PLCamera.EncoderSourceAEnum.Off Property#
No source signal is set for the A input of the encoder control.
Applies to: racer 2 CXP