pylon Software Suite#
As it is based on GenICam technology, the pylon Software Suite allows you to work with the latest camera models and features.
Supported Operating Systems and Their Features#
Platforms#
| Windows | Linux x86 | Linux ARM | macOS | Android | |
|---|---|---|---|---|---|
| Latest pylon Version | pylon 26.10 | pylon 26.10 | pylon 26.10 | pylon 26.10 | pylon 6.1.0 |
| Supported OS Version | 10 (64 bit), 11 (64 bit) | Ubuntu 20.04 or newer (64 bit), CentOS 9 or newer (64 bit) | Ubuntu 20.04 or newer (64 bit) | 15 (Intel/ARM 64 bit) | 8, 9, 10, 11 |
| Download | Visit Basler website | Visit Basler website | Visit Basler website | Visit Basler website | Visit Basler website |
Configuration Tools#
| Windows | Linux x86 | Linux ARM | macOS | Android | |
|---|---|---|---|---|---|
| pylon Workbench & vTools | |||||
| pylon Viewer | |||||
| pylon GigE Configurator | |||||
| pylon IP Configurator | |||||
| pylon USB Configurator | |||||
| pylon Camera Link Configurator | |||||
| Camera API Generator | |||||
| Firmware Updater | |||||
| CXP Grabber Firmware Updater | |||||
| CXP gpioTool | |||||
| Color Calibrator | |||||
| MPEG-4 Video Recording | |||||
| blaze 3D Viewer |
Application Development#
| Windows | Linux x86 | Linux ARM | macOS | Android | |
|---|---|---|---|---|---|
| Data Processing C++ API | |||||
| C++ API | |||||
| C API | |||||
| .NET API (.NET Framework) | |||||
| .NET 5+ API | |||||
| Java API |
GenTL#
| Windows | Linux x86 | Linux ARM | macOS | Android | |
|---|---|---|---|---|---|
| USB3 Vision | |||||
| GigE Vision | |||||
| CoaXPress 2.0 | |||||
| BCON for MIPI | |||||
| blaze 3D |
Interface Drivers#
| Windows | Linux x86 | Linux ARM | macOS | Android | |
|---|---|---|---|---|---|
| Direct Show Driver (U3V, GEV) | |||||
| TWAIN Driver (U3V, GEV) | |||||
| NeuroCheck Driver (U3V, GEV) | |||||
| CoaXPress 2.0 Driver | |||||
| GigE Vision Driver | |||||
| USB3 Vision Driver | |||||
| Camera Link Driver | |||||
| BCON for MIPI Driver |
SDK and APIs#
The pylon Software Suite provides the pylon SDK (software development kit) that includes the following APIs (application programming interfaces):
- C++ API (Windows, Linux, and macOS)
-
API for .NET languages. Two language bindings are provided:
- .NET Language binding targeting .NET Framework (version 4.0 and higher) on Windows
- .NET Language binding targeting .NET 5+ (version 8.0 and higher) on Windows, Linux, and macOS
The language bindings provide the same pylon .NET API. Differences because of the targeted .NET may occur.
-
C API (Windows and Linux)
- Data Processing C++ API (Windows and Linux): This API extends the pylon C++ image acquisition API to enable the use of vTools.
You can access all of the camera's parameters and control the camera's full functionality from within your application software by using the matching pylon API (C++, C, or .NET). Sample programs illustrate how to use the pylon APIs to parameterize and operate the camera.
Documentation for the image acquisition APIs is available in the pylon API Documentation section. It gives you an introduction to programming with pylon and provides information about all methods and objects of the respective API.
The documentation for the Data Processing C++ API (pylon C++ Data Processing Programmer's Guide) is available via the Help menu in the pylon Viewer.
Configuration Tools#
A set of configuration tools allows you to configure the camera, the interface adapter, and the operating system:
- pylon Viewer (available for Windows, Linux, and macOS)
- pylon GigE Configurator (available for Windows and Linux)
- pylon IP Configurator (available for Windows, Linux, and macOS)
- pylon USB Configurator (available for Windows only)
Drivers#
- The pylon USB3 Vision Driver is fully compliant with the USB3 Vision standard. It enables Basler USB 3.0 cameras to use the full speed and bandwidth of USB 3.0 for image transmission, while reducing resource load and using off-the-shelf hardware components.
-
The pylon GigE Vision Filter Driver is an advanced and robust GigE Vision network driver that is compatible with all network adapters. The advantages of the filter driver are:
- Extensive compatibility with 1/5/10 Gigabit network adapters
- Optimizes and lowers the CPU load caused by network traffic between the computer and the cameras
- Very robust packet resend mechanisms
This driver is available for Windows only. For best performance and reliability, Basler recommends using the filter driver in combination with the pylon GigE Configurator.
-
The pylon GigE Vision Socket Driver is not a real driver, but uses the Socket API of the given operating system, e.g., Windows, Linux, or macOS, to communicate with cameras instead. The advantage of the socket driver is that it doesn't need any installation and is compatible with all 1/5/10 Gigabit network adapters. The socket driver has very robust packet resend mechanisms.
For best performance and reliability, Basler recommends using the filter driver in combination with the pylon GigE Configurator. - The pylon GigE Vision Performance Driver (deprecated in pylon version 7.1) is a hardware-specific GigE Vision network driver. The performance driver is only compatible with 1 Gigabit network adapters that use compatible chipsets. The advantage of the performance driver is that it lowers the CPU load caused by network traffic between the computer and the cameras. It also has a robust packet resend mechanism. This driver is available for Windows only.
- The RDMA Driver is not a real driver but allows cameras to transfer data packets directly into the application buffer on the host computer. This results in high-throughput, low-latency memory access over a network.
- The pylon BCON I²C Driver Adapter (Linux only, deprecated in pylon version 6.3) can be used to develop software for embedded systems. pylon provides the driver's source code as well as a compiled binary file. It can be used as-is, but you can also write your own adapter by implementing the BCON Adapter API.
- The pylon Camera Link Configuration Driver (Windows only) gives you access to all camera parameters of Basler's Camera Link cameras.
- The pylon CXP Interface Driver (not available for macOS) allows you to use Basler's CoaXPress cameras.
- The pylon GigE Accelerator filters GVSP packets during grabbing and groups them to images to reduce CPU load. This driver is for macOS only.
System Requirements#
- x86_64 CPU: Latest Intel Core i5 (or better) or equivalent.
- aarch64 CPU: Armv8-A with AArch64 support. ARM processors used on NVIDIA Jetson modules (or better) or equivalent are recommended.
- Memory: Minimum 4 GB of available RAM. 8 GB or more of available RAM are recommended.
- Disk type: SSD is recommended.
- Disk space: Minimum 2 GB of free disk space for installation.
Info
Depending on the following aspects, higher system requirements may be necessary:
- Number of cameras used
- Resolution and/or acquisition frame rate of the camera
- Types or number of vTools used
If you're planning to use the pylon AI features, the following system requirements apply:
- x86_64 CPU: Latest Intel Core i5 (or better) or equivalent.
- Memory: Minimum 8 GB of available RAM. 16 GB or more of available RAM are recommended.
- Disk type: SSD is recommended.
- Disk space: Minimum 50 GB of free disk space for installation.
The space required for the model repository depends on the size and number of models you plan to deploy. Models can range from a few megabytes to several gigabytes each. - GPU models: All NVIDIA models matching architectures mentioned here: https://docs.nvidia.com/deeplearning/frameworks/support-matrix/index.html
- CUDA version: 12+
- GPU cards: Examples of suitable cards include NVIDIA RTX A5000, NVIDIA RTX A2000 Laptop GPU, NVIDIA Jetson Xavier NX, NVIDIA Tesla T4, etc.
Installation#
→ See Software Installation (Windows)
→ See Software Installation (Linux)
Documentation#
You can access the Basler Product Documentation directly from the suite's various tools.
In the pylon Viewer, you can get context-sensitive help. If you need more information about a parameter or want to know more about your camera model, select the desired item in the Devices or the Features pane and open the documentation by pressing F1 or right-clicking and then clicking Get Help.
The Help menu also gives you access to the pylon Deployment Guide, the pylon SDK Samples Manual, the pylon API documentation, and the C++ Data Processing Programmer's Guide.