Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Software Installation (Stereo ace)#

This topic explains how to install the software required for a Basler Stereo ace camera.

You need to install the following software components:

  • pylon Software Suite (version 8.1 or higher)
  • pylon Supplementary Package for Stereo ace

The software is available for the following operating systems:

  • Windows
  • Linux x86_64
  • Linux ARM

You can download the software from the Basler website.

Software Installation (Windows)#

To install the Stereo ace software:

  1. Download the following installers from the Basler website:
    • Basler_pylon_version.exe
    • pylon_Supplementary_Package_for_stereo_ace_version.exe
  2. Navigate to the folder where you downloaded the installers and double-click the Basler_pylon_version.exe file.
    The pylon Setup Wizard opens.
  3. Accept the license agreement and click Next.
  4. On the Profiles page, select the Developer profile and click Next.
  5. On the Interfaces page, select the GigE interface and click Next.

    Info

    Choosing the "Custom" Profile Option

    If you prefer to choose the software components to be installed individually, select the Custom option in step 4 (Interfaces page) of the procedure above. If you do, you have to select the following options on the Features page:

    • pylon Runtime
    • GigE Camera Support
    • GenTL Consumer Support
    • SDKs
  6. On the Destination Folder page, you can change the default install location by clicking Change and choosing the desired folder. When you're happy with the install location, click Next.

  7. Review the settings and click Install when you're ready.
    The installation starts. A message will inform you when the installation has been completed successfully. The start menu will now contain a Basler folder.

  8. Navigate to the folder where you downloaded the installers and double-click the pylon_Supplementary_Package_for_Stereo_ace_version.exe file.

  9. Follow the instructions of the wizard to complete the installation.
    A message will inform you when the installation has been completed successfully.

Software Installation (Linux)#

Info

On Debian-based systems (like Ubuntu), Basler recommends downloading and installing the Debian packages (.deb) of the pylon Software Suite and the pylon Supplementary Package for Stereo ace.

For other Linux distributions, download the .tar.gz archives.

Ubuntu and Other Debian-Based Distributions#

To install the Stereo ace software:

  1. Download the following packages from the Basler website:
    • pylon_version_linux-x86_64_debs.tar.gz
    • pylon-supplementary-package-for-stereo-ace-version_amd64.deb
  2. Install the pylon Software Suite:
    • Extract the pylon_version_linux-x86_64_debs.tar.gz package
    • Change to the directory that contains the pylon Debian package
    • Install the Debian packages:
      sudo apt-get install ./pylon_*.deb ./codemeter*.deb
      
  3. Install the pylon Supplementary Package for Stereo ace by issuing one of the following commands:

    sudo apt-get install ./pylon-supplementary-package-for-stereo-ace-*version*_amd64.deb
    

Linux Distributions Not Based on Debian#

To install the Stereo ace software:

  1. Download the following archives from the Basler website:
    • pylon_version_x86_64_setup.tar.gz
    • pylon-supplementary-package-for-stereo-ace-version_x86_64_setup.tar.gz
  2. Extract the pylon_version_x86_64_setup.tar.gz archive and follow the instructions in the INSTALL document included in the archive.
  3. Extract the pylon-supplementary-package-for-stereo-ace-version_x86_64_setup.tar.gz archive.
  4. Change to the extracted directory and extract the pylon-supplementary-package-for-stereo-ace-version_x86_64_setup.tar.gz archive to /opt/pylon.

Example:

tar xf pylon-supplementary-package-for-stereo-ace-*version*-amd64.tar.gz
cd pylon-supplementary-package-for-stereo-ace-*version*-amd64
sudo tar -C /opt/pylon -xzf ./pylon-supplementary-package-for-stereo-ace-*version*-amd64.tar.gz

Next Steps#

Continue with the hardware installation.