Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Color Image Adjustment#

The Color Adjustment features allow you to change the appearance of images from the color sensor.

Before configuring these features, set the SourceSelector parameter to Source3 (Color).

The following parameters are available:

Parameter Display Name Description
BslBacklightCompensation Backlight Compensation Compensates for strong illumination behind the target object.
BslBrightness Brightness Lightens or darkens the entire image.
BslContrast Contrast Changes the difference between light and dark areas in the image.
Gamma Gamma Applies gamma correction to optimize image brightness for display.
BslHue Hue Shifts the colors in the image.
BslSaturation Saturation Changes the intensity of the colors.
BslSharpness Sharpness Applies sharpening to the image.

Set the desired parameter to the required value. The available ranges depend on the camera model and firmware version.