This operator returns the minimum pixel value found for each input frame. The output frame has the same size as the input frame, where each pixel is replaced by the minimum value found in the image so far. If the current pixel is a new minimum the output Link IsMinO, otherwise it is 0.
![]() |
Resource Consumption |
---|---|
The operator's FGPA resource consumption strongly increases with the parallelism. We recommend to use low parallelism at this operator. In many use cases of this operator, the parallelism can be reduced selecting the min parallel component prior to this operator. Use SplitParallel, MergeKernel and MIN for this operation. |
With every new input frame the minimum detection starts again. Additionally, it is possible to clear the current minimum manually when the ClrI link is set to 1. When a manual clear is not necessary, you must ensure a constant 0 at ClrI, to enable normal operation.
The following example shows the relation of input values to output values.

Often, this operator is used in conjunction with operators RemoveLine and RemovePixel to use only the last image pixel containing the results of all frame pixels.
Image Restrictions
-
Empty Images
Empty images, i.e., images with no pixels, are allowed. The operator will output an empty image.
Property | Value |
---|---|
Operator Type | O |
Input Links | I, Image Input ClrI, Clear Input |
Output Links | O, Data Output IsMinO, binary output to indicate a new minimum |
Link Parameter | Input Link I | Input Link ClrI | Output Link O | Output Link IsMinO |
---|---|---|---|---|
Bit Width | [1, 64] unsigned, [2, 64] signed | 1 | as I | 1 |
Arithmetic | {unsigned, signed} | unsigned | as I | unsigned |
Parallelism | any | as I | as I | as I |
Kernel Columns | 1 | as I | as I | as I |
Kernel Rows | 1 | as I | as I | as I |
Img Protocol | VALT_IMAGE2D, VALT_IMAGE1D, VALT_IMAGE0D | as I | as I | as I |
Color Format | VAF_GRAY | as I | as I | as I |
Color Flavor | FL_NONE | as I | as I | as I |
Max. Img Width | any | as I | as I | as I |
Max. Img Height | any | as I | as I | as I |