The HierarchicalBox is a pseudo module provided by the graphical user interface to group several operators into a single module. This makes it feasible for users to maintain complex projects and comfortably re-use parts from previous projects.
On instantiation of a HierachicalBox, it is possible to select an arbitrary number of input and output links. To open a view of the inside, double click onto the HieracialBox.
A detailed explanation of the usage of hierarchical boxes can be found in the user manual of VisualApplets in 'Hierarchical Boxes'.
Property | Value |
---|---|
Operator Type | Operator type depends on context |
Input Link | I[0] .. I[63], data input |
Output Link | O[0] .. O[63], data output |
Link Parameter | Input Link I[0] .. I[63] | Output Link O[0] .. O[63] |
---|---|---|
Bit Width | any | any |
Arithmetic | any | any |
Parallelism | any | any |
Kernel Columns | any | any |
Kernel Rows | any | any |
Img Protocol | any | any |
Color Format | any | any |
Color Flavor | any | any |
Max. Img Width | any | any |
Max. Img Height | any | any |
The use of operator HierarchicalBox is shown in the following examples:
-
Usage and Navigation through design with HierarchicalBox modules in VisualApplets.
-
Tutorial - Basic Acquisition
-
Examples - A high speed and robust laser line detection algorithm. The algorithm determines center of gravity coordinates to obtain sub-pixel resolution results.