This operator generates a blank binary image of the specified width and height. The operator does not require any input links. The output image width and height is specified using parameters ImageWidth and ImageHeight.
The operator will output the blank images at the maximum possible speed. Thus the output speed is only limited by the output link parallelism and the following operators. The VisualApplets flow control will limit the bandwidth if further operators cannot process the data rates produces by CreateBlankImage.
Often, this operator is used to test the functionality of an implementation without the need to connect a camera. Using operators such as Coordinate_x, Coordinate_y and ImageNumber, the operator can be used to generate test patterns. In conjunction with operator ImageValve the frame, line or pixel rate can be controlled.
The image dimensions of the generated images can only be changed when the acquisition is not running i.e. stopped.
In case of 1D application the ImageHeight parameter is ignored. In case of 0D application both ImageWidth and ImageHeight are ignored.
The operator can easily be used with the VisualApplets simulation. The operator generates simulation images itself. It is working as a simulation source. Therefore, it is not required to add a simulation source probe to the output link of the operator.
![]() |
Behavior during simulation |
---|---|
The operator outputs at least one data set per simulation step. Depending on the current link configuration at the output port this data set is
The default value of those parameters is 1. Depending on the current link configuration at the output port only the relevant parameter is editable and the others are inactive. I.e., for 0D only PixelsToSimulate is editable while for 1D the parameters LinesToSimulate and ImageWidth are editable. |
The operator guarantees image integrity while parameters ImageHeight or ImageWidth are changed during acquisition. After the completion of the current frame output the operator will start using the new parameter values.
Link Parameter | Output Link O |
---|---|
Bit Width | [1, 64] |
Arithmetic | unsigned |
Parallelism | any |
Kernel Columns | 1 |
Kernel Rows | 1 |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} |
Color Format | VAF_GRAY |
Color Flavor | FL_NONE |
Max. Img Width | any |
Max. Img Height | any |
ImageWidth | |
---|---|
Type | dynamic/static read/write parameter |
Default | 1024 |
Range | [0, Maximum Output Image Width], step size = output parallelism |
Specifies the width of the generated images. This parameter is enabled only if the operator's output image protocol is set to VALT_IMAGE2D or VALT_LINE1D. |
ImageHeight | |
---|---|
Type | dynamic/static read/write parameter |
Default | 1024 |
Range | [1, Maximum Output Image Height] |
Specifies the height of the generated images. This parameter is enabled only if the operator's output image protocol is set to VALT_IMAGE2D. |
LinesToSimulate | |
---|---|
Type | static parameter |
Default | 1 |
Range | [1, 2^32 - 1] |
If the output link image protocol is set to VALT_LINE1D, it is required to specify the number of lines for simulation. This parameter is used to specify the simulation image height. See 'Simulation' for more information on 1D simulations. This parameter can only be changed if the output image protocol is set to VALT_LINE1D. |
PixelsToSimulate | |
---|---|
Type | static parameter |
Default | 1 |
Range | [1, 2^32 - 1], step size = output parallelism |
If the output link image protocol is set to VALT_PIXEL0D, it is required to specify the size of the pixel stream for simulation. This parameter is used to specify the simulation pixel stream width. See 'Simulation' for more information on 0D simulations. This parameter can only be changed if the output image protocol is set to VALT_LINE0D. |
The use of operator CreateBlankImage is shown in the following examples:
-
'Color Plane Separation Option 5 - Sequential Output with Advances Processing'
Example on separation of color planes. The RGB input is split into its component and sequentially output via one DMA channel. The splitting if performed by collecting same components in parallel words and reading with FrameBufferRandomRead.
-
An example for hardware self test of DMA, RAM, GPIOs, Trigger and LEDs.
-
Example - The image dimension is measured and can be used to analyze the design flow.
-
Example - For debugging purposes images can be inserted manually.
-
Example - For debugging purposes image transfer states on links can be investigated.
-
Example - For debugging purposes the Scope operator provides options for analyzing gray-scale pictures. .
-
'A rolling average is applied on a dynamic number of images'
Examples - Rolling Average - Loop