Operator Library: Signal
The operator generates a signal pulse when the end of a input image line is detected. The operator input is an image stream. The operator waits for the end of lines at the input image stream. When the line end is detected, a signal pulse of one clock cycle is output. Note that the end of a line might not occur directly after the last line pixel. See the following figure for explanation:
![](../../images/library/Signal/Images/LineEndToSignal1.png)
The end of a frame always occurs at the same time as the end of the last frame line. Note that empty lines can exist in VisualApplets. The operator will generate a signal pulse for empty lines, too.
This operator is excluded from the VisualApplets functional simulation.
Property | Value |
---|---|
Operator Type | M |
Input Link | I, image data input |
Output Link | O, signal output |
The use of operator LineEndToSignal is shown in the following examples:
-
'Rebuild of Operator TrgPortLine with VisualApplets Signal Processing Operators'
A VisualApplets design example where all functions of operator TrgPortLine are rebuild using other signal processing operators. Allows custom trigger modules.
-
'Functional Example for Specific Operators of Library Memory and Library Signal'
Examples - Demonstration of how to use the operator