Operator Library: Arithmetics
The operator ARCSIN is calculating the arc sine of the input.
The input range of arc sine is [-1,1].
The operator maps the input interval range [-1, 1] to
where
is the bit width at the input.
As can be seen, not the full value range of the input is used.
If an input value is outside the allowed value range, the operator will clip the value to -1 or 1.
Thus, the argument x of the arc sine is determined by
![](../../images/math/math-snippet-358.png)
The operator's output range is [-π/2, π/2]. The output value range of the operator in VisualApplets is mapped to
![](../../images/math/math-snippet-359.png)
where
![](../../images/math/math-snippet-360.png)
is the bit width at the output link. Thus the output value is
![](../../images/math/math-snippet-361.png)
The following image shows the plot of the normal inverse arc sine function.
![](../../images/library/Arithmetics/arcsin.png)
In the next figure, the VisualApplets operator implementation is shown. Note the input and output bit widths.
![](../../images/library/Arithmetics/arcsin_imlementation.png)
Link Parameter | Input Link I | Output Link O |
---|---|---|
Bit Width | [8, 12] | [8,32] |
Arithmetic | signed | signed |
Parallelism | any | as I |
Kernel Columns | 1 | as I |
Kernel Rows | 1 | as I |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
Color Format | VAF_GRAY | as I |
Color Flavor | FL_NONE | as I |
Max. Img Width | any | as I |
Max. Img Height | any | as I |
The use of operator ARCSIN is shown in the following examples:
-
'Functional Example for Specific Operators of Library Arithmentics: Trigonometric Functions'
Examples - Demonstration of how to use the operator