Table of Contents
Disclaimer: The Prototype library is absolutely preliminary and subject to extensive changes, even removal. The functionality of the operators cannot be guaranteed. Therefore, the operators must not be used for productive designs. It is included for testing purposes only.
The following list summarizes all Operators of Library Prototype
Operator Name | Short Description | available since | |
---|---|---|---|
![]() |
COUNTER |
Hardware Multiplier. |
Version 1.1 |
![]() |
CustomSignalOperator |
Hardware Multiplier. |
Version 1.1 |
![]() |
HWMULT |
Hardware Multiplier. |
Version 1.1 |
![]() |
PackBitsRLE |
Simple image compression through run-length encoding (RLE). |
Version 1.1 |
![]() |
TrgBoxLine |
Generates the trigger (Exsync signal) for the Camera and is also responsible to assemble the acquired lines to images. |
Version 1.2 |
![]() |
RGB2XYZ |
Converts the color space from RGB to XYZ. |
Version 1.1 |
![]() |
XYZ2LAB |
Converts the color space from XYZ to LAB. |
Version 1.1 |
Table 51. Operators of Library Prototype