Operator Library: Signal
The operator implements a set-reset flip-flop. If a one (HIGH) is at input link Set, the operator sets the output value to HIGH and keeps the value until a zero (LOW) is present at input link Reset. When Reset is set to HIGH, the output value on output link O is set to LOW. Parameter Priority is used to define if Set or Reset is the master. The value defined with parameter Init is output at startup. See the following truth table and waveform for explanation.
Set | Reset | O |
---|---|---|
0 | 0 | O(t-1) |
0 | 1 | 0 |
1 | 0 | 1 |
1 | 1 | 1 (Priority = Set) |
![](../../images/library/Signal/Images/RsFlipFlop1.png)
![](../../images/library/Signal/Images/RsFlipFlop2.png)
This operator is excluded from the VisualApplets functional simulation.
Property | Value |
---|---|
Operator Type | O |
Input Links | Set, signal data input Reset, signal data input |
Output Link | O, signal data output |
Link Parameter | Input Link Set | Input Link Reset | Output Link O |
---|---|---|---|
Bit Width | 1 | 1 | as Set |
Arithmetic | unsigned | unsigned | as Set |
Parallelism | 1 | 1 | as Set |
Kernel Columns | 1 | 1 | as Set |
Kernel Rows | 1 | 1 | as Set |
Img Protocol | VALT_SIGNAL | VALT_SIGNAL | as Set |
Color Format | VAF_GRAY | VAF_GRAY | as Set |
Color Flavor | FL_NONE | FL_NONE | as Set |
Max. Img Width | any | any | as Set |
Max. Img Height | any | any | as Set |
Priority | |
---|---|
Type | static parameter |
Default | RESET |
Range | {RESET, SET} |
This parameter specifies behavior of the operator for the case when both Set and Reset are set to HIGH simultaneously. RESET: the value on the link O will be set to LOW. SET: the value on the output link O will be set to HIGH. |
Init | |
---|---|
Type | static parameter |
Default | 0 |
Range | [0, 1] |
This parameter specifies the start up value. |
The use of operator RsFlipFlop is shown in the following examples:
-
'Rebuild of Operator TrgPortLine with VisualApplets Signal Processing Operators'
A VisualApplets design example where all functions of operator TrgPortLine are rebuild using other signal processing operators. Allows custom trigger modules.