Operator Library: Parameters
You find a general introduction into the library Parameters
in Library Parameters.
This operator generates a 1:1 map parameter (in the parameter ResourceIndex) out of a device resource mapping for a module located anywhere in the design. You specify the referenced module in the parameter Reference and the device resource type in the parameter ResourceName.
![]() |
Availability |
---|---|
To use the ResourceReference operator, you need either an Expert license, a Parameter Module license, or the VisualApplets 4 license. |
The referenced resource mapping is represented as an integer value.
You can define a target within the design hierarchy where the referenced resource mapping will be visible and accessible. The target is defined by two parameters: DisplayHierarchy and DisplayName. In DisplayHierarchy you address a hierarchical box within the same process the rerence operator itself is located in. In parameter DisplayName you set up the name for the target parameter. This means:
- If DisplayHierarchy and DisplayName are both set, the parameter defined by DisplayName is available in the hierarchical box addressed by DisplayHierarchy.
- If DisplayName is empty, no parameter is created.
- If DisplayName is set, but DisplayHierarchy is empty, the parameter defined by DisplayName is added to the parent hierarchy (i.e. the hierarchical box the reference operator itself is located in).
This allows you to make the parameter for the resource mapping available on any hierarchical level of the design you want. For example, you can make the resource mapping of modules within a protected hierarchical box available for parametrization directly under the properties of the protected hierarchical box itself.
Mapped resource parameters can be referenced themselves. Thus, you can reference either the content of the parameter ResourceIndex in a reference operator, or reference the parameter you have defined in the parameters DisplayName and DisplayHierarchy. This is especially important when protected hierarchical boxes are built up out of other protected hierarchical boxes.
![]() |
All connected parameters update at once |
---|---|
If one of the connected parameters is changed (the referenced resource mapping, the map parameter ResourceIndex, or the display reference parameter), the value is changed in all other connected parameters, too. |
The operator has no inputs and outputs, as it doesn't interfere with the data flow structure of the design.
For further details, refer to the general description of the the library Parameters
in Library Parameters.
Status | |
---|---|
Type | static read (although the GUI displays write) parameter |
Default | None |
Range | OK or an error message occurs
|
Displays the error status. If parameter Activate is set to Yes, the other operator settings are checked. This parameter displays the result of this check, i.e., either OK or an error message occurs. This parameter is not part of the final applet. |
DisplayName | |
---|---|
Type | static write parameter |
Default | None |
Range | Any string |
If you want to grant access from and to the referenced parameter defined in the parameter Reference at another point in the design in addition to the reference operator instance itself, you need to define a new parameter. Specify here the name of this new parameter. If this field is empty, no new parameter is created. |
DisplayHierarchy | ||||
---|---|---|---|---|
Type | static write parameter | |||
Default | None | |||
Range | Any string | |||
Specify here the hierarchical box to which you want to attach the new map parameter you defined in the parameter DisplayName. If you defined a new parameter DisplayName, but leave parameter DisplayHierarchy empty: The new parameter is added to the hierarchical box that contains the reference operator instance. If the reference operator instance is located on the highest process level, this is not possible.
|
ResourceIndex | |
---|---|
Type | static, dynamic, write, read parameter |
Default | 0 |
Range | Depends on the index range of the connected device resource |
Map parameter for access from and to the referenced device resource mapping value. |
ResourceName | |
---|---|
Type | static, dynamic, write parameter |
Default | 0 |
Range | Any string |
Define the device resource type which shall be accessed. The name is the same as provided in the device resources dialog. |
Reference | |
---|---|
Type | static write parameter |
Default | None |
Range | Any string defining the referenced module: relative path to module |
Here, you define the position of the referenced module within the design. |
Description | |
---|---|
Type | static write parameter |
Default | None |
Range | Any string |
Here, you define a description of the generated reference parameter. |
Activate | |
---|---|
Type | dynamic write parameter |
Default | No |
Range | {No, Yes} |
Yes = Access to and from the referenced device resource mapping (via the map parameter ResourceIndex) is activated. No = Access to and from the referenced device resource mapping is de-activated and the parameter Status is disabled. The parameters DisplayName and DisplayHierarchy have no effect. |
The use of operator ResourceReference is shown in the following examples:
-
'Functional Example for Specific Operators of Library Signal, Logic, Filter and Parameters'
Examples - Demonstration of how to use the operator