This operator returns the maximum pixel value found inside each image column. The operator replaces each pixel value by the maximum value found in the very same column so far. Only if a current pixel is a new maximum, the output IsMaxO is set to 1. Otherwise, it is 0.
It is possible to clear the current maximum manually by setting the ClrI link to 1. When a manual clear is not required, a constant 0 must be applied to ClrI.
With every new input frame, the detection of the maximum value restarts for each column.
Often, this operator is used in conjunction with the RemoveLine operator to remove all but the last line of a frame. This last line of a frame contains the results of the ColMax operator.
The following example shows the relation of input values to output values:

Operator Restrictions:
-
Image Size
All lines of an input image must have the same length. Images with varying line lengths are not allowed.
-
Empty Images
Empty Images, i.e., images with no pixels, are allowed. The operator will output an empty image.
-
Image Protocols
Only VALT_IMAGE2D and VALT_LINE1D image protocols are supported.
Property | Value |
---|---|
Operator Type | O |
Input Links | I, Image Input ClrI, Clear Input |
Output Links | O, Data Output IsMaxO, Binary output to indicate a new maximum |
Link Parameter | Input Link I | Input Link ClrI | Output Link O | Output Link IsMaxO |
---|---|---|---|---|
Bit Width | [1, 64] unsigned, [2, 64] signed | 1 | as I | 1 |
Arithmetic | {unsigned, signed} | unsigned | as I | unsigned |
Parallelism | any | as I | as I | as I |
Kernel Columns | 1 | as I | as I | as I |
Kernel Rows | 1 | as I | as I | as I |
Img Protocol | {VALT_IMAGE2D,VALT_LINE1D} | as I | as I | as I |
Color Format | VAF_GRAY | as I | as I | as I |
Color Flavor | FL_NONE | as I | as I | as I |
Max. Img Width | any | as I | as I | as I |
Max. Img Height | any | as I | as I | as I |
The use of operator ColMax is shown in the following examples:
-
Examples - A high speed and robust laser line detection algorithm. The algorithm determines center of gravity coordinates to obtain sub-pixel resolution results.
-
Examples - Shows how to split an merge image streams. Appends a trailer to the image.