The operator CONST provides a fixed value at the output link. All input values are discarded and replaced by the constant. The constant can be defined by parameter Value. This can either be a static or dynamic value. Thus the value can be changed during runtime.
Note that for multi component formats like RGB, the constant value is defined as a single value for the full pixel and not just the component.
Example: Output link RGB 24bit, constant value is set to 11862494 (0xB501DE). The output components will then be set to the following const values: R = 222 (0xDE), G = 01 (0x01) and B = 181 (0xB5). The constant concatenates the component values to a single value. The component 0 is placed in LSB area and the highest component in MSB area, i.e. for RGB, the constant value is {B-G-R}. Value = {component N-1, ..., component 0}, with N being the number of the components.
The range of the input bit width is [1, 64]. For signed inputs, the range is [2, 64]. For unsigned color inputs, the range is [3, 63] and for signed color, the range is [6, 63]. |
|
The range of the output for unsigned arithmetic is [1, 63]. For signed outputs, the range is [2, 64]. For unsigned color outputs, the range is [3, 63] and for signed color, the range is [6, 63]. |
|
The same const value is used for all kernel components. |
Value | |
---|---|
Type | static/dynamic read/write parameter |
Default | 0 |
Range | depends on arithmetic and bit width of the output link |
This parameter defines the value at the output link. If the parameter is set to Static, the value is selected at design time. If the parameter is Dynamic, it is possible to alter the value during runtime. |
The use of operator CONST is shown in the following examples:
-
Examples - A high speed and robust laser line detection algorithm. The algorithm determines center of gravity coordinates to obtain sub-pixel resolution results.
-
A binarization example for local adaptive thresholding. A kernel size of 8 by 8 pixel is used.
-
Examples - Shows how to vertically mirror an image. Note the mirroring of the parallel words and the pixel.