The operator IS_NotEqual sets the output to a logical "1" if the value at the input link I is not equal to the value of parameter Number, otherwise the output is "0".
To compare the values of two input links use operator CMP_NotEqual instead.
Link Parameter | Input Link I | Output Link O |
---|---|---|
Bit Width | [1, 63] unsigned, [2, 64] signed | 1 |
Arithmetic | {unsigned, signed} | unsigned |
Parallelism | any | as I |
Kernel Columns | any | as I |
Kernel Rows | any | as I |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
Color Format | VAF_GRAY | as I |
Color Flavor | FL_NONE | as I |
Max. Img Width | any | as I |
Max. Img Height | any | as I |
Number | |
---|---|
Type | static/dynamic read/write parameter |
Default | 0 |
Range | same as range of input link I |
Value to compare the input link value with. |
ImplementationType | ||||
---|---|---|---|---|
Type | static write parameter | |||
Default | AUTO | |||
Range | (AUTO, EmbeddedALU, LUT) | |||
Parameter ImplementationType allows you to influence the implementation of the operator, i.e., to define which logic elements are used for implementing the operator. You can select one of the following values: AUTO: When the operator is instantiated, the optimal implementation strategy for the given FPGA architecture is selected automatically, based on the parametrization of the operator. EmbeddedALU: The operator uses the embedded ALU elements of the FPGA. LUT: The operator uses the LUT elements of the FPGA.
|
The use of operator IS_NotEqual is shown in the following examples:
-
' Multiple DMA Channel Designs '
Remove 9 out of 10 images.
-
Examples - Downsampling by factor 3x3 without the use of operator SampleDn.
-
Examples - Shows how to split an merge image streams. Appends a trailer to the image.