The operator MAX identifies and outputs the maximum value of an input kernel-stream. This maximum value is output at O. The operator will not output the kernel index of the maximum value.
Link Parameter | Input Link I | Output Link O |
---|---|---|
Bit Width | [1, 64] unsigned, [2, 64] signed | as I |
Arithmetic | {unsigned, signed} | as I |
Parallelism | any | as I |
Kernel Columns | any | 1 |
Kernel Rows | any | 1 |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
Color Format | VAF_GRAY | as I |
Color Flavor | FL_NONE | as I |
Max. Img Width | any | as I |
Max. Img Height | any | as I |
The use of operator MAX is shown in the following examples:
-
Examples - The Kirsch filter is a good edge detection filter for non directional edges.