The operator CMP_AltB (compare A less than B) sets the output to a logical "1" if the value at the input link A is less than the value at the input link B, otherwise the output is "0".
To compare the value of input A with a dynamic parameter value use operator IS_LessThan instead.
Property | Value |
---|---|
Operator Type | O |
Input Links | A, data input B, data input |
Output Link | O, data output |
Link Parameter | Input Link A | Input Link B | Output Link O |
---|---|---|---|
Bit Width | [1, 64] unsigned, [2, 64] signed | [1, 64] unsigned, [2, 64] signed | 1 |
Arithmetic | {unsigned, signed} | as A | unsigned |
Parallelism | any | as A | as I |
Kernel Columns | any | as A | as I |
Kernel Rows | any | as A | as I |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as A | as I |
Color Format | VAF_GRAY | as A | as I |
Color Flavor | FL_NONE | as A | as I |
Max. Img Width | any | as A | as I |
Max. Img Height | any | as A | as I |
ImplementationType | ||||
---|---|---|---|---|
Type | static write parameter | |||
Default | AUTO | |||
Range | (AUTO, EmbeddedALU, LUT) | |||
Parameter ImplementationType allows you to influence the implementation of the operator, i.e., to define which logic elements are used for implementing the operator. You can select one of the following values: AUTO: When the operator is instantiated, the optimal implementation strategy for the given FPGA architecture is selected automatically, based on the parametrization of the operator. EmbeddedALU: The operator uses embedded ALU elements of the FPGA. LUT: The operator uses the LUT elements of the FPGA.
|