Operator CastColorSpace

The operator CastColorSpace changes the logical attribute Color Flavor. The values of the input link are copied to the output link. The operator will not influence the data stream and will not require any FPGA resources.

I/O Properties

Property Value
Operator Type O
Input Link I, data input
Output Link O, data output

Supported Link Format

Link Parameter Input Link I Output Link O
Bit Width [3, 63] unsigned, [6, 63] signed as I
Arithmetic {unsigned, signed} as I
Parallelism any as I
Kernel Columns any as I
Kernel Rows any as I
Img Protocol {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} as I
Color Format VAF_COLOR as I
Color Flavor any any except FL_NONE
Max. Img Width any as I
Max. Img Height any as I

Parameters

None