The operator ExpandPixel copies the last pixel of a line or a frame to all pixels in the next line or frame. The operator is used in two modes
-
Line sync mode
For each line, the last pixel value in a line is stored and kept constant for the next line.
Set parameter AutoSync to EoL to use this mode.
-
Frame sync mode
For each frame, the last pixel in the image is stored and kept constant during the next frame.
Set parameter AutoSync to EoF to use this mode.
Mind that the behavior of this operator will only affect the following line or frame and not the current line or frame. For this reason the output for the first lines or frame has to be specified using parameter Init.
Operator Restrictions
-
Empty images are not supported.
Images with varying line lengths are not supported.
Init | |
---|---|
Type | static parameter |
Default | 0 |
Range | [0, 2^InputBitWidth - 1] |
The parameter specifies the initialization value of of the pixels of the first image lines if AutoSync is set to EoL or the parameter specifies the pixels of the first output frame if AutoSync is set to Eof. The parameter will only accept unsigned values. For signed initialization values enter its unsigned representation. |
AutoSync | |
---|---|
Type | static parameter |
Default | EoL |
Range | {EoL, EoF} |
Specifies the synchronization mode of the operator. Use mode EoL to copy the last pixel of each line to all pixels of the following line. Use mode EoF to copy the last pixel of each frame to all pixels of the following frame. If the image protocol at the output is set to VALT_LINE1D, the parameter can only be set to EoL. |
The use of operator ExpandPixel is shown in the following examples:
-
Determines the mean value of an image and used the value as threshold value for the next image processed.
-
Example - Histogram thresholding