The operator IS_GreaterThan sets the output to a logical "1" if the value at the input link I is greater than the value of parameter Number, otherwise the output is "0".
To compare the values of two input links use operator CMP_AgtB instead.
Link Parameter | Input Link I | Output Link O |
---|---|---|
Bit Width | [1, 63] unsigned, [2, 64] signed | 1 |
Arithmetic | {unsigned, signed} | unsigned |
Parallelism | any | as I |
Kernel Columns | any | as I |
Kernel Rows | any | as I |
Img Protocol | {VALT_IMAGE2D, VALT_LINE1D, VALT_PIXEL0D} | as I |
Color Format | VAF_GRAY | as I |
Color Flavor | FL_NONE | as I |
Max. Img Width | any | as I |
Max. Img Height | any | as I |
Number | |
---|---|
Type | static/dynamic read/write parameter |
Default | 0 |
Range | same as range of input link I |
Value to compare the input link value with. |
ImplementationType | ||||
---|---|---|---|---|
Type | static write parameter | |||
Default | AUTO | |||
Range | (AUTO, EmbeddedALU, LUT) | |||
Parameter ImplementationType allows you to influence the implementation of the operator, i.e., to define which logic elements are used for implementing the operator. You can select one of the following values: AUTO: When the operator is instantiated, the optimal implementation strategy for the given FPGA architecture is selected automatically, based on the parametrization of the operator. EmbeddedALU: The operator uses the embedded ALU elements of the FPGA. LUT: The operator uses the LUT elements of the FPGA.
|
The use of operator IS_GreaterThan is shown in the following examples:
-
' Multiple DMA Channel Designs '
Threshold binarization
-
'ED Morphological Edge Detection'
Examples - A binary eroded image is compared with the original. An edge is detected if both differ.
-
Examples - Shows the implementation of a morphological close applied to binary images.
-
Examples - Shows the implementation of a morphological open applied to binary images.