Table of Contents
- BRANCH
- CastBitWidth
- CastColorSpace
- CastKernel
- CastParallel
- CastType
- CONST
- ConvertPixelFormat
- Coordinate_X
- Coordinate_Y
- Dummy
- DynamicROI
- EventToHost
- ExpandToKernel
- ExpandToParallel
- GetStatus
- HierarchicalBox
- ImageNumber
- KernelRemap
- MergeComponents
- MergeKernel
- MergeParallel
- MergePixel
- NOP
- PARALLELdn
- PARALLELup
- PseudoRandomNumberGen
- SampleDn
- SampleUp
- SelectBitField
- SelectComponent
- SelectFromParallel
- SelectROI
- SelectSubKernel
- SetDimension
- SplitComponents
- SplitKernel
- SplitParallel
- Trash
The Base library include common function operators required in most VisualApplets designs.
The following list summarizes all Operators of Library Base
Operator Name | Short Description | available since | |
---|---|---|---|
![]() |
BRANCH |
Clones the input link to a number of output links you can define. |
Version 1.1 |
![]() |
CastBitWidth |
Changes the bit width by selecting the lower bits of the input. |
Version 1.1 |
![]() |
CastColorSpace |
Changes the logical attribute <parameter>ColorFlavor.</parameter> |
Version 1.1 |
![]() |
CastKernel |
This operator re-organizes the parallelism and kernel size of the incoming data. |
Version 1.1 |
![]() |
CastParallel |
Enables the re-interpretation of the input link bits. |
Version 1.1 |
![]() |
CastType |
Changes the link property Arithmetic |
Version 1.1 |
![]() |
CONST |
Replaces each input value by a fixed value at the output link. |
Version 1.1 |
![]() |
ConvertPixelFormat |
Preserve as much information as possible, while arithmetic and bit width are adjusted to a desired output pixel format. |
Version 1.1 |
![]() |
Coordinate_X |
Provides the x coordinate of the input pixel at its output. |
Version 1.1 |
![]() |
Coordinate_Y |
Provides the y coordinate of the input pixel at its output. |
Version 1.1 |
![]() |
Dummy |
Is a place holder for non existing operators. |
Version 2 |
![]() |
DynamicROI |
Allows an ROI selection using input links. |
Version 1.2 |
![]() |
EventToHost |
Generates software events for rising edges at its input links. |
Version 2.2 |
![]() |
ExpandToKernel |
The operator expands the input link I to an arbitrary kernel size. |
Version 1.3 |
![]() |
ExpandToParallel |
The operator expands the input link I with parallelism 1 to an arbitrary parallelism at output link O. |
Version 1.1 |
![]() |
GetStatus |
Obtain the current value of a signal link. |
Version 1.2 |
![]() |
HierarchicalBox |
Groups several operators into a single module. |
Version 1.1 |
![]() |
ImageNumber |
Provides the image index of the current image of the input link at the output link. |
Version 1.1 |
![]() |
KernelRemap |
Remapping of kernel components. |
Version 1.4 |
![]() |
MergeComponents |
Merges three gray input links to one RGB output link |
Version 1.1 |
![]() |
MergeKernel |
Merges the input links into a kernel. |
Version 1.2 |
![]() |
MergeParallel |
The operator merges N input links to a single output link by concatenating the input links to parallelism components. |
Version 1.3 |
![]() |
MergePixel |
Merges pixels of multiples input links of the same parallelism into one pixel of larger bit width. |
Version 1.1 |
![]() |
NOP |
No operation. Outputs the registered input. |
Version 1.1 |
![]() |
PARALLELdn |
Decreases the parallelism between the input link and the output link. |
Version 1.1 |
![]() |
PARALLELup |
Increases the parallelism between the input link and the output link. |
Version 1.1 |
![]() |
PseudoRandomNumberGen |
Generates a stream of random values. |
Version 1.4 |
![]() |
SampleDn |
Reduces the image size by downsampling the input image. |
Version 1.1 |
![]() |
SampleUp |
Increases the image size by upsampling the input image. |
Version 1.1 |
![]() |
SelectBitField |
Enables the selection of a bit field. |
Version 1.1 |
![]() |
SelectComponent |
Extracts a single color component form the input link. |
Version 1.1 |
![]() |
SelectFromParallel |
Extracts a single parallelism component from the input link. |
Version 1.1 |
![]() |
SelectROI |
Extracts a rectangular region of interest (ROI) from the frames at the input link. |
Version 1.1 |
![]() |
SelectSubKernel |
Extracts a rectangular subset of the kernel matrix at the input link. |
Version 1.1 |
![]() |
SetDimension |
Enables to change of the link properties maximum image width and maximum image height. |
Version 1.1 |
![]() |
SplitComponents |
Separates the components of a color stream into three separate gray image streams. |
Version 1.1 |
![]() |
SplitKernel |
Splits the N x M kernel components of the input link into N * M output links. |
Version 1.3 |
![]() |
SplitParallel |
Splits the input link of parallelism degree N into N output links of parallelism degree 1 |
Version 1.3 |
![]() |
Trash |
A data sink for unused links. |
Version 1.1 |
Table 28. Operators of Library Base